Infineon Enables Accton’s New Portable WLAN VoIP Gateway
Munich, Germany and Taipei, Taiwan – January 23, 2006 – Infineon Technologies AG (FSE/NYSE: IFX), a leading provider of communication ICs, today announced that its WildPass
™ WLAN network processor system-on-chip (SoC) has been selected by Accton Technology Corporation, the Taiwan-based premier provider of networking and communications solutions. The WildPass SoC enables Accton’s VG2211i secure, portable wireless VoIP gateway. The gateway is ideally suited as a portable WLAN access point and VoIP router, meeting the increased mobility requirements of end-users, and can also be used to seamlessly and economically add WLAN and VoIP capabilities to existing broadband connections.
According to market research firm Point Topic, the number of broadband connections worldwide topped 205 million at the end of 2005, while research firm Infonetics indicates that the WLAN gateway market for broadband users is expected to grow between 2006 and 2008 by nearly 50 percent to around 37 million units.
The Accton VG2211i gateway enabled by Infineon’s WildPass SoC can be easily plugged into a broadband connection and provide WLAN connectivity for such applications as home networking and office access points. In addition, existing analog telephones can be connected to the VG2211i for making Voice over IP (VoIP) calls, allowing end-users to benefit from services such as a single phone number worldwide and lower calling rates.
“Infineon’s voice and networking knowledge, combined with its excellent silicon architecture and understanding of customer requirements, played a major role in our selection. The standard-compliant WLAN and fast routing capabilities of the WildPass SoC, as well as its multiple interfaces, perfectly meet the requirements of our gateway system,” said Cashew Chen, Marketing Vice President, Accton Technology Corporation.
“We are very proud that Accton, a key player in the broadband and VoIP gateway market, selected the Infineon WildPass SoC, which is the industry’s most integrated secure WLAN network processor SoC,” commented Christian Wolff, Senior Vice President of the Communication Business Group and General Manager of the Wireline Access Business Unit at Infineon. “With our engineering know-how, operational excellence and ‘ready-to-go’ software, we enable our customers to place more economical, high-quality solutions on the market well ahead of the competition.”
The WildPass SoC is part of Infineon’s advanced CPE (customer premises equipment) solutions portfolio, which also includes Amazon (ADSL2+), VINAX-CPE (VDSL 2), VINETIC (VoIP processor), ADM5120 (network processor) and a number of Ethernet switch and PHY devices. It can be seamlessly integrated into a wide variety of network applications, such as VoIP access points, broadband routers and gateways, as well as media and print servers.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for automotive, industrial and multimarket sectors, for applications in communication, as well as memory products. With a global presence, Infineon operates through its subsidiaries in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2005 (ending September), the company achieved sales of Euro 6.76 billion with about 36,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at
www.infineon.com.
Information Number
INFCOM200601.027
Press Photos
-
The WildPass SoC enables Accton's VG2211i secure, portable wireless VoIP gateway. The gateway is ideally suited as a portable WLAN access point and VoIP router, meeting the increased mobility requirements of end-users, and can also be used to seamlessly and economically add WLAN and VoIP capabilities to existing broadband connections. WildPass kommt im neuen tragbaren VoIP-Gateway-System VG2211i von Accton für sichere drahtlose Übertragung zum Einsatz. Als tragbarer Access Point bzw. VoIP-Router erfüllt das Gateway-System die Anforderungen der zunehmend mobilen Endverbraucher. Zudem können damit bestehende Breitbandzugangslösungen einfach und preiswert um WLAN- und VoIP-Funktionalität erweitert werden.Infineon Enables Accton’s New Portable WLAN VoIP GatewayJPG | 1.65 mb | 3543 x 2531 px