Infineon Introduces Ethernet Switch Platform: Shows VDSL and LAN Access Solutions Based on Flexible, High-Integration Switch-on-Chip
Supercomm, Atlanta GA June 3, 2003 Infineon Technologies (FSE/NYSE: IFX), today introduced the Purple (PLB2800) Layer2+ Ethernet Access Switch-on-Chip solution. With twice the port density of existing Ethernet switches, the single-chip Purple device supports seven different configurations, ranging from 48 Fast Ethernet (FE) + 2 Gigabit Ethernet (GbE) ports up to 8 GbE ports, for access switch designs handling standard Ethernet, Ethernet-over-Fiber, and VDSL links.
Infineon is showing two switch configurations, available as complete reference designs, in its booth at Supercomm (#22637/22737), June 3- 5 in Atlanta. The Purple2800x, a fully functional LAN Access switch evaluation platform, and the SP-VDSL2800, a fully operational Ethernet Access system based on the Purple and Infineons high-speed QAM VDSL PHYs.
The small size 388 P-BGA package Switch-on-Chip offers industry leading Fast Ethernet system integration with no external packet memory or controller, resulting in space, power and cost efficient designs. It allows for up to 48 high-speed Ethernet downlink ports, enabling system manufacturers to engineer high-density broadband access switching systems. The range of applications supported by the Purple Switch-on-Chip include IP-DSLAM/DLCs, high port count workgroup switches, GbE aggregators, LAN Access Switches, Cellular base stations and Packet over SONET/SDH systems.
As a part of its Agenda 5-to-1 strategy to build on current leading market positions, Infineon is focusing on providing feature-rich system solutions that enable our customers to streamline design efforts, shorten time to market and add value in higher level applications and integration, said Christian Wolff, Vice President of Infineons Wireline Communications Business Group and General Manager of the Access Business Unit. The Purple Ethernet access Switch-on-Chip is a powerful component of our solution offering, as it supports designs using multiple access technologies, as well as products from our optical transceiver portfolio. It represents an industry first in terms of port-density as well as advanced security features, and helps to strengthen our position in the Ethernet access market.
The new Purple is a complete Layer2+ Switch-on-Chip solution. The device is also the first Ethernet Switch-on-Chip to integrate the high-performance MIPS 5Kc 64-bit core as an embedded CPU subsystem, enabling execution of management software protocols, stacking and handling, and Quality-of-Service (QoS) policies. The feature set of the Purple includes a 21Gbps/12Mpps switching engine for solid L2+ wire speed switching performance, 16MBit embedded DRAM packet buffer; SRAM for 8k MAC addresses resolution; sophisticated L2-L7 Flow Engine to implement security, QoS guarantees and bandwidth control as well as billing and accounting functions and Stacked VLAN (Virtual Local Area Network) capability to uniquely identify customer traffic in a public network. Built-in stacking support offers scalability and flexibility. This advanced feature set and processing power provides the performance headroom to easily master complex and demanding traffic patterns across different types of networks.
The Purple2800x is the evaluation and demonstration platform for Infineons Purple (PLB 2800) 48FE + 2GbE up to 8GbE Configurable Switch-on-Chip with embedded memory and CPU. The Purple2800x comes complete with a chassis, main board, power supply, and LED front panel. In addition, Plug and Play modules are supplied in three basic configurations: Octal FE, GbE Copper, and GbE Fiber.
Infineon's SP-VDSL2800 is a highly integrated Layer 2+ Ethernet over VDSL (EoVDSL) switch evaluation and demonstration system. It combines Infineons high-capacity Purple Switch-on-Chip and Infineons field proven PoVDSL (Packet over VDSL) PHYs for a one-stop shop Ethernet access solution. The SP-VDSL2800 comes complete with chassis, power supply, and LED front panel. It features 24 single-port PoVDSL PHYs, as well as two Plug and Play GbE Copper or GbE Fiber uplink modules. The main board is expandable up to 48 PoVDSL PHYs.
The Purple (PLB 2800) Switch-on-Chip is priced at $103 in sample quantities (up to 1k). Device samples, software drivers and reference designs for the Purple are available now, and the device is in production. Extended temperature range versions (PLF2800), for operating environments of 40oC to 85oC, are also available.
Infineon is showing two switch configurations, available as complete reference designs, in its booth at Supercomm (#22637/22737), June 3- 5 in Atlanta. The Purple2800x, a fully functional LAN Access switch evaluation platform, and the SP-VDSL2800, a fully operational Ethernet Access system based on the Purple and Infineons high-speed QAM VDSL PHYs.
The small size 388 P-BGA package Switch-on-Chip offers industry leading Fast Ethernet system integration with no external packet memory or controller, resulting in space, power and cost efficient designs. It allows for up to 48 high-speed Ethernet downlink ports, enabling system manufacturers to engineer high-density broadband access switching systems. The range of applications supported by the Purple Switch-on-Chip include IP-DSLAM/DLCs, high port count workgroup switches, GbE aggregators, LAN Access Switches, Cellular base stations and Packet over SONET/SDH systems.
As a part of its Agenda 5-to-1 strategy to build on current leading market positions, Infineon is focusing on providing feature-rich system solutions that enable our customers to streamline design efforts, shorten time to market and add value in higher level applications and integration, said Christian Wolff, Vice President of Infineons Wireline Communications Business Group and General Manager of the Access Business Unit. The Purple Ethernet access Switch-on-Chip is a powerful component of our solution offering, as it supports designs using multiple access technologies, as well as products from our optical transceiver portfolio. It represents an industry first in terms of port-density as well as advanced security features, and helps to strengthen our position in the Ethernet access market.
About Infineons Purple (PLB2800) Ethernet Switch-on-Chip
The new Purple is a complete Layer2+ Switch-on-Chip solution. The device is also the first Ethernet Switch-on-Chip to integrate the high-performance MIPS 5Kc 64-bit core as an embedded CPU subsystem, enabling execution of management software protocols, stacking and handling, and Quality-of-Service (QoS) policies. The feature set of the Purple includes a 21Gbps/12Mpps switching engine for solid L2+ wire speed switching performance, 16MBit embedded DRAM packet buffer; SRAM for 8k MAC addresses resolution; sophisticated L2-L7 Flow Engine to implement security, QoS guarantees and bandwidth control as well as billing and accounting functions and Stacked VLAN (Virtual Local Area Network) capability to uniquely identify customer traffic in a public network. Built-in stacking support offers scalability and flexibility. This advanced feature set and processing power provides the performance headroom to easily master complex and demanding traffic patterns across different types of networks.
About Infineons VDSL and LAN Access Evaluation Platforms
The Purple2800x is the evaluation and demonstration platform for Infineons Purple (PLB 2800) 48FE + 2GbE up to 8GbE Configurable Switch-on-Chip with embedded memory and CPU. The Purple2800x comes complete with a chassis, main board, power supply, and LED front panel. In addition, Plug and Play modules are supplied in three basic configurations: Octal FE, GbE Copper, and GbE Fiber.
Infineon's SP-VDSL2800 is a highly integrated Layer 2+ Ethernet over VDSL (EoVDSL) switch evaluation and demonstration system. It combines Infineons high-capacity Purple Switch-on-Chip and Infineons field proven PoVDSL (Packet over VDSL) PHYs for a one-stop shop Ethernet access solution. The SP-VDSL2800 comes complete with chassis, power supply, and LED front panel. It features 24 single-port PoVDSL PHYs, as well as two Plug and Play GbE Copper or GbE Fiber uplink modules. The main board is expandable up to 48 PoVDSL PHYs.
Pricing and Availability
The Purple (PLB 2800) Switch-on-Chip is priced at $103 in sample quantities (up to 1k). Device samples, software drivers and reference designs for the Purple are available now, and the device is in production. Extended temperature range versions (PLF2800), for operating environments of 40oC to 85oC, are also available.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2002 (ending September), the company achieved sales of Euro 5.21 billion with about 30,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at http://www.infineon.com
Infineon, Infineon Technologies, and the stylized Infineon Technologies design are registered trademarks and service marks of Infineon Technologies AG in the United States and/or other countries. Other company, product and service names may be trademarks or service marks of others.
Information Number
INFCOM200306.081
Press Photos
-
The flexible and highly integrated Purple (PLB2800) Switch-on-Chip offers industry leading Fast Ethernet system integration with no external packet memory or controller, resulting in space, power and cost efficient designs.Press PhotoJPG | 196 kb | 1535 x 1063 px
Press PhotoJPG | 9 kb | 160 x 111 px