Infineon Selects Sonim as Preferred Partner for Push-To-Talk - Adding Instant Voice Messaging Functionality to Infineon´s Mobile Platform Solution
Munich, Germany and San Mateo, USA, October 29, 2002 Infineon Technologies (FSE/NYSE: IFX) today announced that it has selected Sonim Technologies Instant Communications Platform for its APOXI (Application Programming Object-oriented eXtendable Interface) framework and development environment - an integral part of Infineons complete wireless system solution. Sonims Instant Communications Platform allows operators for the first time to deploy presence-enabled, instant voice messaging services such as Push-To-Talk over wireless data networks.
For wireless users, Push to Talk offers a new means of communicating with one or many individuals at the push of a button on a wireless device. With a Push-To-Talk enabled wireless device, a user can review the availability of contacts or buddies in the address book, similar to text instant messaging services like ICQ or Yahoo. Based on who is available, the user can simply push a button and start a Push-to-Talk dialog in a walkie-talkie or chat room like mode. Additionally, with the Direct Message service, a user can select one or many individuals in the contact list of the wireless device, create a voice message of any length and send it at the push of a button. As a recipient of a Direct Message, the user is alerted of a new voice message, and can retrieve that message instantly.
Adding Sonims solution to our APOXI framework represents yet another key milestone in our strategy to provide our customers, with compelling solutions, said Karl Lange, Vice President and General Manager Customized Wireless Solutions at Infineon. Based on Infineons wireless design offering, manufacturers of wireless communication devices and mobile operators will achieve a significant time-to-market advantage for these types of killer applications, allowing them to differentiate themselves and create additional revenue streams. Most importantly, being the first provider of this solution, gives Infineon a clear market advantage in the highly competitive market for GPRS solutions.
We are excited to partner with a market leader like Infineon Technologies, who has demonstrated thought leadership in enabling its customers to build high-value applications. said John Burns, CEO and president of Sonim Technologies. The wireless industry recognizes that interoperability is a key to the success of new services, and working with leading vendors like Infineon creates the foundation for broad acceptance of Sonims Instant Communications solutions.
Infineon and Sonim will market the joint APOXI/Sonim solution to Infineons large base of branded device manufacturers as well as original device manufacturers (ODMs). The Sonim Instant Communications Client will be available on Infineons APOXI platform and supported by a wide range of Infineon chipsets. APOXI is an excellent development framework for the Sonim Client as it allows us to leverage core functionality within the chip set, ensuring superior quality of service as well as minimizing power consumption, said Bob Plaschke, Executive Vice President of Marketing at Sonim.
The Sonim Instant Communications Platform allows wireless carriers to deliver voice and text applications that fully leverage IP/SIP protocol efficiencies to generate high value traffic for 802.11, GPRS and 3G networks. The platform also leverages new codec technology with IP, which allows the solution to use a fraction of the network resources that would typically be used over a circuit network.
APOXI is an object-oriented framework and development environment designed to speed and enhance mobile application development, as well as to meet the special requirements for emerging applications on wireless communication devices. The APOXI framework is an integral part of Infineons strategy to provide a complete solution with a broad set of applications for wireless communication devices complementing a best-in-class protocol stack and high performance chip sets. APOXI has been developed by Comneon, a hundred percent subsidiary of Infineon.
For wireless users, Push to Talk offers a new means of communicating with one or many individuals at the push of a button on a wireless device. With a Push-To-Talk enabled wireless device, a user can review the availability of contacts or buddies in the address book, similar to text instant messaging services like ICQ or Yahoo. Based on who is available, the user can simply push a button and start a Push-to-Talk dialog in a walkie-talkie or chat room like mode. Additionally, with the Direct Message service, a user can select one or many individuals in the contact list of the wireless device, create a voice message of any length and send it at the push of a button. As a recipient of a Direct Message, the user is alerted of a new voice message, and can retrieve that message instantly.
Adding Sonims solution to our APOXI framework represents yet another key milestone in our strategy to provide our customers, with compelling solutions, said Karl Lange, Vice President and General Manager Customized Wireless Solutions at Infineon. Based on Infineons wireless design offering, manufacturers of wireless communication devices and mobile operators will achieve a significant time-to-market advantage for these types of killer applications, allowing them to differentiate themselves and create additional revenue streams. Most importantly, being the first provider of this solution, gives Infineon a clear market advantage in the highly competitive market for GPRS solutions.
We are excited to partner with a market leader like Infineon Technologies, who has demonstrated thought leadership in enabling its customers to build high-value applications. said John Burns, CEO and president of Sonim Technologies. The wireless industry recognizes that interoperability is a key to the success of new services, and working with leading vendors like Infineon creates the foundation for broad acceptance of Sonims Instant Communications solutions.
Infineon and Sonim will market the joint APOXI/Sonim solution to Infineons large base of branded device manufacturers as well as original device manufacturers (ODMs). The Sonim Instant Communications Client will be available on Infineons APOXI platform and supported by a wide range of Infineon chipsets. APOXI is an excellent development framework for the Sonim Client as it allows us to leverage core functionality within the chip set, ensuring superior quality of service as well as minimizing power consumption, said Bob Plaschke, Executive Vice President of Marketing at Sonim.
The Sonim Instant Communications Platform allows wireless carriers to deliver voice and text applications that fully leverage IP/SIP protocol efficiencies to generate high value traffic for 802.11, GPRS and 3G networks. The platform also leverages new codec technology with IP, which allows the solution to use a fraction of the network resources that would typically be used over a circuit network.
APOXI is an object-oriented framework and development environment designed to speed and enhance mobile application development, as well as to meet the special requirements for emerging applications on wireless communication devices. The APOXI framework is an integral part of Infineons strategy to provide a complete solution with a broad set of applications for wireless communication devices complementing a best-in-class protocol stack and high performance chip sets. APOXI has been developed by Comneon, a hundred percent subsidiary of Infineon.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2001 (ending September), the company achieved sales of Euro 5.67 billion with about 33,800 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Sock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.
About Sonim Technologies, Inc.
Sonim Technologies is a leading provider of IP-based Instant Communications solutions optimized for GPRS, 3G and 802.11 wireless data networks. Based on open, global standards, the Sonim platform combines presence and availability with high-margin messaging services such as Push-To-Talk. These solutions allow wireless operators to leverage existing investments in data networks, create new revenue streams and deliver superior return on bandwidth. Sonim is headquartered in San Mateo, Calif., with sales and engineering offices in Italy, the United Kingdom, and India. For more information, visit the company's Web site at www.sonimtech.com.
Information Number
INFWS200210.008e