Infineon Technologies Introduces Fully Integrated SiGe Ultra Low Noise Amplifier for UMTS and further Mobile Applications
Munich, September 25, 2001 Infineon Technologies (NYSE/DAX: IFX) today announced the availability of BGA622, an integrated Low Noise Amplifier (LNA) especially designed for the high linearity and sensitivity requirements of existing and next generation wireless applications including GSM, GPS, UMTS and Wireless LAN. Based on Infineon`s B7HF Silicon-Germanium (SiGe) bipolar process technology the Monolithic Microwave IC offers very low noise figures and high gain for reliable and high performance mobile communication applications.
By addressing the specific front-end requirements such as high linearity, low noise figures and low power consumption, the BGA622 is an ideal solution for actual and future mobile applications up to 6 GHz, said Thomas Pollakowski, Vice President and General Manager Discretes from Infineon Technologies. The introduction of this new high-performance LNA underlines Infineon`s strengths in process technologies and the capability of providing solutions for high volume, mobile communications applications to ensure a fast time to market for the customers.
The high-end amplifier features a gain of 15 dB and an ultra low noise figure of 1.1 dB at 2.1 GHz, an industry wide new benchmark record for SiGe based LNA in volume production. The BGA622 takes full advantage of the high performance B7HF SiGe process technology, which allows transition frequencies of up to 75 GHz. The new LNA also provides matched input/outputs and requires no further external components for in-circuit application. A low supply current and an integrated on/off feature enable low power consumption and increased standby time for 3G handsets.
As a "Plug and Play" gain block the BGA622 can be combined with any 2G or 3G transceiver chip on the market to improve gain and NF at 900 MHz to 6 GHz.
The BGA622 is available in sample quantities in an ultra small SOT343 package. Mass production will commence in November 2001.
By addressing the specific front-end requirements such as high linearity, low noise figures and low power consumption, the BGA622 is an ideal solution for actual and future mobile applications up to 6 GHz, said Thomas Pollakowski, Vice President and General Manager Discretes from Infineon Technologies. The introduction of this new high-performance LNA underlines Infineon`s strengths in process technologies and the capability of providing solutions for high volume, mobile communications applications to ensure a fast time to market for the customers.
The high-end amplifier features a gain of 15 dB and an ultra low noise figure of 1.1 dB at 2.1 GHz, an industry wide new benchmark record for SiGe based LNA in volume production. The BGA622 takes full advantage of the high performance B7HF SiGe process technology, which allows transition frequencies of up to 75 GHz. The new LNA also provides matched input/outputs and requires no further external components for in-circuit application. A low supply current and an integrated on/off feature enable low power consumption and increased standby time for 3G handsets.
As a "Plug and Play" gain block the BGA622 can be combined with any 2G or 3G transceiver chip on the market to improve gain and NF at 900 MHz to 6 GHz.
Availability
The BGA622 is available in sample quantities in an ultra small SOT343 package. Mass production will commence in November 2001.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2000 (ending September), the company achieved sales of Euro 7.28 billion with about 29,000 employees world-wide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com
Information Number
INFWS200109.119e
Press Photos
-
Infineon Technologies Introduces Fully Integrated SiGe Ultra Low Noise Amplifier for UMTS and further Mobile ApplicationsPress PictureJPG | 620 kb | 1535 x 1063 px