IBM, Infineon to Advance Revolutionary Memory Technology
Joint News Release by IBM and Infineon
East Fishkill, N.Y., and Munich, Germany -- December 7, 2000 -- IBM and Infineon Technologies AG (FSE/NYSE: IFX) today announced plans to jointly develop a breakthrough memory technology that could significantly increase battery life of portable computing devices and lead to "instant-on" computers.
The two companies have signed an agreement to collaborate in the development of Magnetic Random Access Memory (MRAM), which uses magnetic, rather than electronic, charges to store bits of data. MRAM may significantly improve electronic products - from computers to cell phones to game systems - by storing more information, accessing it faster and using less battery power than the electronic memory used today. MRAM also retains information when power is turned off, meaning products like personal computers could start up instantly, without waiting for software to boot up.
IBM Research pioneered the development of a miniature component called the magnetic tunnel junction as early as 1974, eventually adapting it as a means to store information and to build an actual working MRAM chip in 1998. Using this IBM technology, coupled with Infineons considerable expertise in creating very high density semiconductor memory, the companies believe actual MRAM products could be commercially available as soon as 2004.
"MRAM has the potential to replace todays memory technologies in electronic products of the future," said Bijan Davari, IBM Fellow and Vice President of Technology and Emerging Products, IBM Microelectronics. "Todays announcement represents a major step forward for MRAM, quickly moving the technology out of the pure research stage into product development.
IBM and Infineon have more than 10 years experience successfully developing new chip technologies together, including traditional Dynamic RAM (DRAM), logic and embedded-DRAM technologies.
"Infineon and IBM are combining their technological capabilities and resources to help bring MRAM technology to maturity on a fast track, said Wilhelm Beinvogl, Senior Vice President of Technologies and Innovations, Memory Products, Infineon Technologies. Our proven track record in the joint development of advanced memory and logic technologies is thus further extended by a very exciting and new kind of technology. For Infineon, MRAM technology offers equally interesting potential both for embedded logic products and standalone memory chip applications.
MRAM combines the best features of todays common semiconductor memory technologies -- the high speed of Static RAM (SRAM), the storage capacity and low-cost of DRAM and the non-volatility of Flash memory.
This non-volatility carries significant implications, especially for emerging pervasive computing devices. Memory technologies like DRAM and SRAM require constant electrical power to retain stored data; when power is cut off, all data in memory is lost. A laptop computer, for example, works from a copy of its software stored in memory. When turned on, a working version of the software is copied from the hard disk drive into memory so the user can access it quickly. When power is turned off and then back on, the process has to start over. By using MRAM, the laptop could work more like other electronic devices such as a television or radio - turn the power on and the machine jumps to life.
Non-volatility can save power as well. Since MRAM will not need constant power to keep the data intact, it could consume much less than current random access memory technologies, extending the battery life of cell phones, handheld devices, laptops and other battery powered products.
A combined workforce of approximately 80 IBM and Infineon engineers and scientists will be assisting with the project. Development work will be conducted at IBMs Thomas J. Watson Research Center in Yorktown Heights, NY., IBMs Almaden Research Center in San Jose, Calif., and the IBM Microelectronics Semiconductor Research & Development Center (SRDC) in East Fishkill, NY., with additional design and test activity at IBMs facility in Burlington, VT.
IBM Microelectronics is a key contributor to IBM's role as the world's premier information technology supplier. IBM Microelectronics develops, manufactures and markets state-of-the-art semiconductor technologies, products, packaging and services. Its superior integrated solutions can be found in many of the world's best-known electronic brands. More information about IBM Microelectronics can be found at http://www.chips.ibm.com. IBM Research is the world's largest information technology research organization, with more than 3,000 scientists and engineers at eight labs in six countries. IBM has produced more research breakthroughs than any other company in the IT industry. IBMs early work with MRAM was conducted in cooperation with the U.S. Defense Advanced Research Agency (DARPA). For more information on IBM Research, visit www.research.ibm.com.
East Fishkill, N.Y., and Munich, Germany -- December 7, 2000 -- IBM and Infineon Technologies AG (FSE/NYSE: IFX) today announced plans to jointly develop a breakthrough memory technology that could significantly increase battery life of portable computing devices and lead to "instant-on" computers.
The two companies have signed an agreement to collaborate in the development of Magnetic Random Access Memory (MRAM), which uses magnetic, rather than electronic, charges to store bits of data. MRAM may significantly improve electronic products - from computers to cell phones to game systems - by storing more information, accessing it faster and using less battery power than the electronic memory used today. MRAM also retains information when power is turned off, meaning products like personal computers could start up instantly, without waiting for software to boot up.
IBM Research pioneered the development of a miniature component called the magnetic tunnel junction as early as 1974, eventually adapting it as a means to store information and to build an actual working MRAM chip in 1998. Using this IBM technology, coupled with Infineons considerable expertise in creating very high density semiconductor memory, the companies believe actual MRAM products could be commercially available as soon as 2004.
"MRAM has the potential to replace todays memory technologies in electronic products of the future," said Bijan Davari, IBM Fellow and Vice President of Technology and Emerging Products, IBM Microelectronics. "Todays announcement represents a major step forward for MRAM, quickly moving the technology out of the pure research stage into product development.
IBM and Infineon have more than 10 years experience successfully developing new chip technologies together, including traditional Dynamic RAM (DRAM), logic and embedded-DRAM technologies.
"Infineon and IBM are combining their technological capabilities and resources to help bring MRAM technology to maturity on a fast track, said Wilhelm Beinvogl, Senior Vice President of Technologies and Innovations, Memory Products, Infineon Technologies. Our proven track record in the joint development of advanced memory and logic technologies is thus further extended by a very exciting and new kind of technology. For Infineon, MRAM technology offers equally interesting potential both for embedded logic products and standalone memory chip applications.
MRAM combines the best features of todays common semiconductor memory technologies -- the high speed of Static RAM (SRAM), the storage capacity and low-cost of DRAM and the non-volatility of Flash memory.
This non-volatility carries significant implications, especially for emerging pervasive computing devices. Memory technologies like DRAM and SRAM require constant electrical power to retain stored data; when power is cut off, all data in memory is lost. A laptop computer, for example, works from a copy of its software stored in memory. When turned on, a working version of the software is copied from the hard disk drive into memory so the user can access it quickly. When power is turned off and then back on, the process has to start over. By using MRAM, the laptop could work more like other electronic devices such as a television or radio - turn the power on and the machine jumps to life.
Non-volatility can save power as well. Since MRAM will not need constant power to keep the data intact, it could consume much less than current random access memory technologies, extending the battery life of cell phones, handheld devices, laptops and other battery powered products.
A combined workforce of approximately 80 IBM and Infineon engineers and scientists will be assisting with the project. Development work will be conducted at IBMs Thomas J. Watson Research Center in Yorktown Heights, NY., IBMs Almaden Research Center in San Jose, Calif., and the IBM Microelectronics Semiconductor Research & Development Center (SRDC) in East Fishkill, NY., with additional design and test activity at IBMs facility in Burlington, VT.
About IBM Microelectronics & Research Divisions
IBM Microelectronics is a key contributor to IBM's role as the world's premier information technology supplier. IBM Microelectronics develops, manufactures and markets state-of-the-art semiconductor technologies, products, packaging and services. Its superior integrated solutions can be found in many of the world's best-known electronic brands. More information about IBM Microelectronics can be found at http://www.chips.ibm.com. IBM Research is the world's largest information technology research organization, with more than 3,000 scientists and engineers at eight labs in six countries. IBM has produced more research breakthroughs than any other company in the IT industry. IBMs early work with MRAM was conducted in cooperation with the U.S. Defense Advanced Research Agency (DARPA). For more information on IBM Research, visit www.research.ibm.com.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2000 (ending September), the company achieved sales of Euro 7.28 billion with about 29,000 employees worldwide. Infineons early work with MRAM was conducted in cooperation with the German Ministry of Education and Technology (BMBF). Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com.
Media Relations Contacts IBM Microelectronics Division:
Michael Loughran
Phone: ++1 914 892 5463
Fax: ++1 914 892 5334
Rupert Deighton
Phone: ++41 229 18 46 11
Rupertmicro@fr.ibm.com
Information Number
INFMP200012.020e