Shareholder Structure

Shareholder Structure

Sec. 33 of the German Securities Trading Act (Wertpapierhandelsgesetz – “WpHG”) requires each person whose shareholding reaches, exceeds or, after exceeding, falls below the 3%, 5%, 10%, 15%, 20%, 25%, 30%, 50% or 75% voting rights thresholds of a listed corporation to notify such to the corporation and to the German Federal Supervisory Authority for Financial Services (Bundesanstalt für Finanzdienstleistungsaufsicht - "BaFin") immediately, but no later than four trading days after they have reached, exceeded or fallen below such a threshold. For the purpose of determining the relevant shareholding, voting rights which are deemed to be held by way of attribution according to sec. 34 WpHG must also be taken into consideration. Non-compliance with the notification requirement has serious consequences: such holders cannot exercise any rights from any of the shares concerned until the disclosure requirement has been complied with (and in certain cases six months longer). In addition, severe fines can be imposed on the relevant shareholder.

The voting rights held by the investors listed in the following table are taken from the respective latest shareholder notification to Infineon. The stated percentages in the second column refer to the number of shares on which the notification has been based.

Investor relating to the number of shares on which the notification has been based

BlackRock, Inc.

5.36%
(as of 24 Jun 2019, relating to 1,250,188,637 shares)

Kingdom of Norway

4.85%
(as of 30 Sep 2019, relating to 1,250,295,877 shares)

Allianz Global Investors GmbH

4.82%
(as of 18 Jun 2019, relating to 1,250,188,637 shares)

 (Status: 01 October 2019)

Publication of Shareholder Notifications

According to sec. 40 of the German Securities Trading Act Infineon is obligated to disclose notifications of voting rights made pursuant to sec. 33, 34 and 38 and 39 WpHG. We comply to this obligation by using the Internet platform of DGAP (Deutsche Gesellschaft für Ad-hoc-Publizität mbH). The complete wording of these disclosures is available here.

Total Voting Rights Announcements

Click here for total voting rights according to sec. 41 WpHG.