| Title |
Description |
| mbed-os-example-capsense |
This example demonstrates implementing CapSense buttons and slider for PSoC™ 6 MCU with Mbed OS. |
| mbed-os-example-csdidac |
This example demonstrates using the CSD current digital-to-analog converter (IDAC) as a current source and a current sink. |
| mbed-os-example-csdadc |
This example demonstrates the usage of CSD analog to digital converter (ADC) for PSoC™ 6 MCU with Mbed OS using the CSDADC Middleware Library. |
| mbed-os-example-xip |
This example demonstrates the Execute-In-Place (XIP) feature of PSoC™ 6 MCU using external serial memory. |
| mbed-os-example-wlan-lowpower |
This code example demonstrates low power operation of the host MCU and WLAN device. |
| mbed-os-example-emwin-eink |
This code example demonstrates displaying graphics on an EInk display using EmWin graphics library in Mbed OS. |
| mbed-os-example-emwin-oled |
This example demonstrates how to display graphics on an OLED display using emWin graphics library in Mbed OS. |
| mbed-os-example-enterprise-security |
This code example demonstrates connecting to an enterprise network with one of the following protocols EAP, PEAP or EAP-TTLS. |
| mbed-os-example-https-server |
This code example demonstrates the implementation of an HTTPS server with PSoC™ 6 MCU and CYW43xxx connectivity devices. It employs the HTTPS server middleware library, which takes care of all the underlying socket connections with the HTTPS client. In this example, the HTTPS server establishes a secure connection with a HTTPS client through SSL handshake. Once the SSL handshake completes successfully, the HTTPS client can make GET, POST, and PUT requests with the secure server. |
| mbed-os-example-wlan-offload-discard-packet |
This application demonstrates the discard packet filter offload. The application is configured with a discard packet filter for the ICMP packet type using ModusToolbox 2.0 Device Configurator tool so that the WLAN will discard ICMP packets that are trying to reach the host. |
| mbed-os-example-wlan-offload-packet-filter |
This code example demonstrates packet filter offload functionality offered by WLAN devices. The packet filter offload functionality helps host to enter and stay in Deep Sleep longer and wake up only for the WLAN packets the host wants to service. |
| mbed-os-example-wlan-offload-arp |
The example demonstrates the Host MCU sleep/deepsleep while offloading the ARP(Address Resolution Protocol) service to the WLAN device. |
| mbed-os-example-wifi-provisioning-via-ble |
This code example demonstrates how to connect a kit to WiFi by provisioning the WiFi credentials via BLE. |
| mbed-os-example-aws-iot-client |
The applications connect to a Wi-Fi network as a STA(client), establish a secure TCP connection over MQTT to the AWS endpoint and publish or subscribe messages to/from the AWS cloud. |
| mbed-os-example-aws-greengrass |
The applications connect to a Wi-Fi network as a STA(client), discover Greengrass core devices, establish a secure TCP connection over MQTT to the AWS Greengrass endpoint and publish or subscribe messages periodically to/from the AWS cloud. |
| mbed-os-example-zipkey |
This code example demonstrates onboarding a device to a Wi-Fi network using ZipKey (or) SoftAP onboarding feature that is provided by the cirrent library. |