| Title |
Description |
| mtb-example-anycloud-ota-mqtt |
This code example demonstrates Over-the-Air (OTA) firmware update using the AnyCloud SDK for PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-tcp-client |
This code example demonstrates implementing a TCP client using the AnyCloud SDK for PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-wifi-scan |
This example demonstrates how to configure different scan filters provided in the Wi-Fi Connection Manager (WCM) middleware and scan for the available Wi-Fi networks using PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-tcp-server |
This code example demonstrates implementing a TCP server using the AnyCloud SDK for PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-mqtt-client |
This code example demonstrates connecting to an MQTT Broker using the AnyCloud MQTT Client library that implements an MQTT 3.1.1 Client. |
| mtb-example-anycloud-wps-enrollee |
This example demonstrates how to use the connection management and WPS Enrollee features provided in the AnyCloud Wi-Fi Connection Manager (WCM) middleware using PSoC™ MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-wlan-lowpower |
This code example demonstrates the low-power operation of PSoC™ 6 MCU and CYW43xxx connectivity devices using the AnyCloud Low Power Assistant (LPA) middleware library. |
| mtb-example-anycloud-secure-tcp-server |
This code example demonstrates implementing a secure TCP server using the AnyCloud SDK for PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-offload-tcp-keepalive |
This code example demonstrates the TCP Keepalive Offload functionality offered by Wi-Fi devices using PSoC™ 6 MCU. It employs the AnyCloud Low Power Assistant (LPA) middleware library which helps in developing low power wireless applications for the Infineon devices. |
| mtb-example-anycloud-secure-tcp-client |
This code example demonstrates implementing a secure TCP client using the AnyCloud SDK for PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-ble-multi-beacon |
This code example demonstrates the implementation of a beacon which advertises multiple Eddystone ADV data. |
| mtb-example-anycloud-ble-wifi-onboarding |
This example uses the Arm Cortex-M4 (CM4) CPU of PSoC™ 6 MCU to communicate with the CYW43xxx combo devices and control the Wi-Fi and BLE functionality. It uses BLE on the combo device to help connect the Wi-Fi to the AP. It also enables low-power mode on Wi-Fi and BLE. |
| mtb-example-anycloud-ble-battery-server |
This code example demonstrates the implementation of a simple BLE Battery Service using the Combo (WiFi+BT) SoCs and ModusToolbox™ Software Environment. |
| mtb-example-anycloud-ble-capsense-buttons-slider |
This code example features a 5-segment CapSense slider and two CapSense buttons with BLE custom service. Button 0 turns the LED on, Button 1 turns the LED off and the slider controls the brightness of the LED. The LED status is notified to the client via BLE GATT profile. |
| mtb-example-anycloud-ble-cts-server |
This code example demonstrates the implementation of a simple BLE GAP Central - GATT Server with Current Time Service (CTS) using the Combo (Wi-Fi+BT) SoCs and ModusToolbox™ Software Environment. |
| mtb-example-anycloud-ble-cts-client |
This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP peripheral - GATT client with Current time service (CTS) using the Cypress Combo (Wi-Fi+Bluetooth®) SoCs and ModusToolbox™ Software Environment. |
| mtb-example-anycloud-ota-https |
This code example demonstrates Over-the-Air (OTA) update with PSoC™ 6 MCU and CYW43xxx connectivity devices. |
| mtb-example-anycloud-ble-findme |
This Code Example implements a BLE FMP that consists of an IAS. FMP and IAS are BLE standard Profile and Service respectively, as defined by the Bluetooth SIG. |
| mtb-example-anycloud-ble-wifi-gateway |
This code example demonstrates implementing a Bluetooth IoT gateway using the MQTT client library and Bluetooth LE host stack for Infineon connectivity devices with AIROC™ Wi-Fi & Bluetooth combo chip. |