FLASH USB Programmer New 8FX
综述
General Description
FLASH USB Programmer New 8FX is software which writes data to flash memory from PC. It can also get data from flash memory.
| Tool name | Version | Download | File name |
|---|---|---|---|
| 32bit/64bit OS | V03L03 | (EXE)USBProgrammer-V03L03.zip | flash.exe |
| 32bit OS (Windows XP SP3, Vista, 7) | V03L01 | (EXE)USBProgrammer-32bit-V03L01.zip | flash.exe |
| 64bit OS (Windows 7) | V03L01 | (EXE)USBProgrammer-64bit-V03L01.zip | flash.exe |
- OS:
- 32bit: Microsoft Windows XP Professional with Service Pack 3, Windows Vista, Window
- 64bit: Windows 7 - Memory: 512 MB of system memory or higher recommended
- Download xxx.zip.
- Unzip xxx.zip
- Double-click "flash.exe".
- Respond to the messages displayed and specify the directory in the product to be installed.
支持