| CE# |
Title |
Part# |
Description |
| CE95271 |
Delta Sigma ADC in Differential Mode with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The ADC Differential project contains an example for the use of the ADC_DelSig component in differential mode. The input analog voltage fed to the ADC input terminal is converted to the corresponding digital value and this is displayed on the LCD module. |
| CE95272 |
SAR ADC in Differential Mode using Pre-Amplifier with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates how to sample four different channels with Sequencing ADC, use Opamps to form a Differential preamplifier, and send results to HyperTerminal (PC) using UART. |
| CE95273 |
Delta Sigma ADC in single-ended mode using DMA and VDAC with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example shows the usage of DMA with ADC and VDAC components. The ADC is configured in default single ended mode. The ADC EOC signal is connected to DRQ input of DMA. On each rising edge of EOC signal, ADC output is transferred to VDAC input register. VDAC converts this digital value to analog signal which can be measured using a multimeter. |
| CE95274 |
SAR ADC and PrISM with PSoC™ 5LP |
PSoC™ 5LP |
This datasheet code example demonstrates operation of the ADC_SAR (ADC Successive Approximation Register) and PrISM (Precision Illumination -Signal Modulation) components with the PSoC™ Creator Software. The ADC_SAR measurements are transferred using ISR and DMA to the PrISM and Character LCD components. |
| CE95275 |
Sequencing SAR ADC and Die temperature sensor with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This project demonstrates two channel measurements by the PSoC™ 4 sequencing SAR ADC, transferring results to the LCD and PWM using an ISR. |
| CE95276 |
Sequencing SAR ADC with PSoC™ 5LP |
PSoC™ 5LP |
This datasheet code example demonstrates the operation of the PSoC™ 5LP ADC SAR Sequencer. |
| CE95277 |
Delta Sigma ADC in single-ended mode with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The ADC Single Ended mode code example demonstrates use of the ADC_DelSig component in single ended mode. The input analog voltage fed to the ADC input terminal is converted to the corresponding digital value and this is displayed on the LCD module. |
| CE95278 |
Basic Design project with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
The BasicDesign project contains an example for use with the PSoC™ Creator Help tutorials: "Basic Design" and "Debugging a Design." This project and tutorials provide more details about working with a design, including pins, clocks, and interrupts. They also provide a simple example that can be used with the debugger. |
| CE95279 |
Boost Converter with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates operation of the BoostConv (Boost Converter) -component with the PSoC™ Creator Software. code example demonstrates the usage of the Boost Converter component as a power source for a PSoC™ chip. |
| CE95280 |
Bootloadable Project with PSoC™ 4 |
PSoC™ 4 |
This code example demonstrates the basic operation of the Bootloader and Bootloadable components. This is the bootloadable application project. Refer to the Bootloader_PSoC™4_code example for the bootloader application. |
| CE95281 |
Bootloader Project with PSoC™ 4 |
PSoC™ 4 |
This code example demonstrates the basic operation of the Bootloader and Bootloadable components. This is the bootloader application project. Refer to the Bootloadable_PSoC™4_code example for the bootloadable application. |
| CE95282 |
CAN as Control Node with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
The CANExampleControl code example demonstrates use of the CAN Component. CAN Configuration, transmitting and receiving Full messages, and handling Tx and Rx errors are demonstrated. For additional information on use of the CAN component also refer to the CANExampleRemote project. |
| CE95283 |
CAN as Remove Node with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ |
The CANExampleRemote code example demonstrates use of the CAN Component.CAN Configuration, transmitting and receiving Full messages, handling Tx and Rx error is demonstrated. This is only one part of code example, for getting entire example you should also find CANExampleControl project. |
| CE95284 |
CAPSENSE™ CSD with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This CAPSENSE™_CSD_Design code example demonstrates operation of the CAPSENSE™ CSD component with the PSoC™ Creator Software and DVK hardware. The component is configured with 2 buttons and linear slider. Visual feedback of a Button/Slider touch can be observed via LEDs/LCD. |
| CE95285 |
CAPSENSE™ CSD with PSoC™ 4 |
PSoC™ 4 |
This CAPSENSE™_CSD_P4_Design code example demonstrates operation of the CAPSENSE™ CSD component with the PSoC™ Creator Software and PSoC™ 4 Pioneer Kit (CY8CKIT-042) or PSoC™ 4 S0 Kit (CY8CKIT-040) hardware. The component is configured with a linear slider. Visual feedback of a Slider touch can be observed via LEDs. |
| CE95286 |
CAPSENSE™ CSD using Tuner with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This CAPSENSE™_CSD_P4 Tuner Design code example demonstrates operation of the CAPSENSE™ CSD component with the PSoC™ Creator software, CAPSENSE™ Tuner software and PSoC™ 4 Pioneer Kit hardware (CY8CKIT-042). The component is configured with a linear slider. The CAPSENSE™ Tuner software is used for displaying scanning results. Visual feedback of a Slider touch can be observed via LEDs. |
| CE95287 |
CAPSENSE™ CSD using Tuner with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This CAPSENSE™_CSD Tuner Design code example demonstrates operation of the CAPSENSE™ CSD (Capacitive Sensing using a Delta-Sigma Modulator) component with the PSoC™ Creator Software and CAPSENSE™ Tuner software. The component is configured with 2 buttons and linear slider. The CAPSENSE™ Tuner software is used for displaying scanning results. |
| CE95288 |
CAPSENSE™ Low Power with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4000) |
For PSoC™ 4000 devices only, this code example demonstrates a low power CAPSENSE™ system. Any battery driven equipment requires very low system power consumption, while maintaining the required performance. The PSoC™ 4000 family supports a capacitive touch sensing known as CAPSENSE™ and two device low power modes: Sleep and Deep-Sleep. These low power modes enable PSoC™ 4 to achieve the required performance while operating at very low system power consumption. |
| CE95289 |
CAPSENSE™ Proximity with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4000) |
For PSoC™ 4000 devices only, this project demonstrates a CAPSENSE™ based proximity sensing design to control brightness of a LED. It will help user learn how to design a proximity sensor in their design using a PSoC™ 4 (4000 family) device and see how an approaching hand controls the intensity of a LED. It will employ the CAPSENSE™ auto tuning ability, SmartSense®, to tune the proximity sensor of any wire/trace length. The project will also help user understand and design a simple Sleep-scan routine using the proximity sensor where the device will enter a periodic scan mode at a configurable rate and sleep once the sensor scan is complete to save power. |
| CE95290 |
Char LCD using Custom Font with PSoC™ 4 |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP, |
This code example demonstrates the use of available custom font with the LCD component. |
| |
| PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
| CE95291 |
Char LCD using Horizontal Bar Graph (Hbar) with PSoC™ 4 |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP, |
The CharLCD Hbar design project contains an example for the use of the CharLCD component. A series of horizontal bar graphs are drawn, left to right. Bars move towards the right, becoming shorter and shorter. |
| |
| PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
| CE95292 |
Analog Voltage Comparator with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates use of the Comparator components. |
| CE95293 |
Analog Voltage Comparator with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates the PSoC™ 4 Comparator in Non-Inverting mode. |
| CE95294 |
7-bit Down Counter with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This code example demonstrates functionality of the Count7 component. |
| |
| PSoC™ 5LP |
| CE95295 |
8-bit UDB Counter with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This project contains an example for the use of the Counter, ISR and clock components. A clock is connected to Count input of Counter via a Sync block. On each rising edge of this clock signal, the Counter will be decremented by one count. The Counter is configured to trigger interrupt on terminal count event. This simple example reads the Counter Period, Count and Compare values and displays them on the LCD module. |
| CE95296 |
Cyclic Redundancy Check with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This datasheet code example demonstrates operation of the CRC (Cyclic Redundancy Check) component with the PSoC™ Creator Software. The CRC-16 polynomial, 16 bit resolution and single cycle configuration is demonstrated. |
| |
| PSoC™ 5, PSoC™ 5LP |
| CE95297 |
1.2 Volt Comparator (CSD Comp) using Analog Multiplexer with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4000) |
This code example demonstrates how the comparator's input can be multiplexed using the Amux component. |
| CE95298 |
Switch Debouncer with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This code example shows how to do switch debouncing in hardware using the PSoC™ Creator Debouncer component. |
| |
| PSoC™ 5LP |
| CE95299 |
Delta Sigma ADC using 16 multiplexed single-ended inputs with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates a convenient way to implement a multi-channel ADC completely in PSoC™ hardware |
| CE95300 |
Delta Sigma ADC and I2C Master with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This Starter Design provides an 8-channel multiplexed Delta Sigma ADC with sequencing logic. The analog inputs to the ADC are converted to digital sequentially and then made available through an I2C Master interface. This design additionally makes use of the LCD character display to provide a debugging output interface. |
| CE95301 |
Delta Sigma ADC and I2C Master testbench with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This is the test project for the 8-ch DelSig ADC and I2C master code example |
| CE95302 |
Delta Sigma ADC and I2C Slave with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This Starter Design provides an 8-channel multiplexed Delta Sigma ADC with sequencing logic. The analog inputs to the ADC are converted to digital sequentially and then made available through an I2C Slave interface. This design additionally makes use of the LCD character display to provide a debugging output interface. |
| CE95303 |
Delta Sigma ADC and I2C Slave testbench with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This is the test project for the 8-ch DelSig ADC and I2C Slave Example |
| CE95304 |
Delta Sigma and SPI Master with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This Starter Design provides an 8-channel multiplexed Delta Sigma ADC with sequencing logic. The analog inputs to the ADC are converted to digital sequentially and then made available through a SPI Master interface. This design additionally makes use of the LCD character display to provide a debugging output interface. |
| CE95305 |
Delta Sigma and SPI Master testbench with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This is the test project for the 8-ch DelSig ADC and SPI Master Example |
| CE95306 |
Digital Filter Block Assembler with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates the use of the Digital Filter Block (DFB) Assembler component for matrix multiplication by a scalar. It also demonstrates the DFB interaction with DMA. |
| CE95307 |
Die Temperature sensor with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
The DieTemp basic design project contains an example for the use of Die Temp. This simple example uses a Character LCD to display the current Die Temperature value. |
| CE95308 |
Digital Utility Components with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This project contains an example of the use of some of the Digital Utility components. Using an Edge Detector and a Basic Counter, falling edge events on a pin are counted and driven to a Status Register. Using a Digital Comparator and a Digital Constant, the Basic Counter is reset whenever the count value reaches 100. |
| CE95309 |
Dithered Voltage DAC with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates the basic functionality of the DVDAC component. The Delta Sigma ADC component is used to measure the output voltage. |
| CE95310 |
EEPROM memory with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The EEPROM basic design project contains an example for the use of the EEPROM component. This simple example uses a Character LCD to display data written to EEPROM memory. |
| CE95311 |
Emulated File System with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates emFile component operation |
| CE95312 |
External Memory Interface (EMIF) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This data sheet code example demonstrates operation of the EMIF (External Memory Interface) component with the PSoC™ Creator Software. The Asynchronous External Memory Type, 24 bits Address Width, 8 bits Data Width, 30 ns External Memory Speed configuration is demonstrated. |
| CE195313 |
Emulated EEPROM memory with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4100, |
The code example demonstrates the basic functionality of the Emulated EEPROM component. |
| |
| PSoC™ 4200), PSoC™ 5LP |
| CE95314 |
EZI2C design with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the EZI2C (EZ I2C Slave) and I2C (Inter-Integrated Circuit Master/Multi-Master/Slave) components communication. The EZI2C component is configured as one slave device with the 8 bit sub-address size and 100 kbps data rate. |
| CE95315 |
Auto Firmware Fan Control with Alert with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4200) |
This data sheet code example demonstrates operation of the Fan Controller component in Automatic (Firmware) mode with the PSoC™ Creator Software. |
| CE95316 |
Filter from ADC to VDAC using DFB with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The Filter_ADC_VDAC contains an example for the use of the Filter component. FIR Low pass filter with Blackman window is used to filter the 8-bit ADC output. The filtered output is converted into an unsigned value, then fed via an ISR to VDAC to convert it to analog signal. |
| CE95317 |
Filter from ADC to VDAC using DFB in polling mode with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The Filter_ADC_VDAC_poll contain a polling example for the Filter component. FIR Low pass filter with Blackman window is used to filter the 8-bit ADC output. The filtered output is converted into an unsigned value, then fed via an ISR to VDAC to convert it to analog signal. |
| CE95318 |
Firmware Fan Control with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This project demonstrates the Fan Controller component configured for firmware based Fan Control enabling designers to customize the control algorithm. |
| |
| PSoC™ 5LP |
| CE95319 |
Hardware Glitch Filter with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This code example shows how to do glitch filtering in hardware using the PSoC™ Creator GlitchFilter component. |
| |
| PSoC™ 5LP |
| CE95320 |
Hello World and Blinky LED with 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This project provides an introduction into the process of creating a design in PSoC™ Creator. It accomplishes the simple tasks of printing "Hello World" on an LCD, and blinking an LED using a PWM component. |
| CE95321 |
Hibernate and Stop Power Modes with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates how to enter and wake up from hibernate and stop low power modes, and how to retain SRAM variables in hibernate mode. |
| CE95322 |
Hibernate and Wake Up with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This System Reference Guide code example demonstrates operation of the Power Manager API with the PSoC™ Creator Software. The Hibernate low power mode entry and wake up on external event are implemented. |
| CE95323 |
Hardware Fan Control with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This project demonstrates the Fan Controller component configured for hardware (UDB) based Fan Control. This method completely frees-up the CPU for other system tasks. This example also demonstrates how to handle FanController exceptions such as fan stall/rotor lock etc. through the use of the alert pin and CPU interrupts. |
| CE95324 |
I2C LCD with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstartes functionality of I2C LCD component. |
| CE95325 |
I2C LCD with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstartes functionality of I2C LCD component. |
| CE95326 |
8-Bit Current Digital to Analog Converter (IDAC8) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The IDAC8_Example design project contains an example to demonstrate the use of IDAC8 component. This simple example sets the IDAC range to 255µA and the current value to 100µA. The output can be verified using a Multimeter. |
| CE95327 |
8-Bit Current Digital to Analog Converter (IDAC8) with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstartes basic functionality of PSoC™4 IDAC8. |
| CE95328 |
1kHz ILO Trimming with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates 1kHz ILO trimming for PSoC™3 and PSoC™5LP. |
| CE95329 |
Compensation of ILO Trimming with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates the compensation operation of the ILO Trim component for PSoC™ 4. |
| CE95330 |
Inter-IC Sound Bus (I2S) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the I2S (Inter-IC Sound Bus) component with the PSoC™ Creator Software. The operation of I2S, configuring a DMA transfer and displaying results on LCD screen are described and implemented. |
| CE95331 |
External 8 digit 7-Segment Display with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates driving an external 8 digit 7-segment display |
| CE95332 |
Local Interconnect Network (LIN) Slave with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates the LIN Slave component operation: signal interaction APIs, Transport Layer and Configuration services usage. |
| CE95333 |
Low Power Comparator with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This is code example demonstrates the PSoC™ 4 LP Comparator. |
| CE95334 |
Lookup table (LUT) with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
The LUT Example design project contains an example for the use of the LUT component. This simple example sets the input and output to 2. Output is verified using a Character LCD. |
| |
| PSoC™ 5, PSoC™ 5LP |
| CE95335 |
Management Data Input/Ouput (MDIO) Interface in Advance Mode with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates the advanced mode of the MDIO Interface component by letting the hardware process the frames, and concurrently prints the derived information on the LCD. |
| CE95336 |
Management Data Iinput/Output (MDIO) Interface in Basic Mode with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates the basic mode of the MDIO Interface component by processing the received frame in firmware, and then prints the derived information on the LCD |
| CE95337 |
Analog Signal Mixer with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
The Mixer_SampleProject contains an example for the use of the Mixer component. The mixer type used is Up mixer or Multiply mixer which multiplies the input signal frequency with the local oscillator frequency. The resultant output waveform can be viewed using an oscilloscope. |
| CE95338 |
Multiplexed Analog Comparator with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4200) |
This code example demonstrates how to monitor multiple input signals using multiplexed analog comparator without any CPU intervention. |
| CE95339 |
Operational Amplifier (OpAmp) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example contains an example for the use of the OpAmp component in Non-inverting Mode. |
| CE95340 |
Amplifier with Dynamic Gain Switching with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4200) |
This code example demonstrates how to multiplex three different channels with ADC using Analog Mux and send results to HyperTerminal (PC) using UART. The ADC input and gain can be changed on the fly by pressing a switch. |
| CE95341 |
Operational Amplifier (OpAmp) with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This is code example demonstrates the functionality of the PSoC™ 4 OpAmp. |
| CE95342 |
Programmable Gain Amplifier (PGA) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This design project contains an example for the use of the PGA component. This simple example sets the PGA gain to 1 and outputs a Voltage set in the firmware to a fixed pin. This voltage can be verified using a Multimeter. |
| CE95343 |
Inverting Programmable Gain Amplifier with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This design project contains an example for the use of the PGA_Inv component. This simple example sets the PGA_Inv gain to 1 and outputs a Voltage set in the firmware to a fixed pin. This voltage can be verified using a Multimeter. |
| CE95344 |
PMBus Slave in Power Supervision Application with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates usage of the PMBus Slave component in a simulated Power Supervision application. |
| CE95345 |
PMBus Slave in Thermal Management Application with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates usage of the PMBus Slave component in a simulated Thermal Management application. |
| CE95346 |
Power Management and Hibernate with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This System Reference Guide code example demonstrates operation of the Power Manager API with the PSoC™ Creator Software. The Hibernate low power mode entry and wake up on external event are implemented. |
| CE95347 |
Power Monitoring with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This project demonstrates the PowerMonitor component configured for using with 035-Power Management EBK development kit. |
| CE95348 |
Precise Illumination Signal Modulation (PrISM) with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This datasheet code example demonstrates operation of the PrISM component with the PSoC™ Creator Software. The LED blinking is demonstrated. |
| |
| PSoC™ 5, PSoC™ 5LP |
| CE95349 |
Pseudo Random Sequence (PRS) generator with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This datasheet code example demonstrates operation of the PRS (Pseudo Random Sequence) component with the PSoC™ Creator Software. The clocked and API Single Step run modes, 16 bit resolution and single cycles implementation configuration is demonstrated. |
| |
| PSoC™ 5, PSoC™ 5LP |
| CE95350 |
Pulse Counter with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This project contains an example of the use of the Pulse Converter component. 2 Basic Counter components, clocked slower than BUS_CLK, count the number of DMA nrq pulses. One uses the nrq output directly, so it misses pulses. The other uses a Pulse Converter component to guarantee that it does not miss pulses. |
| CE95351 |
Fixed Function PWM with PSoC™ 4 |
PSoC™ 4 |
This data sheet code example demonstrates operation of the TCPWM (PWM Mode) component with the PSoC™ Creator Software. |
| CE95352 |
Fixed Function PWM with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates operation of the PWM Fixed Function component. This simple example uses a Character LCD to display the current PWM Period, Compare values and status of PWM output on the LCD module. |
| CE95353 |
Quadrature Decoder with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the QuadDec (Quadrature Decoder) component with the PSoC™ Creator Software. The quadrature counts handling and index input usage is demonstrated. |
| CE95354 |
Quadrature Decoder with PSoC™ 4 |
PSoC™ 4 |
This data sheet code example demonstrates operation of the TCPWM (Quadrature Decoder Mode) component with the PSoC™ Creator Software. |
| CE95355 |
Real Time Clock (RTC) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates operation of the RTC (Real Time Clock) component with the PSoC™ Creator Software. The operation with full time, data and alarm features, including Daylight Savings Time (DST) is -implemented. |
| CE95356 |
Resistance Temperature Detector (RTD) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This data sheet code example demonstrates operation of the RTD (resistance temperature detector) calculator component with the PSoC™ Creator Software. The PT100 RTD type, [-50, 150] Temperature Range, minimal calculation error budget, IEC60751 Coefficients is demonstrated. |
| CE95357 |
Sample and Hold with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates operation of the Sample/Track and Hold component in Sample and Hold mode. This simple example uses a Character LCD to display the Sample and Hold value which is converted using an ADC. |
| CE95358 |
SAR sampling with SPI and USBUART communication with PSoC™ 5LP |
PSoC™ 5, PSoC™ 5LP |
This Starter Design provides two 4-channel SAR ADCs with two analog muxes to choose input channels. The channel to be read is dictated by the USB host device. The ADC then processes the input and then outputs it to a SPI Slave and to the USB host. This design will additionally make use of the LCD character display to provide a debugging output interface. |
| CE95359 |
SAR sampling with SPI and USBUART communication testbench with PSoC™ 5LP |
PSoC™ 5, PSoC™ 5LP |
This is the test project for the 4ch dual SAR with SPI master and USBUART code example |
| CE95360 |
Scanning Comparator using common mode with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
This data sheet code example demonstrates operation of the Scanning Comparator (Common Mode) component with the PSoC™ Creator Software. |
| |
| PSoC™ 5LP |
| CE95361 |
Scanning Comparator using Internal VDAC with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This data sheet code example demonstrates operation of the Scanning Comparator (Internal VDAC Per channel Mode) component with the PSoC™ Creator Software. |
| CE95362 |
EzI2C communication using a Serial Communication Block (SCB) with PSoC™ 4 |
PSoC™ 4 |
This code example demonstrates the basic operation of the EZI2C slave (SCB mode) component. The EZI2C slave accepts packet with command from I2C master to control RGB LED color. The EZI2C slave updates its buffer with status packet in response to the accepted -command. |
| CE95363 |
I2C Master using a Serial Communication Block (SCB) with PSoC™ 4 |
PSoC™ 4 |
This code example demonstrates the basic operation of the I2C master (SCB mode) component. I2C master sends packet with command to I2C slave to control RGB LED color. The packet with status is read back. |
| CE95364 |
I2C Slave using a Serial Communication Block (SCB) with PSoC™ 4 |
PSoC™ 4 |
This code example demonstrates the basic operation of the I2C slave (SCB mode) component. The I2C slave accepts packet with command from I2C master to control RGB LED color. The I2C slave updates its buffer with status packet in response to the accepted command. |
| CE95365 |
SPI Transmit and Receive using a Serial Communication Block (SCB) with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This datasheet code example demonstrates operation of the SCB component configured in SPI. The first instance of SCB is configued as SPI master and the second as SPI Slave mode. The SPI master communicates with slave (bit rate 1Mbps). |
| CE95366 |
UART Transmit and Receivce using a Serial Communication Block (SCB) with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This datasheet code example demonstrates operation of the SCB component configured in UART Tx+Rx mode. Data typed on the HyperTerminal is sent through serial port to the DVK and displayed on the LCD.After that this data is sent back and displayed on the HyperTerminal. |
| CE95367 |
Segment LCD with PSoC™ 5 |
PSoC™ 5 |
This code example demonstrates the Segment Display component operation in Always Active mode. In this code example, Bar graph, 7 Segment and 14 Segment helpers handle data processing and proper pixel reflection output on the LCD's Bar graph, 7 segments or 14 Segment digits. |
| CE95368 |
Segment LCD in Low Power mode with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
The SegLCD Low Power design project contains an example for the use of the Segment LCD component. This example features the Segment LCD in Low Power (ILO) mode at a 62Hz refresh rate. It displays 14 Segment helper. |
| CE95369 |
Segment LCD with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates the PSoC™ 4 Segment LCD. |
| CE95370 |
My first PSoC™ Creator Component Library with PSoC™ 3 |
PSoC™ 3 |
The My1stLib project contains an example of a library project for use with the PSoC™ Creator Help tutorial "Library Component Project." This project and tutorial provide an introduction into the process of creating simple shifter components. Add this project to the Shifter code example Workspace and add the dependency to the Shifter to generate the correct code example. |
| CE95371 |
Using custom components in a Hierarchical Design with PSoC™ 3 |
PSoC™ 3 |
The Shifter project contains an code example for use with the PSoC™ Creator tutorial: "Basic Hierarchical Design." This project and tutorial demonstrate how to re-use components created in the "Library Component Project" tutorial to create a simple hierarchical design. This project requires the My1stLib project be located in the same root directory. |
| CE95372 |
Shift register with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the ShiftReg (Shift Register) component with the PSoC™ Creator Software. The basic functionality of 8-bit and 16-bit shift register is demonstrated. |
| CE95373 |
Waking up from Low Power modes with the Sleep Timer with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the Sleep Timer component with the PSoC™ Creator Software. The wake up from Sleep low power mode every 4 milliseconds with interrupt issuing is implemented. The Power Management API is used for proper low power mode entry. |
| CE95374 |
S/PDIF Transmitter with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the S/PDIF Transmitter (SPDIF_Tx) component with the PSoC™® Creator™ Software. The operation of the SPDIF_Tx and configuring a DMA transfer for this component are described and implemented. |
| CE95375 |
SPI Master and DMA with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates the operation of the SPI(Serial Peripheral Interface) Master component with the PSoC™ Creator Software. The operation of the SPI Master, configuring a DMA transfer and displaying results on an LCD screen are described and implemented. This example is intended to be used with the SPIS_code example. |
| CE95376 |
SPI Slave and DMA with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates operation of the SPI(Serial Peripheral Interface) Slave component with the PSoC™ Creator Software. The operation of the SPI Master, configuring a DMA transfer and displaying results on LCD screen are described and implemented. This example is intended to be used with the SPIM_code example |
| CE95377 |
SPI Master and Slave with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This datasheet code example demonstrates operation of the SPI (Serial Peripheral Interface) component with the PSoC™ Creator Software. The communication between SPI Master and SPI Slave is implemented. The SPI Mode 0 (CPOL = 0, CPHA = 0) with 8 byte Rx and Tx software buffers is configured. The bit rate is set to 1 Mbps. |
| CE95378 |
Static Segment LCD and Sleep with PSoC™ PSoC™ 3 |
PSoC™ 3 |
The SegLCD Low Power design project contains an example for the use of the Static Segment LCD in Sleep mode. It shows operation of 7 Segment helper. |
| CE95379 |
Software based UART transmit with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4100, |
This code example demonstrates basic functionality of Software Transmit UART component. |
| |
| PSoC™ 4200), PSoC™ 5LP |
| CE95380 |
TCPWM configuration with PSoC™ 4 |
PSoC™ 4 |
This data sheet code example demonstrates operation of the TCPWM (Unconfigured TCPWM Mode) component with the PSoC™ Creator Software. |
| CE95381 |
Thermistor temperature calculation with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This code example demonstrates the use of the Thermistor Calculator component for temperature measurement. |
| CE95382 |
Thermocouple with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This data sheet code example demonstrates operation of the Thermocouple calculator component with the PSoC™ Creator Software. The K-type thermocouple type, 0.1 Calculation error budget is demonstrated. |
| CE95383 |
Transimpedance Amplifier (TIA) with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This design project contains an example for the use of the TIA component. |
| CE95384 |
16 bit UDB based timer with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This design project contains an example for the use of the Timer, ISR and clock components. The 16-bit UDB timer counts down on the positive edge of each clock, and captures the count value for the rising edge of a slower clock given as input. An interrupt is triggered on every terminal count, and the number of interrupts generated is displayed on the Character LCD. In addition, this simple example reads the timer Period, Capture, and Counter values and displays them on the LCD module. |
| CE95385 |
TCPWM Timer/Counter Operation with PSoC™ 4 |
PSoC™ 4 |
This data sheet code example demonstrates operation of the TCPWM (Timer / Counter Mode) component with the PSoC™ Creator Software. |
| CE95386 |
TMP05 temperature sensor interface with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4(PSoC™ 4200, |
This data sheet code example demonstrates operation of theTMP05 Temp Sensor Interface component with the PSoC™ Creator Software. The continuous mode is demonstrated. |
| |
| PSoC™ 5, PSoC™ 5LP) |
| CE95387 |
Trim voltage rails with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates the basic operation of the Trim Margin component |
| CE95388 |
UART Receive with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
The UART Rx design project contains an example for the use of the UART component. This example demonstrates the UART Reception (Rx) mechanism. Data input via Hyperterminal is sent through the serial port and displayed on the LCD module. |
| |
| PSoC™ 5, PSoC™ 5LP |
| CE95389 |
UART Transmit with PSoC™ 3/4/5LP |
PSoC™ 3, PSoC™ 4 (PSoC™ 4200), |
The UART Tx design project contains an example for the use of the UART component. This example demonstrates the UART Transmission (Tx) -mechanism. Data sent via the serial port is displayed on Hyperterminal and the LCD module. |
| |
| PSoC™ 5, PSoC™ 5LP |
| CE95390 |
USB Audio with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the 8-bit, 32-kHz, mono USB Audio Device. |
| CE95391 |
USB Bootloadable Application with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the Bootloadable component. Add this project to the USBFS_Bootloader code example Workspace and add Dependency to the USBFS_Bootloader to generate the correct code example. |
| CE95392 |
USB Bootloader with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the Bootloader with USBFS as an I/O component. |
| CE95393 |
USB Bulk Transfer with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the USBFS (Full Speed USB) component with the PSoC™ Creator software. It also shows the Bulk transfers implementation. |
| CE95394 |
USB HID Mouse with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the USBFS (Full Speed USB) component with the PSoC™ Creator software. It also shows the USB mouse implementation. |
| CE95395 |
USB MIDI with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the MIDI interface device operation. |
| CE95396 |
USB UART with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the USBFS component as an RS-232 logical cable replacement. |
| CE95397 |
Voltage DAC with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5, PSoC™ 5LP |
This design project contains an example for the use of the VDAC component. This simple example sets the VDAC range to 1.020V and outputs a Voltage set in the firmware to a fixed pin. This voltage can be verified using a Multimeter. |
| CE95398 |
Voltage Fault Detector with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This datasheet code example demonstrates the operation of the Voltage Fault Detector. |
| CE95399 |
Voltage Sequencer and power rail monitoring with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates the basic operation of the Voltage Sequencer component. |
| CE95400 |
Watchdog timer interrupts and device reset for CY8CKIT-040 with PSoC™ 4000 |
PSoC™ 4 (PSoC™ 4000) |
This code example demonstrates the basic operation of the WDT: device reset and periodic interrupt generation. |
| CE95401 |
Watchdog timer example using LCD with PSoC™ 4 |
PSoC™ 4 (PSoC™ 4100, PSoC™ 4200) |
This code example demonstrates basic functionality of PSoC™4 watchdog. |
| CE95402 |
Generating a Sine wave with the WaveDAC8 Component with PSoC™ 3/5LP |
PSoC™ 3, PSoC™ 5LP |
This code example demonstrates basic functionality of WaveDAC8 component. |