功率高达150kW的充电设备
用可扩展的直流充电,填补住宅和高速公路充电之间的空白
如今,电动汽车(EV)的车主不再仅限于城市居民或短途通勤人员。正因如此,电动汽车的充电也不再局限于住宅或办公室。尽管高达350kW的大功率直流充电器给高速公路带来了快速充电的机会,但其实在城市中,150kW的充电器才是日常会用到的理想解决方案,它填补了住宅和高速公路充电之间的空白。
考虑到150kW电动汽车快速充电器的模块化设计及其可扩展选项,它正成为城市地区和商业应用的首选。一个50kW的充电模块可实现充电48分钟左右,续航200公里,而如果通过并联三个这种50kW的充电模块或5个30kW的充电模块,使之成为一个150kW的充电设备的话,则可在大约16分钟里,经济高效地进行相同续航里程的充电。尽管不论哪种并联选项,16分钟对于稍事休息的司机而言都太久了,但这刚好够他们来购买一些杂物或用餐,同时能够便捷地完成充电。
英飞凌150kW充电解决方案
在设计150 kW的大功率直流充电设备时,需要考虑很多因素——从安全数据和通信,到可靠性、效率和价格。对此,英飞凌提供了市面上最为全面的产品组合。借助我们的系统解决方案组合,您将能使用适合您的具体情况的最佳产品和技术、获得最高性价比,同时从我们专家丰富的系统能力上获益。这其中包括我们的600 V CoolMOS™ SJ MOSFET P7和CFD7系列、我们的650 V TRENCHSTOP™ IGBT7 T7系列和我们的1200 V CoolSiC™ MOSFET。我们的高压开关产品组合配有650V和1200 V CoolSiC™肖特基二极管。由于每个开关都需要一个驱动器,每个驱动器都需要受到控制,因此我们还针对电动汽车充电设备的设计,推出了适用的EiceDRIVER™以及XMC™和AURIX™微控制器。OPTIGA™产品对此进行了完善,确保数据得到保护以及数据安全。
凭借丰富的高质量分立解决方案组合,英飞凌可为您提供合适的电气元器件,助您打造高效、更具性价比的电动汽车充电设备设计。简而言之,英飞凌是唯一一家电动汽车快速直流充电的一站式供应商,可帮助您实现更高的效率和更高的功率密度。
技术趋势
额定功率在30 kW-150 kW之间的电动汽车充电系统通常依赖于两级电源转换结构,即电网侧的AC-DC电源转换级和电池侧的隔离高频DC-DC电源转换级。它将15 kW到30 kW的基本充电模块并联起来,以提供高达150 kW的功率。这些低功耗充电模块为系统增加了功能方面的模块化性能,从而实现了采用分立功率器件的变流器设计,十分经济高效。您可在此探索150 kW电动汽车充电设备的系统图:
系统图:高达150 kW的电动汽车直流充电器设备
拓扑结构和电源转换
在AC-DC转换级,AC-DC转换系统在EMI滤波器之后,发挥着受控整流器的作用。在这个级别,首选二级有源前端(AFE) 或三级Vienna整流器拓扑。这两种拓扑结构都能够根据充电器的额定功率,确保稳定的直流链路电压(最高可达900V)。特别是Vienna整流器,它以其更高的效率和更柔和的EMI特征,而被广泛使用。此外,它还支持使用600V功率器件。得益于1200 V CoolSiC™ 等元器件,具有功率因数校正(PFC)拓扑结构的二级有源前端变得越来越受欢迎,其双向操作的特点更是使之独具魅力。
在DC-DC转换级,分为两个系统:在隔离变压器初级侧,从DC电压转换为高频AC电压;在次级侧,从高频AC转换为DC电压整流。适用的拓扑结构通常为谐振式、硬开关全桥式、移相式、ZVS、全桥转换器。具有单桥(1200 V SiC)或级联桥(600 V)的谐振LLC转换器拓扑结构被广泛应用于该电源转换级。
参数化产品查找器
网络研讨会:英飞凌 CoolSiC™ 助力实现电动汽车直流快充
随着电动汽车逐渐融入人们的日常生活,对高效充电解决方案的需求也在不断增长。纵览该领域的要求和技术发展,其挑战在于为当下和未来的充电网络提供紧凑型智能电源转换解决方案。在本次网络研讨会中,您将深入了解一系列英飞凌电动汽车直流充电产品,会议将重点介绍碳化硅器件及其在电动汽车超级快充中发挥的重要作用。
工程师播客 #1:蓬勃发展中的电动汽车充电
新播客系列第一集将直切主题,介绍电动汽车相关内容:具体而言即有哪些场合可供充电?这对相应的拓扑结构意味着什么?设计人员如何应对此类问题?我司专家将负责解答,并针对电动汽车的发展开端提出有趣见解。
In this video, you will:
- Understand what Battery Electric Vehicle charging is
- Recognize the three different charging categories available
- Know how these categories can be implemented
With the growing market of electrical vehicles, the industry has put forward more requirements for the performance of charging piles. This e-learning will show you that the emergence of CoolSiC™ MOSFETs has improved the charging pile industry to make the EV charger smaller, faster and with higher efficiency.
In this video, you will:
- Understand how Infineon’s power semiconductor module portfolio is a solution for the main challenges of the electric vehicle industry
- Know Infineon’s general value drivers as well as recent success stories on the electromobility market
Do you want to know the various topologies you can find in this power conversion stage and their top level working principle? Get to know the basic concepts of passive and two-level active rectification methods.
Training topics:
- Get to know how AURIXTM is able to answer the needs of the electric vehicle market
- Recognize and explore how AURIX™ TC3xx addresses key electric vehicle challenges, and understand the main features of the AURIX™ TC3xx microcontroller