英飞凌再度引领业界潮流,推出支持IP电话的低成本手机平台
2008年3月17日,德国Neubiberg讯——三年来,英飞凌销售的低成本手机芯片已经让全球不计其数的用户第一次用上了手机。这些小小的创新芯片集成了手机的所有主要功能。到2007年年底,该 芯片的销售量已逾5,000万,支持世界各地的用户在GSM移动网络上拨打电话。问题是,不同国家的不同运营商收取的电话费大相径庭。如今,基于互联网的电话(VoIP)业务收费便宜得多。然而,迄今为止,只 有被称为智能手机的高端手机才实现了可支持这个应用的尖端技术。通过与美国无线及有线宽带技术专家Atheros公司合作,英飞凌研发了第一个允许用户同时使用GSM移动网络和VoIP业务的芯片平台。英 飞凌提供的低成本芯片负责执行所有的GSM电话功能,而Atheros公司的芯片则负责在接入无线局域网(WiFi热点)时处理数据包,以支持基于互联网的语音或数据业务。此外,用户可以使用物美价廉的包月服务。
英飞凌通信解决方案业务集团负责销售和大客户市场营销的高级副总裁Dominik Bilo表示,“我们的GSP芯片与Atheros公司的无线局域网芯片的组合,可 以让更多的人有机会享用廉价的通信服务。在可以预见的未来,有线宽带网络还不能在诸如印度、中国和部分南美地区等新兴国家实现全面覆盖。相比之下,可以相对较快的速度和较低的成本,在 小乡村建设无线局域网和几个热点或无线IP小区。这样,就能让数十亿人步入无限自由通信的世界。”
独立的市场调查公司认为,面向手机的GSM与VoIP集成式解决方案具有巨大的增长空间。预计仅今年就将售出约1.86亿部双模GSM/Wi-Fi手机,到2010年销售量将增至2.5亿部。
这个GSM/VoIP手机解决方案采用了英飞凌X-GOLD™101 单芯片。这颗只有8平方毫米的小小芯片将语音处理、射频管理、电源管理、内存等等手机的所有核心功能集于一身。此外,该 解决方案还采用了Atheros公司的ROCm™芯片(移动射频芯片)。这颗10平方毫米的芯片也经专门优化,可以提供最强大的功能,同时最大限度地的降低功耗。相比于常规解决方案,A theros芯片将实现创新无线VoIP通信功能所需的器件数量减少了一半。
在2008年3月17日至20日在圣何塞举办的VON.x展会上,英飞凌推出的最新移动通信平台将首次揭开神秘面纱。第一批产品最早将于今年第二季度上市。
关于基于互联网的电话业务的更多信息,请参阅英飞凌指南《关于基于IP的语音业务的7大谬误》(网址:www.infineon.com/presse/VoIP)
Independent market researchers see significant growth opportunities for the combination of GSM and VoIP technology in mobile phones. Some 186 million units are slated to be sold this year alone, and forecasts put the figure for 2010 at 250 million units.
Infineon's contribution to the new GSM/VoIP phones is its X-GOLD™101 single chip, which packs the core functions of a mobile phone – voice processing, radio frequency management, power management, memory and so one – into a footprint of just 8 mm x 8 mm. Atheros adds its 10 mm x 10 mm ROCm™ (radio-on-chip for mobile) chip. This chip too is optimized to deliver maximum functionality while minimizing power consumption. Compared to conventional solutions, Atheros halves the number of components needed for innovative wireless VoIP communication.
Infineon will be taking the wraps off its new mobile communication platform at the VON.x trade show in San Jose (March 17-20, 2008). Initial products will be available to customers as early as the second quarter of this year.
For more information about Internet-based telephony, please refer to our guidebook "The 7 Voice over IP Myths" at www.infineon.com/press/VoIP
About Infineon
总部位于德国Neubiberg的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、连通性和安全性提供半导体和系统解决方案。2007财年(截止到9月份),公司实现销售额77亿欧元( 包括奇梦达的销售额36亿欧元),在全球拥有约43,000名雇员(其中奇梦达雇员约13,500人)。英飞凌科技公司的业务遍及全球,在美国圣何塞、亚太地区的新加坡和日本东京等地拥有分支机构。英 飞凌公司已列入法兰克福股票交易所的DAX指数,并在纽约股票交易所挂牌上市,股票代号:IFX
如欲了解更多信息,敬请登 www.infineon.com
该新闻稿可从以下网站找到: http://www.infineon.com/press
Information Number
INFXX200803-051
Press Photos
-
Combining GSM and VoIP technology in a low-cost mobile plattform will increase coverage and decrease cost per call. A perfect win-win situation created by Infineon and Atheros.Mobile_Over_IPJPG | 956 kb | 1535 x 1063 px