XMC1400微控制器助力实现成本敏感的实时电源控制;相比XMC1000原有产品系列在性能和连接性方面得以增强

2016-2-23 | 市场新闻

德国慕尼黑和纽伦堡讯— XMC1400微控制器将助力英飞凌科技股份公司在工业自动化、数字电源转换和电子控制领域开辟诸多全新应用。相比早先推出的 XMC1000 产品而言,全新XMC1400系列能实现更出色的控制性能和更好的连接性。XMC1400采用ARM® Cortex®-M0处理器,具备针对目标应用精心定制的全面外设功能。目标应用包括:工业自动化领域的执行器,用于控制LED灯和多相电机的数字电源转换,以及对割草机、锯齿机或发电机等配备的小型内燃机进行电子控制。

 

较之早期XMC1000微控制器,XMC1400产品拥有更好的连接性,并具备强大的处理能力,因此可实现更精确的控制。其时钟周期为48MHz,而XMC1000系列的时钟周期为32MHz。在XMC1400中,PWM定时器和AD转换器等控制器外设的重要元件也能以倍频运行,即96MHz。XMC1400还能实时进行三角函数计算和除法运算,这在基于Cortex M0的产品中独具特色。集成式MATH协同处理器与Cortex-M0 CPU并行工作,可以增加实时运算能力。

 

功能强大的XMC1400微控制器系列产品具有四个CCU定时器模块(两个CCU4和两个CCU8模块),因而有多达16个独立的定时器,譬如,可以用于实时产生PWM。这样,在未来价格敏感的小型内燃机市场上,其可以满足对点火、油门和喷油泵进行电子调节与控制的特殊要求。为控制电机,XMC1400配有两个接口,用于连接霍尔传感器或光学编码器。

 

另外,XMC1400还具有一个BCCU外设单元(亮度和颜色控制单元),实现对LED的无闪烁数字调光和颜色控制。这样就可以设计多通道LED开关模式电源,可调节彩色LED,模拟太阳光的光谱(可调白光)。XMC1400具有多达四个比较器,用于调节开关电源。早先的XMC1000微控制器最多只有三个比较器。

 

加强面向自动化技术的连接是实现工业 4.0 的基础

工业4.0需要分散的联网智能。在需要有众多传感器和执行器进行联网的任何应用中,XMC1400不仅可提供所需的实时控制性能,而且还能带来必要接口。另外,XMC1400也能确保不太复杂的解决方案能具有合理的系统成本。所有的XMC1400 型号都配有标准通信接口,如UART、I 2C、SPI和I 2S。XMC1403和XMC1404微控制器还具有两个CAN节点。CAN(控制器局域网)是自动化技术领域最常用的总线标准之一。

 

就像XMC1000微控制器一样,英飞凌还提供XMC1400的客户专用版本,其中,安全引导程序和适当的工具链能以加密形式将固件安全地加载到闪存。

 

XMC1400 供货情况

对于XMC1400系列的产品,以及小评估板或启动包,所有封装版本均有样品提供。采用LQFP-64封装的XMC1400现已开始批量生产。至于其它产品,计划于2016年第二季度开始初期批量生产。XMC1400产品各版本具有不同的参数,如内存大小(32至200 KB闪存)、PWM定时器(8或16)和CAN节点(2或无)。封装版本包括VQFN-40(与XMC1300引脚兼容)、VQFN-48、VQFN-64和LQFP-64。XMC1400系列由免费的  DAVE ™开发环境提供支持。

Press Photos

  • The XMC1400 microcontrollers offer greater control performance and additional connectivity than the earlier XMC1000 products. Target applications are actuators in industrial automation, digital power conversion for the control of LED lamps and multiphase electric motors, and the electronic control of small combustion engines such as those in lawnmowers, chainsaws, or generators.
    The XMC1400 microcontrollers offer greater control performance and additional connectivity than the earlier XMC1000 products. Target applications are actuators in industrial automation, digital power conversion for the control of LED lamps and multiphase electric motors, and the electronic control of small combustion engines such as those in lawnmowers, chainsaws, or generators.
    XMC1400

    JPG | 954 kb | 2126 x 1535 px