英飞凌加固型TRENCHSTOP™ 5 S5 IGBT延长光伏逆变器和不间断电源工作寿命,提高其能源效率

2015-11-12 | 市场新闻

德国慕尼黑讯——英飞凌科技股份公司推出全新S5系列,进一步增强其IGBT的性能。全新推出的这个产品系列立足于超薄晶圆TRENCHSTOP™ 5 IGBT,专门针对开关频率高达40kHz的工业设备的交流-直流电力转换装置而开发。这类工业设备主要包括光伏逆变器(PV)和不间断电源(UPS)。S5系列器件能够满足制造商实现不低于98%的系统效率级别,从而最大限度提高太阳能电池板的发电量,同时降低系统成本的需求。新产品系列更加坚固耐用,质量更高,可帮助最终用户将设备寿命延长至20年。总体而言,新推出的IGBT产品系列可以提高客户产品的能效,提高其价格竞争力和耐用性。

 

新推出的IGBT器件能够提高系统的开关性能,降低电路设计的复杂度,此外由于无需加装电容器和齐纳二极管,它还可以降低系统成本。通常,为了达到最高的能效和耐用性需要加装电容器和齐纳二极管,但采用TRENCHSTOP 5 S5无需加装它们。此外,新器件的浪涌电流处理能力提高了25%,可进一步提高器件的耐用性和质量水平,让客户对自身设计的坚固性更有信心。在175 °C的温度下,新推出的器件的典型饱和电压V CE(sat) 仅为1.60 V,创行业新低。因此,即便在高温工作条件下,新器件也能保持较高的能效。

 

供货情况

 

首批推出的全新IGBT型号的电流级别分别为30A、40A、50A和75A,采用三管脚TO-247封装,混装Rapid1续流二极管。关于TRENCHSTOP 5 S5产品系列的更多信息,可在 www.infineon.com/trenchstop5上找到。

Press Photos

  • The new TRENCHSTOP 5 S5 family has been developed specifically for AC-DC energy conversion in industrial applications switching up to 40 kHz, typically to be found in Photovoltaic Inverters (PV) or Uninterruptible Power Supplies (UPS). The Discrete IGBT features an industry leading low typical saturation voltage VCE(sat) of 1.60 V at 175 °C.
    The new TRENCHSTOP 5 S5 family has been developed specifically for AC-DC energy conversion in industrial applications switching up to 40 kHz, typically to be found in Photovoltaic Inverters (PV) or Uninterruptible Power Supplies (UPS). The Discrete IGBT features an industry leading low typical saturation voltage VCE(sat) of 1.60 V at 175 °C.
    TO-247-650V-S5

    JPEG | 429 kb | 1298 x 1772 px