英飞凌推出全球最小的用于两轮和三轮的引擎管理IC;TLE808x 功率接口解决方案可满足降低油耗和排放的新要求,并可节省占板空间

2012-10-18 | 市场新闻

2012年10月18日,德国纽必堡讯——英飞凌科技股份公司(FSE: IFX / OTCQX: IFNNY)今天推出全球最小的引擎管理IC,与现有的解决方案相比,可 在两轮和三轮控制系统中节省高达三分之二的占板空间。全新的TLE808x系列器件具有单缸内燃机先进的电喷(EFI)系统所要求的全部功能。

TLE808x系列专门用于降低四冲程小型内燃机的排放和油耗,这种内燃机被广泛用于摩托车、踏板车、三轮车、草坪拖拉机、割草机、小型汽油发动机、水上运载工具、水上摩托车和雪地车。

目前, TLE808x系列包括两款量产器件:TLE8088和具有可变磁阻传感器(VRS)接口和增强功能的TLE8080。

在亚洲、非洲和南美洲等许多发展迅猛的国家,摩托车是最受欢迎并且较为经济的交通工具。然而,在全球变暖效应方面,传统的化油器摩托车比普通汽车的影响更大。为 了满足日趋严格的摩托车排放和油耗法规要求,必须针对小型内燃机推出高度集成、经济高效的电喷系统。来自英飞凌的全新TLE808x引擎管理解决方案为此提供鼎力支持。

TLE8080将系统微控制器与外设传感器连接在一起,进行信号处理并驱动小型内燃机所需的执行器。

它包含一个为微控制器供电所需的稳压器。这款5V稳压器可提供高达250mA的电流,并具有欠压复位、上电复位和监控电路功能。

此外, TLE8080具有连接可变磁阻传感器(VRS)的接口,VRS可测量引擎的转速(RPM)。这款接口IC可将具有噪音的传感器输出信号调节至微控制器所需的逻辑输入水平。通过SPI,可 对两个继电器驱动器和故障指示灯以及VRS接口进行控制。两个额外的带有直接输入引脚的低边开关也被包含在内,支持喷油嘴、节流阀或类似感性负载的电磁阀。TLE8080是市场上具有丰富特性集的最小型产品。

供货和封装
TLE808x器件批量供应。它们采用节省空间的24引脚收缩型小外形封装(SSOP)。

更多信息
英飞凌产品组合涵盖创建电控内燃机所需的所有电子元件: XC2700系列16位微控制器或XC800A系列8位微控制器系统、压力传感器(如KP254)和步进式电机驱动IC( 如TLE8444)。如欲了解更多信息,敬请访问: www.infineon.com/motorcycle。
更多关于TLE808x系列的详细技术信息,包括在线学习材料,敬请访问 www.infineon.com/motorcycle

About Infineon

总部位于德国纽必堡的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、交通和安全性提供半导体和系统解决方案。2011财年(截止到9月30日),公司实现销售额40亿欧元,在 全球拥有约26,000名雇员。英飞凌公司目前在法兰克福股票交易所(股票代码:IFX)和美国柜台交易市场(OTCQX)International Premier(股票代号:IFNNY)挂牌上市。

更多信息请访问 www.infineon.com
本新闻稿请访问 www.infineon.com/press

Information Number

INFATV201210.007

Press Photos

  • The engine management ICs of the TLE808x family save up to two-thirds of board space in control systems for two- and three-wheelers compared to today's solutions. They provide all the functionality required for state-of-the-art electronic fuel injection (EFI) in one-cylinder combustion engines.
    The engine management ICs of the TLE808x family save up to two-thirds of board space in control systems for two- and three-wheelers compared to today's solutions. They provide all the functionality required for state-of-the-art electronic fuel injection (EFI) in one-cylinder combustion engines.
    TLE8080-8088

    JPG | 2.45 mb | 2126 x 1535 px

  • Infineon covers all required electronics for setting up an electronically controlled combustion engine.
    Infineon covers all required electronics for setting up an electronically controlled combustion engine.
    TLE8080_System_diagram

    JPG | 1.35 mb | 2362 x 2362 px