英飞凌推出全球最小的低功耗全集成式GPS接收前端模块,进一步提高GPS系统灵敏度

2010-2-2 | 市场新闻

2010年2月2日,德国Neubiberg讯——为满足不断发展的移动GPS市场对更高灵敏度、更高抗扰性和更低功耗的要求,英飞凌科技股份公司(FSE:IFX / OTCQX: IFNNY)今 日推出全球最小的新一代GPS接收前端模块。全新的BGM781N11可进一步提高GPS灵敏度,使手机、个人导航设备和其他手持系统及车载GPS应用能满足E911紧急呼叫定位要求。该 模块包含放大GPS信号和滤除干扰信号的所有主要组件,其尺寸仅为2.5mm x 2.5mm x 0.7mm,比具有类似集成度的最接近的竞争性产品小60%以上。

BGM781N11 GPS接收前端模块在一个小型无管脚TSNP11-2封装内,集成一个GPS低噪放大器(LNA)和两个具备出色ESD防护功能的表面声波(SAW)滤波器。有 了BGM781N11,GPS应用只需两个外置无源组件,而竞争性解决方案通常需要6至10个无源组件。由于新一代高端手机的功能不断增加,PCB空间逐渐成为主要的限制因素,因此尺寸较小、无 需太多额外组件的前端模块备受欢迎。此外,BGM781N11具备极低的功耗,仅为5.94 mW,电压范围在1.5V至3.6V之间。

为了最大限度减少便携式电子产品的ESD损坏,BGM781N11具备极强的ESD防护性能。射频输入引脚具有8kV的ESD接触放电防护功能,这使得GPS设备厂商无需采用其他ESD防护设备,即 可轻而易举地满足系统对ESD的要求(一般为8 kV)。为满足移动GPS行业对更高灵敏度的要求,英飞凌的GPS接收前端模块实现了18.6dB的增益,比竞争性解决方案的16.5dB高出20%以上。

“市场专家预计,GPS有望进一步渗透至各种应用和设备中,在2011年制造的所有手机中,至少三分之一的手机将具备GPS功能。今后,GPS将会成为下一代手机的标准功能。”英 飞凌科技射频与保护器件高级营销总监Mi-chael Mauer指出,“英飞凌将继续致力于开发全集成式高性能GPS接收前端模块产品组合。凭借GPS接收前端模块BGM781N11,英 飞凌进一步巩固了自己在GPS市场的领导地位。”

上市、封装与定价
BGM781N11 GPS接收前端模块目前已实现量产。英飞凌还提供评估套件。订购量达到一万颗时,BGM781N11的单价为1美元。BGM781N11采用小型无管脚TSNP11-2封装,尺 寸仅为2.5mm x 2.5mm x 0.7mm。

关于GPS接收前端模块的更多技术信息可在 www.infineon.com/BGM781N11找到。

About Infineon

总部位于德国Neubiberg的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、连通性和安全性提供半导体和系统解决方案。2009财年(截止到9月份),公司实现销售额30.3亿欧元,在 全球拥有约25,650名雇员。英飞凌科技公司的业务遍及全球,在美国苗必达、亚太地区的新加坡和日本东京等地拥有分支机构。英飞凌公司目前在法兰克福股票交易所(股票代码:IFX)和美国柜台交易市场( OTCQX)International Premier(股票代号:IFNNY)挂牌上市。

更多信息请访问 www.infineon.com
本新闻稿还可从 www.infineon.com/press/找到。

Information Number

INFIMM201002.028

Press Photos

  • The BGM781N11 of Infineon is the world's smallest GPS Receive Front-End Module with just 2.5mm x 2.5mm x 0.7mm in size and includes all key components to amplify a GPS signal and filter out interference.
    The BGM781N11 of Infineon is the world's smallest GPS Receive Front-End Module with just 2.5mm x 2.5mm x 0.7mm in size and includes all key components to amplify a GPS signal and filter out interference.
    BGM781N11_EN

    JPG | 804 kb | 2126 x 1535 px