英飞凌推出支持PFC和FOC功能的8位微控制器系列产品以提高电机驱动能效

2008-5-19 | 市场新闻

2008年5月19日,德国Neubiberg讯——英飞凌科技股份公司(FSE/NYSE:IFX)今日宣布功能强大的XC800家族再添新成员。全新的XC878系列是具有成本效益的8位微控制器( MCU),具有功率因数校正(PFC)和磁场定向控制(FOC)功能,可使工业和汽车应用的电机驱动装置获得出色的扭矩,更低的噪声和更高的能效。英飞凌作为微控制器供应商,在全球范围内率先提供适用于空调系统、 泵和风扇等价格敏感型应用并支持PFC和FOC功能的标准8位MCU。

PFC可控制交流电源的电流。线性供电电机控制应用需要更高的功率效率,同时需要电流谐波失真降低的直流稳压电源。FOC是一种电机操控技术,可使电机在各种速度条件下平稳、高效地运行,使 电机效率最高达到95%。

XC878 MCU可以8位成本提供16位性能,它集成了高达64 KB闪存和16位矢量计算器,工作频率最高为27 MHz。具 备高达10个PWM输出端和4个独立时基的2个独立PWM单元可实现对两台三相电机的独立控制。

XC878 MCU使电机驱动系统成本大约降低50%
8位MCU的PFC与FOC功能的有机结合将会使空调压缩机等电机驱动系统受益匪浅。采用英飞凌XC878可使驱动系统成本降低约50%,由目前的4美元左右降低至2美元左右,这 是因为具备FOC功能的8位MCU可处理以往由16位或32位MCU执行的任务。具备独立时基的2个PWM单元可使电机控制和PFC算法集成至一个芯片,从而降低系统成本。此外,FOC使电机运行更为安静,通 过使电机始终获得最佳扭矩,带来了更高的效率。

8位XC878 MCU系列的技术信息
全新XC878 MCU系列目前包含12款产品,差别主要体现在外设、闪存(52或64 Kb)和温度范围等方面。该产品系列采用零等待闪存、16位矢量计算器、高达64 Kb片上闪存( 存储程序和数字)、2个CAN节点和10位快速模数转换器,实现了更高的性能,进一步增强了8位XC800家族。此外,XC878 MCU还具备2个捕获比较单元,使其能够运行2台电机或控制LED照明。该 器件还经过专门设计,通过适用于施工车辆、铲车、海上电动设备等交通应用和工业自动化应用的片上MultiCAN接口,可简化CAN(控制器局域网)系统的开发。

XC878 MCU配备一个片上时钟生成单元,具备时钟监控功能等集成安全特性。XC878 MCU采用绿色LQFP-64封装,工作温度范围为-40 °C 至 +85和-40 °C至 +105 °C,工作电压范围为3 V至5.5 V。

供货与定价
XC878已开始供应样品,预计到2008年9月实现量产。目前可获得全套低成本开发工具,包括入门套件、开发套件、相关资料和免费的基于小器件C语言编译器(SDCC)的工具链。在 采购量达到1万颗的情况下,采用LQFP-64封装的XC878 MCU的单价为1.50欧元(约合2.20美元)。

XC878 MCU亮相2008年欧洲PCIM展会
英飞凌将在德国纽伦堡举办的2008年欧洲PCIM展会(5月27日至29日)12号展厅404号展台展出全新的XC878系列和适用于采用XC878 MCU的双三相电机控制器的应用套件。

如欲了解更多有关XC878和英飞凌8位微控制器产品系列的信息,敬请登录 www.infineon.com/xc878www.infineon.com/xc800

 

About Infineon

总部位于德国Neubiberg的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、连通性和安全性提供半导体和系统解决方案。2007财年(截止到9月份),公司实现销售额77亿欧元( 包括奇梦达的销售额36亿欧元),在全球拥有约43,000名雇员(其中奇梦达雇员约13,500人)。英飞凌科技公司的业务遍及全球,在美国苗必达、亚太地区的新加坡和日本东京等地拥有分支机构。英 飞凌公司已列入法兰克福股票交易所的DAX指数,并在纽约股票交易所挂牌上市,股票代号:IFX。

如欲了解更多信息,敬请登录 www.infineon.com 


该新闻稿可从以下网站找到: http://www.infineon.com/press 

Information Number

INFAIM200805.062

Press Photos

  • Infineon's XC878 family of 8-bit microcontrollers is capable of supporting both Power Factor Correction (PFC) and Field Oriented Control (FOC). It enables excellent torque dynamics, reduced noise and higher energy efficiency for motor drives in industrial, automotive and price-sensitive applications, such as air conditioning systems, pumps and fans.
    Infineon's XC878 family of 8-bit microcontrollers is capable of supporting both Power Factor Correction (PFC) and Field Oriented Control (FOC). It enables excellent torque dynamics, reduced noise and higher energy efficiency for motor drives in industrial, automotive and price-sensitive applications, such as air conditioning systems, pumps and fans.
    XC878

    JPG | 143 kb | 886 x 710 px