英飞凌推出快速评估3种8位微控制器的超低成本三合一评估平台

2007-7-11 | 市场新闻

2007年7月11日,德国Neubiberg讯——英飞凌科技股份公司(FSE/NYSE: IFX)今日宣布推出面向该公司XC800 8位嵌入式闪存微控制器(MCU)家族的超低成本评估套件。全 新的XC800 USCALE套件采用USB(通用串行总线)插件样式,能在一个平台上为XC866、 XC886和XC888等微控制器提供完整的评估功能。

USCALE套件可访问微控制器多种关键特性,比如:CAN(控制器局域网)、模数转换器、捕获比较单元、定时器和用于磁场定向控制的矢量计算机,同时还可以访问这三种微控制器的硬件信号,便 于进行更广泛的基准测试和评估。该套件具备开发工具链、示例和指南,可快速安装和方便使用。

英飞凌高性能XC800系列微控制器采用了增强的8051内核与嵌入式闪存以及功能强大的片上外设。USCALE套件支持的这三种微控制器适用于多种不同应用,包括电机控制装置、汽车车身和白色家电, 并为工业和楼宇自控系统带来了联网功能。

XC866系列微控制器的相关技术信息
XC866系列微控制器具备出色的性能和成本节省特性,包括26.67 MHz系统频率、4KB-16KB闪存、片上振荡器和PLL时钟发生器、支 持3.3伏或5.0伏电压的嵌入式稳压器和EEPROM支持功能。改进的PWM单元可提供各种先进的特性,包括集成的死区控制、紧急关闭控制、直接霍尔传感器输入和自动触发ADC。转 换时间仅为1.5微秒的10位模数转换器可提供自动扫描和比较器模式等高级特性。英飞凌XC866也可提供多种通信接口,包括LIN、SSC和UART。X C866微控制器采用兼容RoHS的TSSOP-38封装,外形尺寸小巧(9.7毫米X4.4 毫米),可在高达140°C的温度下工作,能提供27个通用I/O。

XC886与XC888系列微控制器的相关技术信息
采用高达32KB闪存的XC886 与 XC888微控制器在一颗芯片上集成了CAN控制器和LIN支持功能,可提供先进的联网功能。该片上CAN模块可执行大多数联网功能,降低了CPU的负荷。X C886 与XC888微控制器的先进特性还包括由可实现快速数学计算的16位乘除法单元(MDU)和专用于矢量旋转角度计算(实现磁场定向电机控制)的16位协处理器的CORDIC(协调旋转数字计算机)单 元提供的强大计算能力。其它关键特性还包括智能PWM单元、高精度8通道10位数模快速转换器和带两个独立16位定时器(专用于生成PWM)的高性能捕获比较单元,能够以8位的成本实现16位的电机控制性能。

XC800 USCALE评估与开发套件特性一览
• 低成本的USB插件样式为8位微控制器XC866, XC886和XC888提供了一个统一的评估平台
• 支持高性能8051系列产品XC800的完整工具链
• 可通过16引脚连接器获得硬件信号
• 包括编译器和调试器
• 安装简单,带有示例和指南

定价与供货情况
XC800 USCALE 入门套件目前可从英飞凌销售代表处和经销商处获得。建议转售价格为39欧元。

更多有关XC800 USCALE入门套件特性的信息和资料订购信息可在www.infineon.com/uscale网站找到。

更多有关英飞凌 8位微控制器产品组合的信息可在 www.infineon.com/XC800网站找到。

About Infineon

总部位于德国慕尼黑的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、连通性和安全性提供半导体和系统解决方案。2006财年(截止到9月份),公司实现销售额79亿欧元( 包括奇梦达的销售额38亿欧元),在全球拥有约42,000名雇员(其中奇梦达雇员约12,000人)。英飞凌科技公司的业务遍及全球,在美国圣何塞、亚太地区的新加坡和日本东京等地拥有分支机构。英 飞凌公司已列入法兰克福股票交易所的DAX指数,并在纽约股票交易所挂牌上市,股票代号:IFX。

如欲了解更多信息,敬请登录www.infineon.com

Information Number

INFAIM200707.071

Press Photos

  • The USCALE kit offers access to the key features and to the hardware signals of each of the three 8-bit microcontrollers for extensive benchmarking and evaluation.
    The USCALE kit offers access to the key features and to the hardware signals of each of the three 8-bit microcontrollers for extensive benchmarking and evaluation.
    USCALE_microC_blue_0707

    JPG | 314 kb | 1535 x 1063 px

  • The USCALE kit offers access to the key features and to the hardware signals of each of the three 8-bit microcontrollers for extensive benchmarking and evaluation.
    The USCALE kit offers access to the key features and to the hardware signals of each of the three 8-bit microcontrollers for extensive benchmarking and evaluation.
    USCALE_microC_white_0707

    JPG | 178 kb | 1535 x 1063 px

  • The USCALE starterkit is contained in a USB (Universal Serial Bus) stick that provides full evaluation capabilities for Infineon's 8-bit microcontrollers XC866, XC886 and XC888, all on an ultra-low-cost 3-in-1 platform.
    The USCALE starterkit is contained in a USB (Universal Serial Bus) stick that provides full evaluation capabilities for Infineon's 8-bit microcontrollers XC866, XC886 and XC888, all on an ultra-low-cost 3-in-1 platform.
    USCALE_white_0707

    JPG | 159 kb | 1535 x 1063 px

  • The USCALE kit offers access to hardware signals through a 16 pin connector for evaluating the key features of the 8-bit microcontrollers XC866, XC886 and XC888: CAN, ADC, Capture Compare Unit, Timers and Vector Computer (for FOC motor control).
    The USCALE kit offers access to hardware signals through a 16 pin connector for evaluating the key features of the 8-bit microcontrollers XC866, XC886 and XC888: CAN, ADC, Capture Compare Unit, Timers and Vector Computer (for FOC motor control).
    USCALE_diagram

    JPG | 67 kb | 1240 x 709 px