我们推动您的成功
降低风险,加快开发项目,缩短上市时间
我们使生活更轻松、更安全、更环保
凭借少投入,多产出的技术,并且受惠于每个人。
创新技术
损耗更低,效率更高

Infineon Technologies Bipolar GmbH & Co. KG

Success is joining together

Low losses and dynamic process control: The advantages of welding diodes from Infineon Technologies Bipolar GmbH & Co. KG in Warstein have developed into the core components of the Bosch Rexroth welding transformer series. This type of transformer is mainly used in welding robots for the automotive industry to connect e.g. body parts. The effective collaboration since 2004 is celebrated by both companies with the symbolic presentation of the 100,000th welding diode.

"We are very proud of our long-standing partnership with Bosch," says Martin Hierholzer, CEO of Infineon Technologies Bipolar. "We understand how modern technology is becoming more and more powerful through semiconductors; thus we enable solutions that make our customers successful in their respective field of application. Every component in Warstein is developed with passion and manufactured with precision - including our welding diodes, of course."

It has a service life of more than 10 million welding spots: One set of the welding diodes from Warstein can theoretically produce 2,000 bodies for automobiles.

新闻

创新成果奖

在Autohaus Sternpark的220位嘉宾出席的颁奖典礼上颁发了“勒夫施塔特创新奖(Lippstadt Innovation Prize)”。每两年颁发一次此奖项以表彰该地区杰出的技术和创新领导者。

“我们很高兴收到此奖项,这是对我们工作的认可和激励。我们非常自豪我们的产品对世界能源供应作出了重要贡献,”英飞凌瓦尔斯泰因总经理Martin Hierholzer在获奖演说中表示。

新型光触发晶闸管是现代高压直流电厂的关键组件。这种技术大大降低了控制电子学的复杂性,并使组件实际上牢不可破,这显著提升了这些工厂的可靠性。

观看颁奖典礼视频

2:34

The Lippstadt Innovation Prize was awarded during a gala ceremony at the Autohaus Sternpark.