Where to find our products in daily life

In the morning when you wake up, do not suspect that the semiconductors manufactured in Cegléd made you possible to switch on the lights at home – from the production till the transport of energy.
When you go to the kitchen and the coffee is made on the induction plate or put your mug into the dishwasher, you do not realize that the new inverter solutions made 40-50% energy savings possible in the field of white goods.
It doesn’t matter that you travel to work by tram, trolley bus or train, the power control of these vehicles are done by Infineon devices.
When you use the lift or the escalator at your workplace, our devices guaranteed the smooth start of these escalators.
When your smartphone is ringing at your desktop, our tools ensure the high quality of communication.
In the afternoon you take a taxi in order to arrive on time to the train station. You can find several semiconductors in an average car, but if you are lucky you will travel by a hybrid or an electric car and you can be sure that almost 75 Infineon semiconductor appliances ensure the safety operation of these vehicles.
If you take a high-speed train the 20 MW or 27.000 horse power is regulated by some of the Infineon semiconductors. Using these devices for optimal acceleration and breaking energy back-feeding, the German railways safe the annual power consumption of a small city with 30.000 inhabitants.
When you look out of the window, you can see a wind power plant in the distance that produce the power consumption of 1000 households, which means 4000 people, and you can also find semiconductors inside of it, which were produced in Cegléd.
When you are at the passport control at an airport, your documentation probably contains an Infineon electronic chips as well.
At the hotel you check-in with your bank card which also contains the Infineon electronic chips and with then you switch on the energy-saving inverter air conditioner.
You are now having a rest, but the metropolis never sleep, you can see the shining lights of the advertisements, you can hear the noises of the metro and high-speed trains, car lights flash on the wall. You do not even realize that the reliable semiconductors, which produced in Cegléd, provide these solutions for more than a decade.
It is visible that you find our semiconductor solutions in all aspects of our daily life, although the medical devices, the harbour cranes, the construction and agricultural machinery are still not mentioned.