-------------------------------------------------------------------------------
CE222460_SPI_FRAM_ACCESS_WITH_PSOC6_SMIF
-------------------------------------------------------------------------------

Requirements
------------
Tool: ModusToolbox™ IDE
Programming Language: C
Associated Parts: All PSoC®6 MCU parts

Software Setup
--------------
This code example requires a PC terminal emulator to display orientation  
information.

Open terminal emulator/software such as Tera Term or PuTTY and select the KitProg3's COM port 
with a baud rate setting of 115200 bps, data bits 8, parity none, and 
stop bit 1.

Supported Kits
--------------
PSoC 6 BLE Pioneer Kit
PSoC 6 WiFi-BT Pioneer Kit

Overview
--------
This code example demonstrates implementing the SPI host controller using PSoC 6 SMIF 
to access the SPI F-RAM. The result is displayed by driving the status LED (RGB) 
which turns green when the result is a pass, and turns red when the result is a fail. 
The code example also enables the UART interface to connect to a PC to monitor the result.

Build and Program
-----------------
Select any project in the application.
In the Quick Panel click the <application name> Program (KitProg3) link.
The IDE builds the application, programs the kit, and starts execution.

Code Example Document
---------------------
The PDF file for this example is in the example folder. It has full details
on the design, how to use the code example, and what to look for when it runs.

-------------------------------------------------------------------------------