Cypress Wifi Linux FMAC Driver Package - README
===============================================

Package Version
---------------
v5.4.18-2020_0925


Release Date
------------
2020-09-25


Description
-----------
This is Cypress's Linux brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.

Files in this release:
* Backports package (cypress-backports-v5.4.18-2020_0925-module-src.tar.gz)
* Firmware/clm_blob files (cypress-firmware-v5.4.18-2020_0925.tar.gz)
* Cypress fmac patch files (cypress-patch-v5.4.18-2020_0925.tar.gz)
* Device tree files (cypress-devicetree-2020-09-25.tar.gz)
* hostapd/wpa_supplicant patch (cypress-hostap_2_9-2020_0925.tar.gz)
* Cirrent Agent (cypress-cirrent-1.60.tar.gz)
* README

For more information about the Linux brcmfmac project, see:

[brcm80211 Wireless Wiki](https://wireless.wiki.kernel.org/en/users/drivers/brcm80211)

For more information about Linux backports project, see:

[Linux Backports Project](https://backports.wiki.kernel.org/index.php/Main_Page)

Checksum
--------
fb71c344e705f5bc9fdae3ce0fbfa299f0af0939ff3ec782aeca0308911d830d cypress-fmac-v5.4.18-2020_0925.zip
5642225573606342615849a2a2db04ad5697f35e669313d2b3492cef3aa10813 cypress-backports-v5.4.18-2020_0925-module-src.tar.gz
ce3bb31020e5ffe24fe549802440c137d14a05ad77af3e8e1fb9e184db96ed55 cypress-cirrent-1.60.tar.gz
d5422a4d1348ca619987cd65e99542ef99a6ea8bb531351bcaf90fcf4849dcac cypress-devicetree-2020-09-25.tar.gz
0b3ce60d745975e45ca1197dad8b7dd2618c5b5ccd8327b0ca69ece99b3edb0f cypress-firmware-v5.4.18-2020_0925.tar.gz
17c50c4398ccfb75e6f886483fc460832e90cde1e2058bc58332672b390bc218 cypress-hostap_2_9-2020_0925.tar.gz
44dfc2c35dc202e6a9cfa1ef20a865c737c89cca212d95e3e08b29311194a147 cypress-patch-v5.4.18-2020_0925.tar.gz

Change Log
----------
[2020-09-25]
Initial Post

Supported Features
------------------
| Feature            | 43455 | 4373SDIO | 4373USB | 43012 | 4356PCIe | 4354 | 43362 | 4343w | 43340 | 4339 | 43570PCIe | 54591PCIe |
|--------------------|:-----:|:--------:|:-------:|:-----:|:--------:|:----:|:-----:|:-----:|:-----:|:----:|:---------:|:---------:|
| SoftAP             |   O   |     O    |    O    |   O   |     O    |   O  |   O   |   O   |   O   |   O  |     O     |     O     |
| APSTA              |   O   |          |         |       |          |      |       |       |       |      |     O     |     O     |
| P2P                |   O   |     O    |    O    |   O   |     O    |   O  |   O   |   O   |   O   |   O  |     O     |     O     |
| WoWL               |   O   |          |         |       |          |      |       |       |       |      |           |           |
| Voice Enterprise   |   O   |          |         |       |          |      |       |       |       |      |           |           |
| OKC                |   O   |          |         |       |          |      |       |       |       |      |           |           |
| WPA3-STA           |   O   |     O    |    O    |   O   |          |      |       |       |       |      |           |           |
| WPA3-AP            |   O   |     O    |    O    |       |          |      |       |       |       |      |           |           |
| Fast Roaming       |   O   |          |         |   O   |          |      |       |       |       |      |           |           |
| Thermal Throttling |   O   |          |         |       |          |      |       |   O   |       |      |           |           |
| CYNC               |       |          |         |       |          |      |       |       |       |      |           |     O     |
| DPP                |   O   |          |         |   O   |          |      |       |       |       |      |           |     O     |


Test Environment
----------------
* ARM (MCIMX6SX-SDB)
   * Linux v4.14.78 (NXP imx_4.14.78_1.0.0_ga)
   * backports
* x86
   * Linux v4.12
   * backports


Instructions
------------
The patch files in this package are based on Linux v5.4.18, so older kernels
need use backports package. Below are examples of how to use this package
with an older kernel or linux-stable v5.4.18.

### Using backports with an older kernel (v3.10+)

Linux kernel image and cypress driver modules need to be built separately.
Below is the example of using with iMX Linux v4.14.78:

#### Build the kernel image
```bash
#1. Have the BSP kernel source available
   git clone https://source.codeaurora.org/external/imx/linux-imx
   cd linux-imx
   git checkout imx_4.14.78_1.0.0_ga
#2. Set up build environment and kernel configuration
   source /opt/poky/1.8/environment-setup-cortexa7hf-vfp-neon-poky-linux-gnueabi
   make imx_v7_defconfig
#3. Edit .config and build cfg80211 as module
#     CONFIG_CFG80211=m
#     CONFIG_BCMDHD=n
#4. Enable below configs in .config
#     CONFIG_ASYMMETRIC_KEY_TYPE=y
#     CONFIG_ASYMMETRIC_PUBLIC_KEY_SUBTYPE=y
#     CONFIG_X509_CERTIFICATE_PARSER=y
#     CONFIG_PKCS7_MESSAGE_PARSER=y
#5. Build the Linux kernel image
   make oldconfig
   make zImage -j 8
#6. The kernel image is available here
   arch/arm/boot/zImage
```

#### Build the cypress driver/backports modules
```bash
#1. Untar the Cypress backports package
    tar zxvf cypress-backports-*.tar.gz
    cd v5.4.18-backports
#2. (Native) compile local tools and generate .config (in a new terminal
#   without sourcing Yoctol toolchain settings)
    bash
    MY_KERNEL=<the 4.14.78 kernel path>
    make KLIB=$MY_KERNEL KLIB_BUILD=$MY_KERNEL defconfig-brcmfmac
#3. (Cross) compile kernel modules
    source /opt/poky/1.8/environment-setup-cortexa7hf-vfp-neon-poky-linux-gnueabi
    make KLIB=$MY_KERNEL KLIB_BUILD=$MY_KERNEL modules
#4. The kernel modules are available here
#      compat/compat.ko
#      net/wireless/cfg80211.ko
#      drivers/net/wireless/broadcom/brcm80211/brcmutil/brcmutil.ko
#      drivers/net/wireless/broadcom/brcm80211/brcmfmac/brcmfmac.ko
```

#### Device tree
```bash
#1. Untar the cypress devicetree package
    tar zxvf cypress-devicetree-*.tar.gz
#2. Find your board's dtb file, for example
#      cypress-devicetree/iMX6SX/4.14.78/imx6sx-sdb-btwifi-fmac.dtb
```
Note: If your board's dtb is not available in the cypress devicetree
      package, please refer to the available dts/dtsi files and create
      them for your board, then compile them for the dtb file. iMX dts
      files are located in linux-imx/arch/arm/boot/dts/ folder of the
      Linux kernel tree. Below command compiles a dtb file
```bash
    make ARCH=arm <devicetree name>.dtb
```

#### Load the cypress wifi driver
```bash
#1. Copy your boards's zImage and dtb files to the target board
    bash
    TARGET_IP=<target board IP>
    scp <dtb file> root@$TARGET_IP:/run/media/mmcblk1p1/cy.dtb
    scp <zImage file> root@$TARGET_IP:/run/media/mmcblk1p1/zImage_cy
#2. Copy firmware files to the target board
    tar zxvf cypress-firmware*.tar.gz
    scp firmware/* root@$TARGET_IP:/lib/firmware/cypress
#3. Copy your nvram file (from board vendor) to the target board and rename it
    scp <nvram file> root@$TARGET_IP:/lib/firmware/cypress/<fw name>.txt
#      (fw name is your chip's *.bin file name in the cypress firmware package)
#4. Copy cypress kernel modules to the target board
    scp <module files> root@$TARGET_IP:/lib/modules/4.14.78
#5. (iMX console) Press ctrl-c after target boot to enter u-boot and configure it
#   for the new zImage/dtb files
   env print image fdt_file
   setenv image zImage_cy
   setenv fdt_file cy.dtb
   saveenv
   env print image fdt_file
   reset
#6. (iMX console) Boot up the target board with the above zImage and insmod cypress modules
    insmod /lib/modules/4.14.78/compat.ko
    insmod /lib/modules/4.14.78/cfg80211.ko
    insmod /lib/modules/4.14.78/brcmutil.ko
    insmod /lib/modules/4.14.78/brcmfmac.ko
```
Note: More on fmac driver [firmware/nvram install](https://wireless.wiki.kernel.org/en/users/drivers/brcm80211#firmware_installation1)

### Using Linux Stable v5.4.18
```bash
#1. Download Linux stable kernel source
    wget https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/snapshot/linux-5.4.18.tar.gz
    tar zxvf linux-5.4.18.tar.gz
#2. In Linux root folder, untar/apply cypress patches with below bash commands
    cd linux-5.4.18
    tar zxvf cypress-patch*.tar.gz
    for i in cypress-patch/*.patch; do patch -p1 < $i; done
#3. Set kernel .config and enable below options, then compile kernel image
#      CONFIG_BRCMUTIL=y
#      CONFIG_BRCMFMAC=y
#      CONFIG_BRCMFMAC_SDIO=y
#      CONFIG_BRCMFMAC_PROTO_BCDC=y
#      CONFIG_BRCMFMAC_PCIE=y
#      CONFIG_BRCMFMAC_PROTO_MSGBUF=y
#4. (optional) Backup original firmware files
    cp /lib/firmware/cypress /lib/firmware/cypress-bak -r
#5. Update firmware files in /lib/firmware/cypress
    tar zxvf cypress-firmware*.tar.gz
    cp firmware/* /lib/firmware/cypress
#6. Boot the system with the new kernel image
```


Instructions - Hostap
---------------------
The patch files in this package are based on Hostap v2.9. Below is an example
of how to apply these files and build hostapd/wpa_supplicant binaries.

### Build the hostapd/wpa_supplicant binaries
```bash
#1. Download Hostap source
    wget https://w1.fi/cgit/hostap/snapshot/hostap_2_9.tar.gz
    tar zxvf hostap_2_9.tar.gz
#2. In Hostap root folder, untar/apply cypress patches with below bash commands
    cd hostap_2_9
    tar zxvf cypress-hostap_2_9*.tar.gz
    for i in cypress-hostap_2_9/*.patch; do patch -p1 < $i; done
#3. (Hostapd) in hostapd root directory, have a build time configuration file,
#   .config, and build hostapd and hostapd_cli
    cd hostapd
    cp defconfig .config
    make clean
    make
#4. (Wpa_supplicant) in wpa_supplicant root directory, have a build time
#   configuration file, .config, and build wpa_supplicant and wpa_cli
    cd wpa_supplicant
    cp defconfig .config
    make clean
    make
#5. The binaries are available here
#     hostap_2_9/hostapd/hostapd
#     hostap_2_9/hostapd/hostapd_cli
#     hostap_2_9/wpa_supplicant/wpa_supplicant
#     hostap_2_9/wpa_supplicant/wpa_cli
```
Note: Set CONFIG_SAE=y in .config to enable WPA3-Personal (SAE) support.


Instructions - Cirrent Agent
----------------------------

The Cirrent Agent with IoT Network Intelligence support has been pre-compiled
for easy installation on platforms with armhf architecture.

### Install the Cirrent Agent files

```bash
#1. Untar the Cirrent Agent installation package
    tar zxvf cypress-cirrent-1.60.tar.gz
#2. Install the required files to the root / directory
    cp -av cypress-cirrent/* /
#3. Edit and uncomment PROVISION_CRED from the /etc/default/cirrent file with
#   credentials from https://console.cirrent.com
#4. Enable the Cirrent Agent to start on boot and reboot with Systemd init
    systemctl enable cirrent
#   or with SysV init
    update-rc.d cirrent defaults
    reboot
```

For more information on using the Cirrent Agent, please visit
https://support.cirrent.com


Cypress Wifi Linux FMAC Driver Package - Release Notes
======================================================

FMAC Driver Changes
-------------------
* 4373 (0001, 0090, 0096)
* Device tree changes (0002)
* APSTA (0003, 0101-103)
* SoftAP (0004, 0070)
* Fast roaming (0005, 0019, 0071-0075)
* Wake on Wireless LAN (0006-0007, 0025, 0030, 0038)
* Throughput enhancement (0008, 0051, 0092, 0094)
* ARP Offload (0009)
* Peer-to-peer (0010-0011, 0041-0042, 0056, 0085, 112)
* USB (0012, 0014, 0022-0024, 0027, 0032, 0034-0035, 0081-0082)
* WMM (0013, 0026, 0040, 0043, 0093, 0095)
* 89359 (0015-0018, 0028, 0033, 0047, 0053, 0063, 0066-0067, 111)
* Miracast (0020)
* 4339 (0021, 0097)
* Power saving (0029, 0045, 0057)
* SDIO (0031, 0083, 115, 125)
* Firmware interface (0036, 0039, 0068, 113)
* 4356 (0037, 0069)
* PCIe (0044, 0058, 0064, 0099-0100, 116-117)
* 43455 (0046, 0098)
* SDIO/USB flow control (0049-0050, 123, 128-129)
* 43012 (0052, 0087-0089)
* 43570 (0054)
* GTK rekey (0055)
* 89459/54591 (0059, 0086, 122)
* Generic bugs (0060, 0061, 0091, 104-107, 114, 118-119)
* WPA3 (0062, 0077-0080, 0084)
* 4354 (0065)
* OKC (0076)
* DPP (108, 124)
* Firmware naming (109)
* Monitor mode (110)
* Debug capability (120, 127)
* Manufacturing (121)
* Auto channel selection (126)


FMAC Driver Patch List
----------------------
* 0001-brcmfmac-set-F2-blocksize-and-watermark-for-4373.patch [v5.8-rc1]
* 0002-non-upstream-add-sg-parameters-dts-parsing.patch [x]
* 0003-brcmfmac-set-apsta-to-0-when-AP-starts-on-primary-in.patch [v5.8-rc1]
* 0004-brcmfmac-support-AP-isolation.patch [-]
* 0005-brcmfmac-make-firmware-eap_restrict-a-module-paramet.patch [-]
* 0006-non-upstream-support-wake-on-ping-packet.patch [x]
* 0007-non-upstream-remove-WOWL-configuration-in-disconnect.patch [x]
* 0008-brcmfmac-make-setting-SDIO-workqueue-WQ_HIGHPRI-a-mo.patch [-]
* 0009-brcmfmac-remove-arp_hostip_clear-from-brcmf_netdev_s.patch [v5.8-rc1]
* 0010-brcmfmac-P2P-CERT-6.1.9-Support-GOUT-handling-P2P-Pr.patch [v5.8-rc1]
* 0011-brcmfmac-only-generate-random-p2p-address-when-neede.patch [v5.8-rc1]
* 0012-brcmfmac-increase-max-hanger-slots-from-1K-to-3K-in-.patch [v5.7-rc1]
* 0013-brcmfmac-map-802.1d-priority-to-precedence-level-bas.patch [v5.8-rc1]
* 0014-brcmfmac-set-state-of-hanger-slot-to-FREE-when-flush.patch [v5.9-rc1]
* 0015-brcmfmac-add-RSDB-condition-when-setting-interface-c.patch [v5.6-rc1]
* 0016-brcmfmac-not-set-mbss-in-vif-if-firmware-does-not-su.patch [v5.6-rc1]
* 0017-brcmfmac-support-the-second-p2p-connection.patch [v5.8-rc1]
* 0018-brcmfmac-add-support-for-BCM4359-SDIO-chipset.patch [v5.6-rc1]
* 0019-brcmfmac-send-port-authorized-event-for-FT-802.1X.patch [v5.5-rc1]
* 0020-brcmfmac-add-vendor-ie-for-association-responses.patch [v5.8-rc1]
* 0021-brcmfmac-fix-4339-CRC-error-under-SDIO-3.0-SDR104-mo.patch [v5.8-rc1]
* 0022-brcmfmac-fix-the-incorrect-return-value-in-brcmf_inf.patch [v5.7-rc1]
* 0023-brcmfmac-Fix-double-freeing-in-the-fmac-usb-data-pat.patch [v5.7-rc1]
* 0024-brcmfmac-Fix-driver-crash-on-USB-control-transfer-ti.patch [v5.7-rc1]
* 0025-brcmfmac-avoid-network-disconnection-during-suspend-.patch [x]
* 0026-brcmfmac-allow-credit-borrowing-for-all-access-categ.patch [v5.9-rc1]
* 0027-non-upstream-Changes-to-improve-USB-Tx-throughput.patch [x]
* 0028-brcmfmac-reset-two-D11-cores-if-chip-has-two-D11-cor.patch [v5.6-rc1]
* 0029-brcmfmac-introduce-module-parameter-to-configure-def.patch
* 0030-brcmfmac-configure-wowl-parameters-in-suspend-functi.patch [x]
* 0031-brcmfmac-keep-SDIO-watchdog-running-when-console_int.patch [v5.9-rc1]
* 0032-brcmfmac-To-fix-kernel-crash-on-out-of-boundary-acce.patch [v5.9-rc1]
* 0033-brcmfmac-reduce-maximum-station-interface-from-2-to-.patch [v5.9-rc1]
* 0034-brcmfmac-validate-ifp-pointer-in-brcmf_txfinalize.patch [v5.2-rc1]
* 0035-brcmfmac-clean-up-iface-mac-descriptor-before-de-ini.patch [v5.2-rc1]
* 0036-brcmfmac-To-fix-Bss-Info-flag-definition-Bug.patch [v5.9-rc1]
* 0037-brcmfmac-disable-command-decode-in-sdio_aos-for-4356.patch [x]
* 0038-brcmfmac-increase-default-max-WOWL-patterns-to-16.patch
* 0039-non-upstream-Enable-Process-and-forward-PHY_TEMP-eve.patch [x]
* 0040-brcmfmac-Use-FW-priority-definition-to-initialize-WM.patch [v5.9-rc1]
* 0041-brcmfmac-Fix-P2P-Group-Formation-failure-via-Go-neg-.patch [v5.8-rc1]
* 0042-brcmfmac-Add-P2P-Action-Frame-retry-delay-to-fix-GAS.patch [v5.8-rc1]
* 0043-brcmfmac-Use-default-FW-priority-when-EDCA-params-sa.patch [v5.9-rc1]
* 0044-brcmfmac-fix-continuous-802.1x-tx-pending-timeout-er.patch [x]
* 0045-brcmfmac-add-sleep-in-bus-suspend-and-cfg80211-resum.patch [x]
* 0046-brcmfmac-fix-43455-CRC-error-under-SDIO-3.0-SDR104-m.patch [v5.8-rc1]
* 0047-brcmfmac-set-F2-blocksize-and-watermark-for-4359.patch [v5.6-rc1]
* 0048-brcmfmac-reserve-2-credits-for-host-tx-control-path.patch [v5.9-rc1]
* 0049-brcmfmac-update-tx-status-flags-to-sync-with-firmwar.patch [v5.9-rc1]
* 0050-brcmfmac-fix-credit-reserve-for-each-access-category.patch [-]
* 0051-brcmfmac-fix-throughput-zero-stalls-on-PM-1-mode-due.patch [v5.9-rc1]
* 0052-brcmfmac-43012-Update-MES-Watermark.patch [v5.8-rc1]
* 0053-brcmfmac-add-support-for-CYW89359-SDIO-chipset.patch [x]
* 0054-brcmfmac-add-CYW43570-PCIE-device.patch
* 0055-brcmfmac-Use-seq-seq_len-and-set-iv_initialize-when-.patch [v5.8-rc1]
* 0056-brcmfmac-use-actframe_abort-to-cancel-ongoing-action.patch [v5.8-rc1]
* 0057-brcmfmac-fix-scheduling-while-atomic-issue-when-dele.patch [x]
* 0058-brcmfmac-increase-message-buffer-size-for-control-pa.patch [v5.9-rc1]
* 0059-brcmfmac-Support-89459-pcie.patch
* 0060-brcmfmac-Fix-for-unable-to-return-to-visible-SSID.patch [v5.9-rc1]
* 0061-brcmfmac-Fix-for-wrong-disconnection-event-source-in.patch [v5.9-rc1]
* 0062-brcmfmac-add-support-for-SAE-authentication-offload.patch [v5.5-rc1]
* 0063-brcmfmac-Support-multiple-AP-interfaces-and-fix-STA-.patch
* 0064-brcmfmac-Support-custom-PCIE-BAR-window-size.patch
* 0065-brcmfmac-set-F2-blocksize-and-watermark-for-4354.patch [v5.8-rc1]
* 0066-brcmfmac-support-for-virtual-interface-creation-from.patch [-]
* 0067-brcmfmac-set-security-after-reiniting-interface.patch [v5.8-rc1]
* 0068-brcmfmac-increase-dcmd-maximum-buffer-size.patch [-]
* 0069-brcmfmac-set-F2-blocksize-and-watermark-for-4356-SDI.patch [v5.8-rc1]
* 0070-brcmfmac-set-net-carrier-on-via-test-tool-for-AP-mod.patch [-]
* 0071-nl80211-add-authorized-flag-back-to-ROAM-event.patch
* 0072-brcmfmac-set-authorized-flag-in-ROAM-event-for-offlo.patch
* 0073-brcmfmac-set-authorized-flag-in-ROAM-event-for-PMK-c.patch
* 0074-nl80211-add-authorized-flag-to-CONNECT-event.patch
* 0075-brcmfmac-set-authorized-flag-in-CONNECT-event-for-PM.patch
* 0076-brcmfmac-add-support-for-Opportunistic-Key-Caching.patch
* 0077-nl80211-support-4-way-handshake-offloading-for-WPA-W.patch [-]
* 0078-brcmfmac-support-4-way-handshake-offloading-for-WPA-.patch [-]
* 0079-nl80211-support-SAE-authentication-offload-in-AP-mod.patch [-]
* 0080-brcmfmac-support-SAE-authentication-offload-in-AP-mo.patch [-]
* 0081-brcmfmac-add-USB-autosuspend-feature-support.patch [v5.7-rc1]
* 0082-brcmfmac-To-support-printing-USB-console-messages.patch [-]
* 0083-brcmfmac-reset-SDIO-bus-on-a-firmware-crash.patch [v5.9-rc1]
* 0084-brcmfmac-fix-for-WPA-WPA2-PSK-4-way-handshake-and-SA.patch [v5.8-rc1]
* 0085-non-upstream-Fix-no-P2P-IE-in-probe-requests-issue.patch [x]
* 0086-brcmfmac-add-54591-PCIE-device.patch
* 0087-brcmfmac-support-DS1-exit-firmware-re-download.patch [x]
* 0088-brcmfmac-fix-43012-insmod-after-rmmod-in-DS1-failure.patch [x]
* 0089-brcmfmac-fix-43012-driver-reload-failure-after-DS1-e.patch [x]
* 0090-brcmfmac-reset-PMU-backplane-all-cores-in-CYW4373-du.patch
* 0091-brcmfmac-do-not-disconnect-for-disassoc-frame-from-u.patch [v5.9-rc1]
* 0092-brcmfmac-Set-pacing-shift-before-transmitting-skb-to.patch [v5.9-rc1]
* 0093-brcmfmac-fix-802.1d-priority-to-ac-mapping-for-pcie-.patch [v5.8-rc1]
* 0094-non-upstream-calling-skb_orphan-before-sending-skb-t.patch [x]
* 0095-non-upstream-workaround-for-4373-USB-WMM-5.2.27-test.patch [x]
* 0096-brcmfmac-disable-command-decode-in-sdio_aos-for-4373.patch [x]
* 0097-brcmfmac-disable-command-decode-in-sdio_aos-for-4339.patch [x]
* 0098-brcmfmac-disable-command-decode-in-sdio_aos-for-43455.patch [x]
* 0099-brcmfmac-support-the-forwarding-packet.patch [-]
* 0100-brcmfmac-add-a-variable-for-packet-forwarding-condit.patch [-]
* 0101-non-upstream-don-t-change-arp-nd-offload-in-multicas.patch [x]
* 0102-non-upstream-revert-don-t-change-arp-nd-offload-in-m.patch [x]
* 0103-brcmfmac-don-t-allow-arp-nd-offload-to-be-enabled-if.patch [-]
* 0104-brcmfmac-fix-permanent-MAC-address-in-wiphy-is-all-z.patch [v5.9-rc1]
* 0105-non-upstream-ignore-FW-BADARG-error-when-removing-no.patch [x]
* 0106-Revert-brcmfmac-validate-ifp-pointer-in-brcmf_txfina.patch [x]
* 0107-Revert-brcmfmac-clean-up-iface-mac-descriptor-before.patch [x]
* 0108-brcmfmac-Support-DPP-feature.patch
* 0109-brcmfmac-move-firmware-path-to-cypress-folder.patch
* 0110-brcmfmac-add-support-for-sof-time-stammping-for-tx-p.patch
* 0111-Revert-brcmfmac-add-support-for-CYW89359-SDIO-chipse.patch [x]
* 0112-brcmfmac-initialize-the-requested-dwell-time.patch [v5.9-rc1]
* 0113-non-upstream-free-eventmask_msg-after-updating-event.patch [x]
* 0114-brcmfmac-fix-invalid-address-access-when-enabling-SC.patch
* 0115-brcmfmac-calling-brcmf_free-when-removing-SDIO-devic.patch
* 0116-brcmfmac-add-a-timer-to-read-console-periodically-in.patch
* 0117-brcmfmac-return-error-when-getting-invalid-max_flowr.patch
* 0118-brcmfmac-Fix-to-add-skb-free-for-TIM-update-info-whe.patch
* 0119-brcmfmac-Fix-to-add-brcmf_clear_assoc_ies-when-rmmod.patch
* 0120-brcmfmac-dump-dongle-memory-when-attaching-failed.patch
* 0121-brcmfmac-update-address-mode-via-test-tool-for-AP-mo.patch
* 0122-brcmfmac-load-54591-firmware-for-chip-ID-0x4355.patch
* 0123-brcmfmac-reserve-tx-credit-only-when-txctl-is-ready-.patch [-]
* 0124-brcmfmac-Fix-interoperating-DPP-and-other-encryption.patch
* 0125-brcmfmac-fix-SDIO-bus-errors-during-high-temp-tests.patch
* 0126-brcmfmac-Add-dump_survey-cfg80211-ops-for-HostApd-Au.patch
* 0127-brcmfmac-Fix-warning-message-after-dongle-setup-fail.patch
* 0128-revert-brcmfmac-set-state-of-hanger-slot-to-FREE-whe.patch
* 0129-brcmfmac-Fix-warning-when-hitting-FW-crash-with-flow.patch

Note: [*] is the upstream tag containing the patch
      [-] means under upstream review
      [x] means no plan to upstream


Hostap Patch List
-----------------
 * 0001-wpa_supplicant-Support-4-way-handshake-offload-for-F.patch
 * 0002-wpa_supplicant-Notify-Neighbor-Report-for-driver-tri.patch
 * 0003-nl80211-Report-connection-authorized-in-EVENT_ASSOC.patch
 * 0004-wpa_supplicant-Add-PMKSA-cache-for-802.1X-4-way-hand.patch
 * 0005-Sync-with-mac80211-next.git-include-uapi-linux-nl802.patch
 * 0006-nl80211-Check-SAE-authentication-offload-support.patch
 * 0007-SAE-Pass-SAE-password-on-connect-for-SAE-authenticat.patch
 * 0008-OpenSSL-Fix-build-with-OpenSSL-1.0.1.patch
 * 0009-non-upstream-Sync-nl80211.h-for-PSK-4-way-HS-offload.patch [x]
 * 0010-nl80211-Support-4-way-handshake-offload-for-WPA-WPA2.patch
 * 0011-AP-Support-4-way-handshake-offload-for-WPA-WPA2-PSK.patch
 * 0012-nl80211-Support-SAE-authentication-offload-in-AP-mod.patch
 * 0013-SAE-Support-SAE-authentication-offload-in-AP-mode.patch
 * 0014-P2P-Fix-P2P-authentication-failure-due-to-AP-mode-4-.patch
 * 0015-AP-Silently-ignore-management-frame-from-unexpected-.patch
 * 0016-DPP-Do-more-condition-test-for-AKM-type-DPP-offload.patch
 * 0017-hostapd-Fix-PMF-connection-issue.patch

Note: [*] is the upstream tag containing the patch
      [x] means no plan to upstream