Cypress Wifi Android FMAC Driver Package - README
=================================================

Package FMAC Version
--------------------
v5.4.18-gamera-android-2

Package Android Version
-----------------------
Android 10.0.0-2.0.0

Release Date
------------
2020-10-05

Description
-----------
This is Cypress's Android brcmfmac driver and firmware support package.
Brcmfmac is an open-source driver project.

The release package includes:
* backports-wireless
	FMAC wireless backports source code
* cypress-fmac-patches
	FMAC Android wireless backports patches
* firmware:
	1. 43455 Firmware/clm_blob files
		Version: 7.45.214
	2. 4354  Firmware/clm_blob files
		Version: 7.35.349.92
	3. 43012 Firmware/clm_blob files
		Version: 13.10.271.245
	4. 4356  Firmware/clm_blob files
		Version: 7.35.180.197
	5. 54591/89459 Firmware/clm_blob files
		Version: 13.35.173
* nvram:
	1. bcm94345wlpagb_p2xx
	2. 43012 Rev C0 WLCSP Murata module EVB
	3. BCM94354 WLBGA iPA, eLNA+switch board with SDIO for production package
	4. CYW4356 1CX WLCSP module for iPA, eLNA board with PCIE for production package 
	5. CYW954591 WLBGA iPA, iLNA board
* aosp-patches:
	Android Open Source Project (AOSP) patches
* utilities:
	wl debugging tool for ARM 32/64 bit.
* build.sh
	The script is for the integration of i.MX8MQ Android build
* 3rd-party
        1. Cirrent Agent 1.50
* README

Test Environment
----------------
* ARM64 (IMX8MQ)
   * Android 10.0.0-2.0.0

Instructions
------------
1. Extract the release package and move cypress folder to $ANDROID_BUILD_TOP/vendor/.

2. Apply or porting the Android patches in $ANDROID_BUILD_TOP/vendor/cypress/patches.

3. Follow build steps in NXP Android_User's_Guide.pdf.
   We build FMAC modules in imx-make.sh becaose Google started to put a limit on the host tools
   used when compiling Android code from Android10.0, but host tools necessary for building FMAC
   modules now cannot be used in the Android build system.
	$ source build/envsetup.sh
	$ lunch evk_8mq-userdebug
	$ ./imx-make.sh

4. Re-flash following images in $OUT folder
	a. boot.img
	b. dtbo-imx8mq.img
	c. vbmeta-imx8mq.img
	d. super.img (vendor+product+system)

Remark
------
1. BT is not integrated in this release.
2. Suspend is not supported in this release but will be in next release.
3. Out of band(HW interrupt) is not supported in this release but will provide HW and SW instruction in next release.

Troubleshooting
---------------
Q1: wl cannot work. The error shows "wl drvier adapter not found"
A1: Please check the wifi is turned ON and the console permission is root.

Q2: How to change to ROOT permission
A2: Execute "adb root" or "su" in uart console mode.

Q3: I cannot push file to vendor or system partition.
A3: Execute "adb root; adb remount" to set write permission first.

Q4: I cannot remount the partition, and error shows "dm_verity is enabled on the system partition."
A4: Execute "adb disable-verity" with adb version 1.0.39 or later version, then reboot the device.

Q5: I cannot find my device in "adb devices"
A5: Please execute adb daemon as root permission.
	Execute "adb kill-server; sudo adb devices", then you can execute "adb devices" to check.

Change Log
[2020-10-12]
* Update FMAC drivers
* Upgrade supporting NXP Android NXP to 10.0.0_2.0.0