CY4541 EZ-PD CCG4 EVK: Hardware Design Files
================================================================================

This directory contains the hardware design files for CY4541 CCG4 EVK. 

The latest HW design files can be found under the current directory. 

Note that this directory also includes archive of the hardware design files
used in the earlier CY4541 kit revisions. All these hardware design files
are located under following directory

.\ARCHIVE

The revision number for a given hardware is etched on the top side of the PCBA
(e.g, 600-60271-01 REV06). Make sure to pick the hardware design files matching
to the PCBA. The schematic file available under each of the hardware directory 
includes the revision history.

================================================================================