--********************************************************************
--** Copyright (c) 2001 Cypress Semiconductor
--** All rights reserved.
--**
--** File Name: cyp15g0401-DXB.bsdl
--** Release: 1.3
--** Last Updated: October 15, 2003
--** Reason: Fixed warnings about port grouping and buffers
--**
--** Function: Quad HOTLink-II Tranceiver, BSDL file for JTAG
--** Part #: CYP15G0401DXB-BGC
--**
--** Notes:
--** IMPORTANT NOTE:
--** Refer to the CYP15G0401DXB-BGC Datasheet at www.cypress.com
--**
--** This BSDL file is 1149.1 compliant.
--**
--** The CYP15G0401DXB-BGC has 12 tri-level select control signals.
--** These signals are SDASEL, SPDSEL, PARCTL, RFMODE etc.
--** The tri state is implemented in the BSDL file as follows:
--** Input vector : 11 => HIGH
--** Input vector : 10 => MID, where 1 is the MSB and 0 is the LSB.
--** Input vector : 00 => LOW.
--** MSB is the higher register no. and LSB is the lower register no.
--**
--** The analog input signal, associated cells, analog input value and
--** the cells capture values are shown in the table below:
--**
--** Analog Input Assoc. Cells Analog Input Voltage, Capture Value
--** (MSB, LSB)
--** ------------ ------------ ------------------------------------
--** SDASEL 171, 170 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** SPDSEL 169, 168 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** PARCTL 167, 166 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** RFMODE 165, 164 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** RXCKSEL 155, 154 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** TXCKSEL 150, 149 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** DECMODE 23, 22 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** FRAMCHAR 20, 19 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** TXMODE(0) 14, 13 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** TXMODE(1) 12, 11 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** RXMODE(0) 10, 9 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--** RXMODE(1) 8, 7 (HIGH, 11), (MID/OPEN, 10), (LOW, 00)
--**
--** Queries ?: Contact DCD Applications at 408-943-2891
--********************************************************************
entity cyp15g0401 is
-- This section identifies the device package selected.
generic (PHYSICAL_PIN_MAP: string:= "BGC_256");
-- This section declares all the ports of the device.
port (
BISTLE : in bit;
BOND_INHn : in bit;
DECMODE : in bit;
FRAMCHAR : in bit;
INA1p : linkage bit;
INA1n : linkage bit;
INA2p : linkage bit;
INA2n : linkage bit;
INB1p : linkage bit;
INB1n : linkage bit;
INB2p : linkage bit;
INB2n : linkage bit;
INC1p : linkage bit;
INC1n : linkage bit;
INC2p : linkage bit;
INC2n : linkage bit;
IND1p : linkage bit;
IND1n : linkage bit;
IND2p : linkage bit;
IND2n : linkage bit;
INSELA : in bit;
INSELB : in bit;
INSELC : in bit;
INSELD : in bit;
LPEN : in bit;
MASTERn : in bit;
OELE : in bit;
PARCTL : in bit;
REFCLKn : in bit;
REFCLKp : in bit;
RFEN : in bit;
RFMODE : in bit;
RXCKSEL : in bit;
RXLE : in bit;
RXRATE : in bit;
SCSEL : in bit;
SDASEL : in bit;
SPDSEL : in bit;
TCLK : in bit;
TDI : in bit;
TMS : in bit;
TRSTZn : in bit;
TXCKSEL : in bit;
TXCLKA : in bit;
TXCLKB : in bit;
TXCLKC : in bit;
TXCLKD : in bit;
TXOPA : in bit;
TXOPB : in bit;
TXOPC : in bit;
TXOPD : in bit;
TXRATE : in bit;
TXRSTn : in bit;
VCC : linkage bit_vector (0 to 31);
GND : linkage bit_vector (0 to 31);
BOE : in bit_vector (0 to 7);
RXMODE : in bit_vector (0 to 1);
TXCTA : in bit_vector (0 to 1);
TXCTB : in bit_vector (0 to 1);
TXCTC : in bit_vector (0 to 1);
TXCTD : in bit_vector (0 to 1);
TXDA : in bit_vector (0 to 7);
TXDB : in bit_vector (0 to 7);
TXDC : in bit_vector (0 to 7);
TXDD : in bit_vector (0 to 7);
TXMODE : in bit_vector (0 to 1);
BOND_ALL : inout bit;
BONDST : inout bit_vector (0 to 1);
RXCLKAp : inout bit;
RXCLKBp : inout bit;
RXCLKCp : inout bit;
RXCLKDp : inout bit;
OUTA1n : linkage bit;
OUTA1p : linkage bit;
OUTA2n : linkage bit;
OUTA2p : linkage bit;
OUTB1n : linkage bit;
OUTB1p : linkage bit;
OUTB2n : linkage bit;
OUTB2p : linkage bit;
OUTC1n : linkage bit;
OUTC1p : linkage bit;
OUTC2n : linkage bit;
OUTC2p : linkage bit;
OUTD1n : linkage bit;
OUTD1p : linkage bit;
OUTD2n : linkage bit;
OUTD2p : linkage bit;
RXCLKAn : inout bit;
RXCLKBn : inout bit;
RXCLKCn : inout bit;
RXCLKDn : inout bit;
RXOPA : out bit;
RXOPB : out bit;
RXOPC : out bit;
RXOPD : out bit;
TDO : out bit;
TXCLKOn : buffer bit;
TXCLKOp : buffer bit;
LFIAn : buffer bit;
LFIBn : buffer bit;
LFICn : buffer bit;
LFIDn : buffer bit;
TXPERA : buffer bit;
TXPERB : buffer bit;
TXPERC : buffer bit;
TXPERD : buffer bit;
RXDA : buffer bit_vector (0 to 7);
RXDB : buffer bit_vector (0 to 7);
RXDC : buffer bit_vector (0 to 7);
RXDD : buffer bit_vector (0 to 7);
RXSTA : buffer bit_vector (0 to 2);
RXSTB : buffer bit_vector (0 to 2);
RXSTC : buffer bit_vector (0 to 2);
RXSTD : buffer bit_vector (0 to 2)
);
use STD_1149_1_1994.all;
attribute COMPONENT_CONFORMANCE of cyp15g0401: entity is "STD_1149_1_1993";
attribute PIN_MAP of cyp15g0401: entity is PHYSICAL_PIN_MAP;
-- This section specifies the pin map for each port. This information
-- is extracted from the port-to-pin map file that was read in using
-- the "read_pin_map" command.
constant BGC_256: PIN_MAP_STRING :=
"BISTLE : F17," &
"BOND_INHn : D17," &
"DECMODE : G17," &
"FRAMCHAR : G19," &
"INA1p : B11," &
"INA1n : A11," &
"INA2p : B14," &
"INA2n : A14," &
"INB1p : B17," &
"INB1n : A17," &
"INB2p : B19," &
"INB2n : A19," &
"INC1p : B1," &
"INC1n : A1," &
"INC2p : B3," &
"INC2n : A3," &
"IND1p : B6," &
"IND1n : A6," &
"IND2p : B9," &
"IND2n : A9," &
"INSELA : D4," &
"INSELB : C4," &
"INSELC : C3," &
"INSELD : D3," &
"LPEN : C19," &
"MASTERn : D20," &
"OELE : G18," &
"PARCTL : C6," &
"REFCLKn : U11," &
"REFCLKp : V11," &
"RFEN : D19," &
"RFMODE : D6," &
"RXCKSEL : F4," &
"RXLE : D18," &
"RXRATE : C18," &
"SCSEL : W12," &
"SDASEL : C7," &
"SPDSEL : D7," &
"TCLK : D1," &
"TDI : C1," &
"TMS : C2," &
"TRSTZn : D2," &
"TXCKSEL : G2," &
"TXCLKA : Y11," &
"TXCLKB : M20," &
"TXCLKC : L3," &
"TXCLKD : Y2," &
"TXOPA : W11," &
"TXOPB : R19," &
"TXOPC : F2," &
"TXOPD : R4," &
"TXRATE : C17," &
"TXRSTn : W10," &
"VCC : (A16, A5, B16, B5, C16, C5, D16, D5, " &
" E20, E19, E18, E17, E4, E3, E2, E1, " &
" T20, T19, T18, T17, T4, T3, T2, T1, " &
" U16, U5, V16, V5, W16, W5, Y16, Y5)," &
"GND : (A13, A8, B13, B8, C13, C8, D13, D8, " &
" H20, H19, H18, H17, H4, H3, H2, H1, " &
" N20, N19, N18, N17, N4, N3, N2, N1, " &
" U13, U8, V13, V8, W13, W8, Y13, Y8)," &
"BOE : (D12, C12, D11, C11, D10, C10, D9, C9)," &
"RXMODE : (C15, D15)," &
"TXCTA : (U15, Y17)," &
"TXCTB : (M18, M17)," &
"TXCTC : (K3, J1)," &
"TXCTD : (V3, U4)," &
"TXDA : (Y14, U12, W14, V14, U14, Y15, W15, V15)," &
"TXDB : (R18, R17, P20, P19, P18, P17, L20, M19)," &
"TXDC : (F3, G4, J3, J4, G3, J2, L4, G1)," &
"TXDD : (U1, U2, U3, V1, V2, W1, Y1, W2)," &
"TXMODE : (C14, D14)," &
"BOND_ALL : U10," &
"BONDST : (V10, V12)," &
"OUTA1n : A12," &
"OUTA1p : B12," &
"OUTA2n : A15," &
"OUTA2p : B15," &
"OUTB1n : A18," &
"OUTB1p : B18," &
"OUTB2n : A20," &
"OUTB2p : B20," &
"OUTC1n : A2," &
"OUTC1p : B2," &
"OUTC2n : A4," &
"OUTC2p : B4," &
"OUTD1n : A7," &
"OUTD1p : B7," &
"OUTD2n : A10," &
"OUTD2p : B10," &
"RXCLKAn : W18," &
"RXCLKAp : Y18," &
"RXCLKBn : L19," &
"RXCLKBp : K20," &
"RXCLKCn : K2," &
"RXCLKCp : L2," &
"RXCLKDn : W4," &
"RXCLKDp : Y4," &
"RXOPA : U18," &
"RXOPB : F19," &
"RXOPC : R2," &
"RXOPD : U9," &
"TDO : C20," &
"TXCLKOn : W9," &
"TXCLKOp : Y9," &
"LFIAn : W17," &
"LFIBn : L18," &
"LFICn : K4," &
"LFIDn : W3," &
"TXPERA : Y12," &
"TXPERB : R20," &
"TXPERC : F1," &
"TXPERD : R3," &
"RXDA : (V19, W20, U17, V18, W19, Y20, Y19, V17)," &
"RXDB : (J18, G20, J20, K17, K18, J19, L17, K19)," &
"RXDC : (P2, P1, K1, L1, M1, M2, M4, M3)," &
"RXDD : (Y7, U7, U6, V6, W6, Y6, V4, Y3)," &
"RXSTA : (V20, U20, U19)," &
"RXSTB : (F20, F18, J17)," &
"RXSTC : (P3, P4, R1)," &
"RXSTD : (V7, W7, V9)";
-- This section defines the grouped ports used to identify system
-- I/O signals that have the special characteristic of using more
-- than one pin to carry a bit of data and for which the allowed
-- states of the pins are restricted
attribute PORT_GROUPING of cyp15g0401: entity is
"Differential_Voltage ((REFCLKp, REFCLKn),"&
"(RXCLKAp, RXCLKAn),"&
"(RXCLKBp, RXCLKBn),"&
"(RXCLKCp, RXCLKCn),"&
"(RXCLKDp, RXCLKDn),"&
"(TXCLKOp, TXCLKOn))";
-- This section specifies the TAP ports.
-- For the TAP TCK port, the parameters in the brackets are:
-- First Field : Maximum TCK frequency.
-- Second Field: Allowable states TCK may be stopped in.
attribute TAP_SCAN_CLOCK of TCLK : signal is (10.0e6, BOTH);
attribute TAP_SCAN_IN of TDI : signal is true;
attribute TAP_SCAN_MODE of TMS : signal is true;
attribute TAP_SCAN_OUT of TDO : signal is true;
-- The following sentence has been commented out while in transition
-- from the earlier revision of the silicon
-- attribute TAP_SCAN_RESET of TRSTZn: signal is true;
-- Specifies the number of bits in the instruction register.
attribute INSTRUCTION_LENGTH of cyp15g0401: entity is 3;
-- Specifies the boundary-scan instructions implemented in the
-- design and their opcodes.
attribute INSTRUCTION_OPCODE of cyp15g0401: entity is
"BYPASS (111)," &
"EXTEST (000)," &
"SAMPLE (001)," &
"IDCODE (010)," &
"USER1 (011)";
-- Specifies the bit pattern that is loaded into the instruction
-- register when the TAP controller passes through the Capture-IR
-- state. The standard mandates that the two LSBs must be "01".
-- The remaining bits are design specific.
attribute INSTRUCTION_CAPTURE of cyp15g0401: entity is "001";
-- Specifies the instruction opcode that is reserved for component
-- test during manufacture.
attribute INSTRUCTION_PRIVATE of cyp15g0401 : entity is
" USER1";
-- Specifies the bit pattern that is loaded into the DEVICE_ID
-- register during the IDCODE instruction when the TAP controller
-- passes through the Capture-DR state.
attribute IDCODE_REGISTER of cyp15g0401: entity is
"0001" & -- 4-bit version number
"1100100000000000" & -- 16-bit part number
"00000110100" & -- 11-bit identity of the manufacturer
"1"; -- Required by IEEE Std 1149.1
-- This section specifies the test data register placed between TDI
-- and TDO for each implemented instruction.
attribute REGISTER_ACCESS of cyp15g0401: entity is
"BYPASS (BYPASS)," &
"BOUNDARY (EXTEST, SAMPLE)," &
"DEVICE_ID (IDCODE)," &
"UTDR1[24] (USER1)";
-- Specifies the length of the boundary scan register.
attribute BOUNDARY_LENGTH of cyp15g0401: entity is 176;
-- The following list specifies the characteristics of each cell
-- in the boundary scan register from TDI to TDO.
-- The following is a description of the label fields:
-- num : Is the cell number.
-- cell : Is the cell type as defined by the standard.
-- port : Is the design port name. Control cells do not
-- have a port name.
-- function: Is the function of the cell as defined by the
-- standard. Is one of input, output2, output3,
-- bidir, control or controlr.
-- safe : Specifies the value that the BSR cell should be
-- loaded with for safe operation when the software
-- might otherwise choose a random value.
-- ccell : The control cell number. Specifies the control
-- cell that drives the output enable for this port.
-- disval : Specifies the value that is loaded into the
-- control cell to disable the output enable for
-- the corresponding port.
-- rslt : Resulting state. Shows the state of the driver
-- when it is disabled.
attribute BOUNDARY_REGISTER of cyp15g0401: entity is
--
-- num cell port function safe
-- [ccell disval rslt]
--
"175 (BC_4, BOE(5), observe_only, X), " &
"174 (BC_4, BOE(4), observe_only, X), " &
"173 (BC_4, BOE(7), observe_only, X), " &
"172 (BC_4, BOE(6), observe_only, X), " &
"171 (BC_4, SDASEL, observe_only, X), " &
"170 (BC_4, SDASEL, observe_only, X), " &
"169 (BC_4, SPDSEL, observe_only, X), " &
"168 (BC_4, SPDSEL, observe_only, X), " &
"167 (BC_4, PARCTL, observe_only, X), " &
"166 (BC_4, PARCTL, observe_only, X), " &
"165 (BC_4, RFMODE, observe_only, X), " &
"164 (BC_4, RFMODE, observe_only, X), " &
"163 (BC_4, INSELB, observe_only, X), " &
"162 (BC_4, INSELA, observe_only, X), " &
"161 (BC_4, INSELC, observe_only, X), " &
"160 (BC_4, INSELD, observe_only, X), " &
"159 (BC_4, TRSTZn, observe_only, X), " &
"158 (BC_1, TXPERC, output2, X), " &
"157 (BC_4, TXOPC, observe_only, X), " &
"156 (BC_4, TXDC(0), observe_only, X), " &
"155 (BC_4, RXCKSEL, observe_only, X), " &
"154 (BC_4, RXCKSEL, observe_only, X), " &
"153 (BC_4, TXDC(1), observe_only, X), " &
"152 (BC_4, TXDC(2), observe_only, X), " &
"151 (BC_4, TXDC(3), observe_only, X), " &
"150 (BC_4, TXCKSEL, observe_only, X), " &
"149 (BC_4, TXCKSEL, observe_only, X), " &
"148 (BC_4, TXDC(4), observe_only, X), " &
"147 (BC_4, TXDC(5), observe_only, X), " &
"146 (BC_4, TXDC(6), observe_only, X), " &
"145 (BC_4, TXDC(7), observe_only, X), " &
"144 (BC_1, LFICn, output2, X), " &
"143 (BC_4, TXCTC(1), observe_only, X), " &
"142 (BC_4, TXCTC(0), observe_only, X), " &
"141 (BC_4, TXCLKC, observe_only, X), " &
"140 (BC_4, *, internal, X), " &
"139 (BC_1, RXCLKCp, output3, X,137,0,Z), " &
"138 (BC_4, RXCLKCp, observe_only, X), " &
"137 (BC_1, *, controlr, 0), " &
"136 (BC_1, RXDC(7), output2, X), " &
"135 (BC_1, RXDC(6), output2, X), " &
"134 (BC_1, RXDC(5), output2, X), " &
"133 (BC_1, RXDC(4), output2, X), " &
"132 (BC_1, RXDC(3), output2, X), " &
"131 (BC_1, RXDC(2), output2, X), " &
"130 (BC_1, RXDC(1), output2, X), " &
"129 (BC_1, RXDC(0), output2, X), " &
"128 (BC_1, RXSTC(0), output2, X), " &
"127 (BC_1, RXSTC(1), output2, X), " &
"126 (BC_1, RXSTC(2), output2, X), " &
"125 (BC_1, RXOPC, output3, X,124,0,Z), " &
"124 (BC_1, *, controlr, 0), " &
"123 (BC_1, TXPERD, output2, X), " &
"122 (BC_4, TXOPD, observe_only, X), " &
"121 (BC_4, TXDD(0), observe_only, X), " &
"120 (BC_4, TXDD(1), observe_only, X), " &
"119 (BC_4, TXDD(2), observe_only, X), " &
"118 (BC_4, TXDD(3), observe_only, X), " &
"117 (BC_4, TXDD(4), observe_only, X), " &
"116 (BC_4, TXDD(5), observe_only, X), " &
"115 (BC_4, TXDD(6), observe_only, X), " &
"114 (BC_4, TXDD(7), observe_only, X), " &
"113 (BC_4, TXCTD(1), observe_only, X), " &
"112 (BC_4, TXCTD(0), observe_only, X), " &
"111 (BC_4, TXCLKD, observe_only, X), " &
"110 (BC_1, LFIDn, output2, X), " &
"109 (BC_1, RXDD(7), output2, X), " &
"108 (BC_1, RXDD(6), output2, X), " &
"107 (BC_1, RXCLKDp, output3, X,105,0,Z), " &
"106 (BC_4, RXCLKDp, observe_only, X), " &
"105 (BC_1, *, controlr, 0), " &
"104 (BC_1, RXDD(5), output2, X), " &
"103 (BC_1, RXDD(4), output2, X), " &
"102 (BC_1, RXDD(3), output2, X), " &
"101 (BC_1, RXDD(2), output2, X), " &
"100 (BC_1, RXDD(1), output2, X), " &
"99 (BC_1, RXDD(0), output2, X), " &
"98 (BC_1, RXSTD(0), output2, X), " &
"97 (BC_1, RXSTD(1), output2, X), " &
"96 (BC_1, RXSTD(2), output2, X), " &
"95 (BC_1, RXOPD, output3, X,124,0,Z), " &
"94 (BC_1, TXCLKOp, output2, X), " &
"93 (BC_1, BONDST(0), output3, X,91,0,Z), " &
"92 (BC_4, BONDST(0), observe_only, X), " &
"91 (BC_1, *, controlr, 0), " &
"90 (BC_4, TXRSTn, observe_only, X), " &
"89 (BC_4, REFCLKp, observe_only, X), " &
"88 (BC_4, SCSEL, observe_only, X), " &
"87 (BC_4, *, internal, X), " &
"86 (BC_1, BOND_ALL, output2, X), " &
"85 (BC_4, BOND_ALL, observe_only, X), " &
"84 (BC_1, BONDST(1), output3, X,91,0,Z), " &
"83 (BC_4, BONDST(1), observe_only, X), " &
"82 (BC_1, TXPERA, output2, X), " &
"81 (BC_4, TXOPA, observe_only, X), " &
"80 (BC_4, TXCLKA, observe_only, X), " &
"79 (BC_4, TXDA(0), observe_only, X), " &
"78 (BC_4, TXDA(1), observe_only, X), " &
"77 (BC_4, TXDA(2), observe_only, X), " &
"76 (BC_4, TXDA(3), observe_only, X), " &
"75 (BC_4, TXDA(4), observe_only, X), " &
"74 (BC_4, TXDA(5), observe_only, X), " &
"73 (BC_4, TXDA(6), observe_only, X), " &
"72 (BC_4, TXDA(7), observe_only, X), " &
"71 (BC_4, TXCTA(0), observe_only, X), " &
"70 (BC_4, TXCTA(1), observe_only, X), " &
"69 (BC_1, RXCLKAp, output3, X,67,0,Z), " &
"68 (BC_4, RXCLKAp, observe_only, X), " &
"67 (BC_1, *, controlr, 0), " &
"66 (BC_1, LFIAn, output2, X), " &
"65 (BC_1, RXDA(7), output2, X), " &
"64 (BC_1, RXDA(6), output2, X), " &
"63 (BC_1, RXDA(5), output2, X), " &
"62 (BC_1, RXDA(4), output2, X), " &
"61 (BC_1, RXDA(3), output2, X), " &
"60 (BC_1, RXDA(2), output2, X), " &
"59 (BC_1, RXDA(1), output2, X), " &
"58 (BC_1, RXDA(0), output2, X), " &
"57 (BC_1, RXOPA, output3, X,124,0,Z), " &
"56 (BC_1, RXSTA(0), output2, X), " &
"55 (BC_1, RXSTA(1), output2, X), " &
"54 (BC_1, RXSTA(2), output2, X), " &
"53 (BC_1, TXPERB, output2, X), " &
"52 (BC_4, TXOPB, observe_only, X), " &
"51 (BC_4, TXCLKB, observe_only, X), " &
"50 (BC_4, TXDB(0), observe_only, X), " &
"49 (BC_4, TXDB(1), observe_only, X), " &
"48 (BC_4, TXDB(2), observe_only, X), " &
"47 (BC_4, TXDB(3), observe_only, X), " &
"46 (BC_4, TXDB(4), observe_only, X), " &
"45 (BC_4, TXDB(5), observe_only, X), " &
"44 (BC_4, TXDB(6), observe_only, X), " &
"43 (BC_4, TXDB(7), observe_only, X), " &
"42 (BC_4, TXCTB(0), observe_only, X), " &
"41 (BC_4, TXCTB(1), observe_only, X), " &
"40 (BC_1, RXCLKBp, output3, X,38,0,Z), " &
"39 (BC_4, RXCLKBp, observe_only, X), " &
"38 (BC_1, *, controlr, 0), " &
"37 (BC_1, LFIBn, output2, X), " &
"36 (BC_1, RXDB(7), output2, X), " &
"35 (BC_1, RXDB(6), output2, X), " &
"34 (BC_1, RXDB(5), output2, X), " &
"33 (BC_1, RXDB(4), output2, X), " &
"32 (BC_1, RXDB(3), output2, X), " &
"31 (BC_1, RXDB(2), output2, X), " &
"30 (BC_1, RXDB(1), output2, X), " &
"29 (BC_1, RXDB(0), output2, X), " &
"28 (BC_1, RXSTB(0), output2, X), " &
"27 (BC_1, RXSTB(1), output2, X), " &
"26 (BC_1, RXSTB(2), output2, X), " &
"25 (BC_1, RXOPB, output3, X,124,0,Z), " &
"24 (BC_4, OELE, observe_only, X), " &
"23 (BC_4, DECMODE, observe_only, X), " &
"22 (BC_4, DECMODE, observe_only, X), " &
"21 (BC_4, BISTLE, observe_only, X), " &
"20 (BC_4, FRAMCHAR, observe_only, X), " &
"19 (BC_4, FRAMCHAR, observe_only, X), " &
"18 (BC_4, BOE(3), observe_only, X), " &
"17 (BC_4, BOE(2), observe_only, X), " &
"16 (BC_4, BOE(1), observe_only, X), " &
"15 (BC_4, BOE(0), observe_only, X), " &
"14 (BC_4, TXMODE(0), observe_only, X), " &
"13 (BC_4, TXMODE(0), observe_only, X), " &
"12 (BC_4, TXMODE(1), observe_only, X), " &
"11 (BC_4, TXMODE(1), observe_only, X), " &
"10 (BC_4, RXMODE(0), observe_only, X), " &
"9 (BC_4, RXMODE(0), observe_only, X), " &
"8 (BC_4, RXMODE(1), observe_only, X), " &
"7 (BC_4, RXMODE(1), observe_only, X), " &
"6 (BC_4, TXRATE, observe_only, X), " &
"5 (BC_4, BOND_INHn, observe_only, X), " &
"4 (BC_4, RXRATE, observe_only, X), " &
"3 (BC_4, RXLE, observe_only, X), " &
"2 (BC_4, LPEN, observe_only, X), " &
"1 (BC_4, RFEN, observe_only, X), " &
"0 (BC_4, MASTERn, observe_only, X) ";
end cyp15g0401;