This is a short step by step instruction to prevent nasty surprises during the usage of the TDA523x Explorer.

Step 1.
-------
   Check if following software is installed on your PC
      # Microsoft .Net Framework 1.1
	
   Check if you have administrative privileges on your PC!
   You need the rights to install following software
      # TDA523x Explorer V2.1.8. or higher
      # USB Driver 
      # Microsoft .Net Framework (if not installed yet)


Step 2.
-------
   Execute the TDA523x Explorer Setup and follow the instructions of the 
   wizard.
   
   !Warning!:
       Do not plug the USB cable before the setup is finished


Step 3.
-------
   If you have already installed an older version of the TDA523x Explorer it is 
   recommended to update also the USB drivers. A complete system clean can be done 
   manually or via the included removal tool  FTClean. After completing the 
   installation process (step 2) a shortcut to this tool is placed 
   in the Programs menu under Infineon Technologies.


Step 4.
-------
   Connect USB cable and install drivers from CD or installation directory


Step 5.
-------
   When you're having a problem with the installation of the USB driver on your windows PC or laptop follow the instructions below:

      1. Plug on USB board on your USB port
      2. Open windows device manager (Start -> Settings -> Control Panel -> System -> Hardware-tab -> Device Manager)
      3. Uninstall USB device/driver marked by "!"
      4. Unplug USB board
      5. Plug on USB board again
      6. Install device driver by user given path
      7. Driver installation is finished


Step 6.
-------
   It may be possible that you have to reconnect the USB cable after you finished
   the driver installation. If not TDA523x Explorer might start with an error.

   !Warning!:
       If you are using a new TDA523x Systemboard Windows will ask you again for
       driver installation. 

   ###########################################################  
   #                                                         #
   # !!You must have administrative privileges on your PC!!  #
   #                                                         #
   ###########################################################