------------------------------------------------------------------------------
FUJITSU USB PROGRAMMER Release Note
                                                     V01L17 (2012-08-22)
------------------------------------------------------------------------------
                              COPYRIGHT(C) FUJITSU SEMICONDUCTOR LIMITED 2012

[VERSION]

   USB-Programmer  (flash.exe)              V01L17


[COMPATIBLE MICROCONTROLLERS]

   This software is compatible with the following microcontrollers.
   
   Caution:
    ( )In the inside, it is Frequency that can be selected by "Crystal Frequency". 
    It uses it to set the best communication timing. 
    If the near frequency can be selected even when 
            the frequency that doesn't exist in the item is used, it will operate. 

   
   8L/8FX
   MB89F202RA			(4MHz)
   MB89F499				(4MHz,8MHz)
   MB95F108B/AM			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F116MA			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F118B/M			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F128/MB			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F136MB			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F146				(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F156M			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F166				(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB95F168MA			(1MHz,2MHz,3MHz,3.58MHz,4MHz,4.19MHz,4.92MHz,5MHz,8MHz,10MHz,12MHz,16MHz,20MHz)

   16LX
   MB90F334				(6MHz)
   MB90F335				(6MHz)
   MB90F337				(6MHz)
   MB90F342E/CE/ES/CES	(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F347				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F349				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F351E/ES/TE/TES	(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F352E/ES/TE/TES	(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F362E/ES/TE/TES	(4MHz,8MHz)
   MB90F387				(4MHz,8MHz)
   MB90F394H			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90MF408			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F428G			(4MHz)
   MB90F438L			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F462				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F482				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F488/B			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F489B			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F497G/MB90F498G	(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F543G/MB90F548G	(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F548GL			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F583C			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F598G			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F803/N			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz,20MHz,24MHz)
   MB90F804				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F809				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F822				(3MHz,4MHz,8MHz,12MHz,16MHz)
   MB90F823				(3MHz,4MHz,8MHz,12MHz,16MHz)
   MB90F867				(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz)
   MB90F882				(4MHz,5MHz,8MHz,10MHz,16MHz,20MHz)
   MB90F883/A/B/C		(4MHz,5MHz,8MHz,10MHz,16MHz,20MHz,24MHz)
   MB90F884/A/B/C		(4MHz,5MHz,8MHz,10MHz,16MHz,20MHz,24MHz)
   MB90F946A			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB90F947A			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB90F949A			(3MHz,4MHz,8MHz,10MHz,12MHz,16MHz,20MHz)
   MB90F952				(3MHz,4MHz,6MHz,8MHz,12MHz,16MHz)
   MB90F983				(5MHz,6MHz,10MHz,12MHz,20MHz,24MHz)

   FR
   MB91F211				(4MHz,5MHz)
   MB91F213				(4MHz,5MHz)
   MB91F223				(4MHz)
   MB91F224				(4MHz)
   MB91F249/S			(4MHz)
   MB91F312A			(10MHz)
   MB91F318R			(10MHz)
   MB91FV319A			(10MHz)
   MB91FV319R			(10MHz)
   MB91F345				(12.5MHz)
   MB91F353/MB91F355	(12.5MHz)
   MB91F467RA			(4MHz)
   MB91F475				(10MHz,20MHz)
   MB91F478				(10MHz,20MHz)
   MB91F479				(10MHz,20MHz)
   MB91F482				(10MHz,20MHz)
   MB91F486				(10MHz,20MHz)
   MB91F487				(10MHz,20MHz)
   MB91F492				(10MHz,20MHz)
   MB91F610 : PROG		(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F610 : FONT		(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F625				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F627				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F637				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F639				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F635A				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F637A				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F639A				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F644				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F647				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F644A				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F647A				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F662				(4MHz,8MHz,16MHz,24MHz,48MHz)
   MB91F668/F669			(4MHz,8MHz,16MHz,24MHz,48MHz)

   16FX
   MB96F348C/H/T		(4MHz,5MHz,8MHz,10MHz,16MHz)


[INSTALLATION PROCEDURE]

  The installation procedure for this software is explained below.

  (1) Double-click "SETUP.EXE".

  (2) Respond to the messages displayed and specify the directory in 
      the product to be installed.
      When the specified directory does not exist, a new one will be
      created.
      Necessary files will be stored in the specified directory.


[UNINSTALLATION PROCEDURE]

  The uninstallation procedure for this software is explained below.

  (1) Open the Control panel and execute "Add/Remove Programs".

  (2) Select this software from the list and click the "Add/Remove"
      button.

  (3) When the maintenance program starts, select "Remove" and click the 
      "Next" button.

  (4) When the "Confirm File Deletion" dialog appears, click the "OK"
      button.

  (5) When the operation ends, the "Maintenance Complete" dialog appears.


[history]
 2012-08-22 V01L17
  Windows 7 support bug fix

 2011-09-14 V01L16
  Windows 7 support

 2010-08-02 V01L15b02
	add MB90F337
	add MB91F486
	add MB91F625
	add MB91F627
	add MB91F635A
	add MB91F637A
	add MB91F639A
	add MB91F644A
	add MB91F647A
	add MB91F668/F669

2009.06.29 V01L15b01 
	add MB91F492

2009.05.27 V01L14 
	add MB90F362E/ES/TE/TES
	add MB90F883C
	change FLASH area display
	add IntelHex format
	add CheckSum function

2009.01.28 V01L13 
	change suffix from MB90F884/A to MB90F884/A/B/C
	change suffix from MB90F883/A to MB90F883/A/B
	Correction of registration MB91F249/S
2008.09.12 V01L12
	add MB90F335, MB90F912, MB90F997, MB91F224
2008.07.08 V01L11
	add MB95F116M, MB95F166, MB91F312A
2008.06.30 V01L10 
	add MB89F202RA, MB90F351E/ES/TE/TES, MB90F352E/ES/TE/TES
	MB90F952, MB90F342E/CE/ES/CES, MB91F610,MB91F644,MB96F348C/H/T
	del MB89F202
2008.03.07 V01L09 
	add MB90F803/N, MB90F883/A, MB91F482, MB91F637, MB91F662
	change suffix MB90F488/B, MB90F884/A
2007.09.10 V01L08 
	add MB95F176J, MB90F809, MB91F211, MB91F487, MB91F639, MB91F647
	Explanation of Pin9 and 10 of BGM Connector is changed.
2007.03.16 V01L07
	add MB91F356B
	add "3-4.BGM adaptor circuit chart"
	add "5-4.Special specification"
	add "6.SECURITY FUNCTION"
2007.01.22 V01L0704
	MB90F822
2007.01.18 V01L0703
	MB90F438L, MB90F548GL, MB90F583C
2006.12.13 V01L0702
	MB91F249/S
2006.10.26 V01L0701
	MB95F146, MB95F156/M, MB95F168/M
2006.09.13 V01L06
	Add MB91F319R
2006.09.08 V01L06
	Add MB91F213
2006.08.09 V01L06
	Add MB91F475/F478
2006.05.25 V01L05
	Add MB91F479
2006.07.05 V01L04 
	Change EXAMPLE OF CONNECTION FOR ON-BOARD REPROGRAMMING BY 
	PROGRAMMER
2006.04.04 V01L03
	Add MB90F428G
2006.03.16 V01L02
	It changes to the HELP form.
2005.03.01 V01L01
	NEW