Notes for Use of Fujitsu Flash MCU Programmer for FMC8L MB89F202RA

December 2008
Fujitsu Limited

This software writes data to flash memory contained in the Fujitsu microcontroller with flash memory
from a personal computer.

1.  System Requirements
	Personal computer:  IBM PC/AT compatibles with RS-232C port
	OS:  Japanese and English versions of Windows 2000 SP3, Windows XP SP2
	Memory:  Memory capacity more than OS requires
	Available disk space:  10 MB or more

	NOTICE:  The operations of all models that meet the above conditions may not be ensured.

2.  Explanation of Files Provided
	setup.exe:         Installer execution file
	Readme8Lj202.txt:  Document file(english)
	Readme8Lj202.txt:  Document file(japanese)

3.  Installation Procedure
3.1  Outline of Installer
	This installer includes the program for storage of installation information, called Windows 
	Installer.  Windows Installer is installed to the personal computer on which Windows 2000 or 
	earlier OS runs.  In this case, restart may be required.
	If the installation of Windows Installer is completed or Windows Installer has been preinstalled, 
	the installation of this software is started.  Before installation, be sure to uninstall the old
	version and reboot.

3.2  Setup Mode
	When Installer is started in the Setup mode, the window for the selection of "All" or "Custom"
	appears:
	"All" is the standard setup and should be selected.
	"Custom" should be selected only when setting the installation folder in a special place.
	Installation to a deep hierarchy of the folder may prevent Installer from operating.  The full
	path of the folder should be specified within 200 characters and the full path of the 8.3-format
	folder within 100 characters.
	When the operation is continued according to directions from Installer, the installation is 
	completed and the shortcut to this software is created as a program on the Start menu.

4. Uninstallation Procedure
	Open the "Start"-"Settings" "Control Panel" and start "Add/Remove Programs."  Select and 
	delete "FUJITSU FLASH MCU Programmer FMC8L MB89F202."  After uninstallation, the 
	installation folder may be left.  In this case, delete the folder manually.  This software is 
	typically installed to Fujitsu\Fujitsu Flash MCU Programmer\FMC8L MB89F202 below Program Files.
	No registry is used.

5. Cautions
	No operation of this software on the NEC PC98 series of personal computers is assured.
	This software is not intended for writing to mass-produced products.

Note:  Windows is the product name of Microsoft.



-------------------------------------------------------------------------------
History of update

V00L02
	NEW	MB89F202RA

V00L01
    bug fix

V00L00
	NEW	MB89F202