Notes for Use of Fujitsu Flash MCU Programmer for FMC-8L(FLASH)

October 2004
Fujitsu Limited

This software writes data to flash memory contained in the Fujitsu microcontroller with flash memory
from a personal computer.

1.  System Requirements
	Personal computer:  IBM PC/AT compatibles with RS-232C port
	OS:  Japanese and English versions of Windows 98 SE, Windows ME, 
		Windows NT4.0 SP6, Windows 2000 SP3, Windows XP SP1
	Memory:  Memory capacity more than OS requires
	Available disk space:  10 MB or more

	NOTICE:  The operations of all models that meet the above conditions may not be ensured.

2.  Explanation of Files Provided
	PCW8Fsetup.exe:  Installer execution file
	Readme8Fe.txt:  Document file(english)
	Readme8Fj.txt:  Document file(japanese)

3.  Installation Procedure
3.1  Outline of Installer
	This installer includes the program for storage of installation information, called Windows 
	Installer.  Windows Installer is installed to the personal computer on which Windows 2000 or 
	earlier OS runs.  In this case, restart may be required.
	If the installation of Windows Installer is completed or Windows Installer has been preinstalled, 
	the installation of this software is started.  Before installation, be sure to uninstall the old
	version and reboot.

3.2  Setup Mode
	When Installer is started in the Setup mode, the window for the selection of "All" or "Custom"
	appears:
	"All" is the standard setup and should be selected.
	"Custom" should be selected only when setting the installation folder in a special place.
	Installation to a deep hierarchy of the folder may prevent Installer from operating.  The full
	path of the folder should be specified within 200 characters and the full path of the 8.3-format
	folder within 100 characters.
	When the operation is continued according to directions from Installer, the installation is 
	completed and the shortcut to this software is created as a program on the Start menu.

4. Uninstallation Procedure
	Open the "Start"-"Settings" "Control Panel" and start "Add/Remove Programs."  Select and 
	delete "FUJITSU FLASH MCU Programmer for FMC8L(FLASH)."  After uninstallation, the 
	installation folder may be left.  In this case, delete the folder manually.  This software is 
	typically installed to Fujitsu\Fujitsu Flash MCU Programmer\FMC8L(FLASH) below Program Files.
	No registry is used.

5. Cautions
	No operation of this software on the NEC PC98 series of personal computers is assured.
	This software is not intended for writing to mass-produced products.

Note:  Windows is the product name of Microsoft.



-------------------------------------------------------------------------------
History of update

V01L08a
	renew installer

V01L08
	add 217

V01L07
	add 499

V01L06
	CRC checking is added
	internal Motorola S decoder is added
	continuously writeing mode is deleted
	A temporary(binary) file is not created
	popup menu is changed

V01L05
	operation on windows95 is no longer guaranteed.
	add 051.
	add continuously write mode.

V01L04
	make temporary file in everytime.
	change DOWNLOAD sequence.

V01L03
	add 538/L(3V product).