Notes for Use of Fujitsu Flash MCU Programmer for FMC-8FX

June 2009
Fujitsu Limited

This software writes data to flash memory contained in the Fujitsu microcontroller with flash memory
from a personal computer.

1.  System Requirements
	Personal computer:  IBM PC/AT compatibles with RS-232C port
	OS:  Japanese and English versions of Windows 2000 SP3, Windows XP SP2
	Memory:  Memory capacity more than OS requires
	Available disk space:  10 MB or more

	NOTICE:  The operations of all models that meet the above conditions may not be ensured.

2.  Explanation of Files Provided
	setup.exe:       Installer execution file
	Readme8FXe.txt:  Document file(english)
	Readme8FXj.txt:  Document file(japanese)

3.  Installation Procedure
3.1  Outline of Installer
	This installer includes the program for storage of installation information, called Windows 
	Installer.  Windows Installer is installed to the personal computer on which Windows 2000 or 
	earlier OS runs.  In this case, restart may be required.
	If the installation of Windows Installer is completed or Windows Installer has been preinstalled, 
	the installation of this software is started.  Before installation, be sure to uninstall the old
	version and reboot.

3.2  Setup Mode
	When Installer is started in the Setup mode, the window for the selection of "All" or "Custom"
	appears:
	"All" is the standard setup and should be selected.
	"Custom" should be selected only when setting the installation folder in a special place.
	Installation to a deep hierarchy of the folder may prevent Installer from operating.  The full
	path of the folder should be specified within 200 characters and the full path of the 8.3-format
	folder within 100 characters.
	When the operation is continued according to directions from Installer, the installation is 
	completed and the shortcut to this software is created as a program on the Start menu.

4. Uninstallation Procedure
	Open the "Start"-"Settings" "Control Panel" and start "Add/Remove Programs."  Select and 
	delete "FUJITSU FLASH MCU Programmer for FMC8FX."  After uninstallation, the 
	installation folder may be left.  In this case, delete the folder manually.  This software is 
	typically installed to Fujitsu\Fujitsu Flash MCU Programmer\FMC8FX below Program Files.
	No registry is used.

5. Cautions
	No operation of this software on the NEC PC98 series of personal computers is assured.
	This software is not intended for writing to mass-produced products.

Note:  Windows is the product name of Microsoft.



-------------------------------------------------------------------------------
History of update
V01L09
	add CheckSum function

V01L08
	Suffix change

V01L07
	COM PORT 1-20
	ADD MB95F116M,MB95F166

V01L06
	correct chipdef.ini

V01L05
	Internal motorola S decoder specifiction is added.
	When operation ends, Com Port is opened. 
	
V01L04
	operation on WindowsNT is no longer guaranteed.
	
	ADD MB95F176J

V01L03
	ADD MB95F146, MB95F156/M, MB95F168/M

V01L02
	ADD MB95F136H

V01L01
	NEW
		MB95F108/H, MB95F118/H, MB95F128H