Notes for Use of CYPRESS Flash MCU Programmer for FMC-16FX
January 2016
Cypress Semiconductor Corp.

This software writes data to flash memory contained in the Cypress microcontroller with flash memory from a personal computer.

1. Operating Environment

    Required equipment :
     - IBM PC compatible machine equipped with the RS-232C port
     - RS-232C cable (commercial item)
    OS :
     - The Japanese version and English version of Windows XP/Vista/7
     * There is fault that some characters are not displayed correctly, in Windows Vista.
       However, we are checking that the program is performing normal operation.
    Memory size :
     - More than the memory quantity that OS recommends
    Hard disk :
     - (Availability) Not less than 10 MB

    NOTICE : The operations of all models that meet the above conditions may not be ensured.

2. Explanation of Files Provided

    setup.exe:        Installer executable file
    Readme16FXe.txt:  Document file(English)
    Readme16FXj.txt:  Document file(Japanese)

3. Installation

    An installation procedure is shown below.

    1) Run setup.exe.
    2) The [Next] button will be clicked if the screen of "Welcome" is displayed.
    3) The screen of "Choose Install Location" is displayed.
       Usually, please click the [Next] button.
       Please click the [Brows] button and specify a directory to change an install destination under a certain situation.
    4) The screen of "Installing" is displayed and installation starts.
    5) The [Finish] button will be clicked if the screen of "Completed" is displayed.
    With this, installation is completed.

    This software will be registered into the start menu of Windows if installation is completed.

    When reinstalling, you should install, after uninstalling this software.
    If reinstallation is tried without uninstalling, the screen which checks file deletion is displayed.
    Please click and quit [Cancel] at this time.
    However, [OK] can also be clicked and uninstalled.

    When upgrading, you should install, after uninstalling this software.
    
4. Uninstallation

    An uninstallation procedure is shown below.

    1) Click the [Start] button and select "Control Panel".
    2) In Control Panel, Select "Add or Remove Programs". 
    3) Select "CYPRESS FLASH MCU Programmer for FMC16FX." 
    4) This software is deleted clicking [Remove] button. 
    
     * After uninstallation, the installation folder may be left.
       In this case, delete the folder manually.
       This software is typically installed to Cypress\CYPRESS Flash MCU Programmer\FMC16FX below Program Files.
     * This software is not using registry.

5. Cautions
    No operation of this software on the NEC PC98 series of personal computers is assured.
    
    The PC programming software has the possibility of receiving the influence by the communications cable, 
    the outside environment, and the PC. Therefore, please evaluate it enough when you use the software. 
    Please use programming systems of programmer venders when you write two or more devices at the same time.

Note:  Windows is the product name of Microsoft.



-------------------------------------------------------------------------------
History of update

V01L18
    change the name and logo of company from SPANSION to CYPRESS

V01L17
    correspond to Intel-Hex format

V01L16
    change the name and logo of company from FUJITSU to SPANSION

V01L15
    change chip name from MB96F6xxAA/RA to MB96F6xxA/R
    change chip name from MB96F6xxRA to MB96F6xxR

@@add MB96F633A/R
@@add MB96F635A/R
@@add MB96F643A/R
@@add MB96F645A/R
@@add MB96F653A/R
@@add MB96F655A/R
@@add MB96F693A/R
@@add MB96F695A/R
@@add MB96F6A5A/R
@@add MB96F6B5A/R
@@add MB96F6C5A/R
    add MB96F8D3K3/4
    add MB96F8D3KD/E/F/U/V/W
    add MB96F8E3K3/4
    add MB96F8E3KD/E/F/U/V/W
    add MB96F8D5K3/4
    add MB96F8D5KD/E/F/U/V/W
    add MB96F8E5K3/4
    add MB96F8E5KD/E/F/U/V/W

 @ add sector select function for MB96610 series
 @ change trimming data area for MB96800 series

V01L14
    add MB96F612AA/RA
    add MB96F613AA/RA
    add MB96F615AA/RA
    add MB96F622AA/RA
    add MB96F623AA/RA
    add MB96F625AA/RA
    add MB96F636RA
    add MB96F637RA
    add MB96F646RA
    add MB96F647RA
    add MB96F656RA
    add MB96F657RA
    add MB96F696RA
    add MB96F6A6RA
    add MB96F6B6RA
    add MB96F6C6RA

V01L13
    add MB96F675AA/RA
    add MB96F673AA/RA
    add MB96F685AA/RA
    add MB96F683AA/RA

V01L12
    If there are out of flash area data in the mhx file,the error message is displayed.

V01L11
    The bug of the kernel was fixed.
    MB96F343D/F
    MB96F345D/F

V01L10
    add MB96F343D/F
    add MB96F345D/F

V01L09
    add MB96F378C/H/T
    The whole sentence of this document was improved.

V01L08
    add MB96F313A/R/Y
    add MB96F315A/R/Y
    add MB96F336U
    add MB96F353A/R
    add MB96F355A/R/Y

V01L07
    correspond to Intel-Hex format
    Addition of Checksum function

V01L06
    Addition of security release function
    add MB96F385R/Y
    add MB96F395R/Y

V01L05
    add MB96F388H,MB96F389R

V01L04
    add MB96F379R/Y(4MHz,5MHz,8MHz,10Mhz,16MHz)

V01L03
    Internal motorola S decoder specifiction is added.

V01L02
    change chip name from MB96F346R/YxA to MB96F346A/R/Y
    change chip name from MB96F347R/YxA to MB96F347A/R/Y
    change chip name from MB96F348H/TxA to MB96F348C/H/T
    change chip name from MB96F348R/YxA to MB96F348A/R/Y
    change chip name from MB96F386R/YxA to MB96F386R/Y
    change chip name from MB96F387R/YxA to MB96F387R/Y
    
    add MB96F326A/R/Y(4MHz,5MHz,8MHz,10Mhz,16MHz)
    add MB96F338R/U/Y(4MHz,5MHz,8MHz,10Mhz,16MHz)
    add MB96F356A/R/Y(4MHz,5MHz,8MHz,10Mhz,16MHz)
    
V01L01
    change chip name from MB96F346R/Y to MB96F346R/YxA
    change chip name from MB96F347R/Y to MB96F347R/YxA
    change chip name from MB96F348H/T to MB96F348H/TxA
    change chip name from MB96F348R/Y to MB96F348R/YxA
    change chip name from MB96F386R/Y to MB96F386R/YxA
    change chip name from MB96F387R/Y to MB96F387R/YxA
    
    add 5,8,10,16MHz-OSC for MB96F347R/YxA
    add 5,8,10,16MHz-OSC for MB96F348R/YxA

V01L00
    add MB96F346R/Y
    add MB96F347R/Y
    add MB96F348H/T
    add MB96F348R/Y
    add MB96F386R/Y
    add MB96F387R/Y

-------------------------------------------------------------------------------