==========================================================================
                   Template Project for MB91265 Series
==========================================================================
                   Fujitsu Microelectronics Europe GmbH                       
                     Pittlerstrasse 47, 63225 Langen                    
                    Tel.: ++49 (6103) 690-0, Fax -122                     
                                                            
 The following  software  is for  demonstration  purposes only.  It is not
 fully  tested, nor validated  in order  to fullfill  its task  under  all
 circumstances.  Therefore,  this software or  any part of it must only be
 used in an evaluation laboratory environment.                        
 This software is subject to the rules of our standard DISCLAIMER, that is
 delivered with our  SW-tools on the Fujitsu Microcontrollers CD 
 (V3.0 or higher "\START.HTM") or on our Internet Page:
 http://www.emea.fujitsu.com  
==========================================================================

History
Date      Ver     Author  Softune     Description
20.03.07  1.0     CHa     V60L05      first version based on template V1.4

==========================================================================

This is a project template for the MB91265 Series. It includes some basic 
settings for e.g. Linker, C-Compiler which must be checked and modified in 
detail, corresponding to the user application.

This is a simple demonstration for the MAC unit of the MB91265 Series.
It simply calculates the average of some values, first using the MAC unit,
and then in 'pure' C-code. To show the time needed for the calculations,
the pin PDRG_PG1 (pin 42 on MB91F267) is used as status pin to connect an
oscilloscope.

In mac.h, some useful macros can be found to ease up the programming of
the MAC unit. Please refer to the comments in the mac.h and main.c files
for more usage details.