==========================================================================
                   Template Project for MB90895 Series
==========================================================================
                   Fujitsu Microelectronics Europe GmbH                       
                 http://emea.fujitsu.com/microelectronics 
                                                            
 The following  software  is for  demonstration  purposes only.  It is not
 fully  tested, nor validated  in order  to fullfill  its task  under  all
 circumstances.  Therefore,  this software or  any part of it must only be
 used in an evaluation laboratory environment.                        
 This software is subject to the rules of our standard DISCLAIMER, that is
 delivered with our  SW-tools on the Fujitsu Microcontrollers CD 
 (V3.4 or higher "\START.HTM") or on our Internet Pages:
 http://www.fme.gsdc.de/gsdc.htm
 http://emea.fujitsu.com/microelectronics 
==========================================================================
               
History
Date      Ver   Author  Softune   Description
09.07.03  1.00  MWi     V30L32    First Version
==========================================================================


This is a project for EEPROM simulation. Please refer to application
note: mcu-an-390094-e-v11-eeprom_emulation_dual_op_flash.pdf


==========================================================================

Important:
The evaluation chip for the MB90895 series is the MB90V495 !

Note:
MB90895series uses a hardwired Reset-vector fixed to 0xFFE000
see Softune Workbench: 
  Project - Setup Project - Linker
  Category: Disposition/Connection - Set Section
  RAM/ROM Area: Specify in Address: Section CODE_START @ 0xFFE000