Matching the CyUsb.sys Driver to USB Devices
Force WindowsXP to use the CYUSB.SYS driver with the device.
Connect the device to the PC
If Windows prompts for a driver or indicates that it needs a driver
Select No, not this time
Click Next
Select Install from a list or specific location (Advanced)
Check the box Include this location in the search
Click Browse
Navigate to the directory containing CYUSB.SYS
CYUSB.INF should be automatically placed in the File name field
Click OK
Click Next
Click Finish
Click Close
If Windows does not prompt for a driver, it has already matched the device to a driver itself. In this case, you will need to see if the CYUSB.SYS driver was selected and, if not, manually instruct Windows to use that driver.
Right-click My Computer and select the Manage menu item.
In the Computer Management window, select Device Manager
In the right window pane, click the + icon next to Universal Serial Bus controllers
Locate your device in the list and double click on it
Select the Driver tab in the Properties dialog that comes up
Click on the Driver Details button.
If the displayed driver file is CYUSB.SYS, Windows has already matched the device to this driver and you should click OK and Cancel. If not, proceed with the remaining steps.
Click OK
Click Update Driver
Select No, not this time
Click Next
Select Install from a list or specific location (Advanced)
Click Next
Select Don't search. I will choose the driver to install.
Click Next
Click Have Disk
Click Browse
Navigate to the directory containing CYUSB.SYS
CYUSB.INF should be automatically placed in the File name field
Click Open
Click OK
Click Next
Click Finish
Click Close
Don't re-boot your system if Windows suggests that you must. You may need to unplug and re-plug your device, however.