+----------------+
                                                           |IO95200  -V01L02|
                                                           +----------------+























                           SAMPLE I/O REGISTER FILES
                      FOR F2MC-8FX FAMILY MB95200 SERIES

                                 USERS MANUAL

                      FUJITSU MICROELECTRONICS LIMITED

                                    V01L02

Preface

  The sample I/O register files for MB95200 series declares and defines
  symbols, thereby enabling the I/O registers
  of the F2MC-8FX family to be handled as Asembler symbols.
  This manual describes the configuration of the I/O register files,
  symbol declaration and definition.




Items to note before using I/O register files

  - The I/O register files are intended for specific series of
    F2MC-8FX family.
    Before applying these programs to any other series of MB95200 series,
    therefore, be sure to modify the I/O register files.

  - When a program for I/O register operation is coded, the I/O register
    access sequence and timing must be considered. Please refer to the
    related hardware manuals.

  - The I/O register files are provided as valuable aids in developing the
    application programs for MB95200 series. In practice, however,
    some of these programs may need be modified depending on the
    target system. Before using any of them, therefore, be sure to verify
    the actual operation of the program.

  - FUJITSU MICROELECTRONICS may assume no liability for errors in the I/O
    register files and no responsibility for correcting errors immediately
    even if they are found.

Reference manuals

  I/O register files for MB95200 series (V01L02) are made based on the
  following manuals.

    - MB95200 series Hardware Manual(CM26-10120-1E)

Contents

CHAPTER 1  CONFIGURATION OF I/O REGISTER FILES

CHAPTER 2  USAGE OF I/O REGISTER FILES

CHAPTER 3  DECLARATION OF I/O REGISTER DECLARATION FILES

CHAPTER 4  SYMBOL AND MACRO NAMES USED IN I/O REGISTER DECLARATION FILES
           FOR MB95200 SERIES

CHAPTER 1  CONFIGURATION OF I/O REGISTER FILES

 ${FETOOL}             (Directory set in environment variable FETOOL)
  +-lib
    +-896
      +-include
        +-sample
          +-MB95200
            +-_f2mc8fx.h (I/O register declaration file)
            |
            +-mb95200.h (I/O register declaration file for MB95200 series)
            |
            +-_f2mc8fx_a.asm (I/O register definition file)

  - I/O register declaration file

    This file declares all the associated I/O register symbols (symbols
    corresponding to I/O registers).
    Please include this file when coding a program that handles associated
    I/O registers.

  - I/O register declaration file for MB95200 series

    This file declares all the structure types corresponding to I/O registers
    for MB95200 series.

  - I/O register definition file for each I/O register

    This file defines each the associated I/O register symbol and specifies
    arrangement address.

CHAPTER 2  USAGE OF I/O REGISTER FILES

  (1) Please assemble the I/O register definition file with the CPU option
      of using MB number.
        example:  > fasm896s -cpu mb***** _f2mc8fx_a.asm

  (2) When you describe the application program which refers to the I/O
      registers, please include the I/O register declaration file.

        example:  #include "_f2mc8fx.h"

                         .....
                    SETB  _IO_TCCS_MODE
                         .....

  (3) Please assemble the application program file with the CPU option of
      using MB number.

        example:  > fasm896s -cpu mb***** sample.asm

        Note: When the MB number of the specified CPU option cannot be used
              for the I/O register file, the following messages are output.

                #error "The I/O register file of the specified CPU option
                        does not exist"

  (4) Please link the I/O register definition object file and the application
      program object file.

        example: > flnk896s -cpu mb***** -o sample.abs *.obj

CHAPTER 3  DECLARATION OF I/O REGISTER DECLARATION FILES

  Each I/O register declaration file declares the symbols corresponding to
  I/O register names and bit names as follows:

    - The I/O register symbols that can be accessed in bits are declared in
      bit type.

    - The I/O register symbols that must be accessed in 1, 2 or 4 bytes
      are declared in byte type.

    - Basically, each symbol name is declared in the form of the
      corresponding I/O  register name plus '_IO_'.
      (However, for access convenience, two or more I/O registers may be
       declared by one symbol name.)

    - A bit symbol name is declared by the corresponding bit name.
      (some bits are declared in one symbol name for access convenience)


  [Example]  Declaration for I/O register PDR0

    - I/O register structure

          7       6       5       4       3       2       1       0    bit No.
      +-------+-------+-------+-------+-------+-------+-------+-------+
      |   P07 |   P06 |   P05 |   P04 |   P03 |   P02 |   P01 |   P00 | PDR0
      +-------+-------+-------+-------+-------+-------+-------+-------+

    - Contents of declaration

        #ifdef __IO_DEFINE
			.SECTION	IO_PDR0,IO,LOCATE=0x0
        _IO_PDR0:
        __pdr0: .res.b 0
        PDR0 .equ 0x00000000
        _IO_PDR0_PD00 .RES.i  1
        _IO_PDR0_PD01 .RES.i  1
        _IO_PDR0_PD02 .RES.i  1
        _IO_PDR0_PD03 .RES.i  1
        _IO_PDR0_PD04 .RES.i  1
        _IO_PDR0_PD05 .RES.i  1
        _IO_PDR0_PD06 .RES.i  1
        _IO_PDR0_PD07 .RES.i  1
        #endif

                      .GLOBAL _IO_PDR0
                      .GLOBAL __pdr0
                      .GLOBAL PDR0
                      .GLOBAL _IO_PDR0_PD00
                      .GLOBAL _IO_PDR0_PD01
                      .GLOBAL _IO_PDR0_PD02
                      .GLOBAL _IO_PDR0_PD03
                      .GLOBAL _IO_PDR0_PD04
                      .GLOBAL _IO_PDR0_PD05
                      .GLOBAL _IO_PDR0_PD06
                      .GLOBAL _IO_PDR0_PD07

CHAPTER 4  SYMBOL AND MACRO NAMES USED IN I/O REGISTER DECLARATION FILES
           FOR MB95200 SERIES

  I/O Register Name : PDR0                    Address : 0x0
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PDR0                                                  
  Bit             _IO_PDR0_P00                                              
                  _IO_PDR0_P01                                              
                  _IO_PDR0_P02                                              
                  _IO_PDR0_P03                                              
                  _IO_PDR0_P04                                              
                  _IO_PDR0_P05                                              
                  _IO_PDR0_P06                                              
                  _IO_PDR0_P07                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : DDR0                    Address : 0x1
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_DDR0                                                  
  Bit             _IO_DDR0_P00                                              
                  _IO_DDR0_P01                                              
                  _IO_DDR0_P02                                              
                  _IO_DDR0_P03                                              
                  _IO_DDR0_P04                                              
                  _IO_DDR0_P05                                              
                  _IO_DDR0_P06                                              
                  _IO_DDR0_P07                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : PDR1                    Address : 0x2
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PDR1                                                  
  Bit             _IO_PDR1_P12                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : DDR1                    Address : 0x3
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_DDR1                                                  
  Bit             _IO_DDR1_P12                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : WATR                    Address : 0x5
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WATR                                                  
  Bit             _IO_WATR_MWT0                                             
                  _IO_WATR_MWT1                                             
                  _IO_WATR_MWT2                                             
                  _IO_WATR_MWT3                                             
                  _IO_WATR_SWT0                                             
                  _IO_WATR_SWT1                                             
                  _IO_WATR_SWT2                                             
                  _IO_WATR_SWT3                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register. 


  I/O Register Name : SYCC                    Address : 0x7
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_SYCC                                                  
  Bit             _IO_SYCC_DIV0                                             
                  _IO_SYCC_DIV1                                             
                  _IO_SYCC_SRDY                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : STBC                    Address : 0x8
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_STBC                                                  
  Bit             _IO_STBC_MRDY                                             
                  _IO_STBC_MCRDY                                            
                  _IO_STBC_SCRDY                                            
                  _IO_STBC_TMD                                              
                  _IO_STBC_SRST                                             
                  _IO_STBC_SPL                                              
                  _IO_STBC_SLP                                              
                  _IO_STBC_STP                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : RSRR                    Address : 0x9
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_RSRR                                                  
  Bit             _IO_RSRR_SWR                                              
                  _IO_RSRR_HWR                                              
                  _IO_RSRR_PONR                                             
                  _IO_RSRR_WDTR                                             
                  _IO_RSRR_EXTS                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register. 


  I/O Register Name : TBTC                    Address : 0xa
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_TBTC                                                  
  Bit             _IO_TBTC_TCLR                                             
                  _IO_TBTC_TBC0                                             
                  _IO_TBTC_TBC1                                             
                  _IO_TBTC_TBC2                                             
                  _IO_TBTC_TBC3                                             
                  _IO_TBTC_TBIE                                             
                  _IO_TBTC_TBIF                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : WPCR                    Address : 0xb
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WPCR                                                  
  Bit             _IO_WPCR_WCLR                                             
                  _IO_WPCR_WTC0                                             
                  _IO_WPCR_WTC1                                             
                  _IO_WPCR_WTC2                                             
                  _IO_WPCR_WTIE                                             
                  _IO_WPCR_WTIF                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : WDTC                    Address : 0xc
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WDTC                                                  
  Bit             _IO_WDTC_WTE0                                             
                  _IO_WDTC_WTE1                                             
                  _IO_WDTC_WTE2                                             
                  _IO_WDTC_WTE3                                             
                  _IO_WDTC_HWWDT                                            
                  _IO_WDTC_CSP                                              
                  _IO_WDTC_CS0                                              
                  _IO_WDTC_CS1                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register. 


  I/O Register Name : SYCC2                   Address : 0xd
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_SYCC2                                                 
  Bit             _IO_SYCC2_MCRE                                            
                  _IO_SYCC2_SCRE                                            
                  _IO_SYCC2_MOSCE                                           
                  _IO_SYCC2_SOSCE                                           
                  _IO_SYCC2_RCS0                                            
                  _IO_SYCC2_RCS1                                            
                  _IO_SYCC2_RCM0                                            
                  _IO_SYCC2_RCM1                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : PDR6                    Address : 0x16
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PDR6                                                  
  Bit             _IO_PDR6_P62                                              
                  _IO_PDR6_P63                                              
                  _IO_PDR6_P64                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : DDR6                    Address : 0x17
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_DDR6                                                  
  Bit             _IO_DDR6_P62                                              
                  _IO_DDR6_P63                                              
                  _IO_DDR6_P64                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : PDRF                    Address : 0x28
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PDRF                                                  
  Bit             _IO_PDRF_PF0                                              
                  _IO_PDRF_PF1                                              
                  _IO_PDRF_PF2                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : DDRF                    Address : 0x29
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_DDRF                                                  
  Bit             _IO_DDRF_PF0                                              
                  _IO_DDRF_PF1                                              
                  _IO_DDRF_PF2                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : PDRG                    Address : 0x2a
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PDRG                                                  
  Bit             _IO_PDRG_PG1                                              
                  _IO_PDRG_PG2                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : DDRG                    Address : 0x2b
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_DDRG                                                  
  Bit             _IO_DDRG_PG1                                              
                  _IO_DDRG_PG2                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : PUL0                    Address : 0x2c
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PUL0                                                  
  Bit             _IO_PUL0_P00                                              
                  _IO_PUL0_P01                                              
                  _IO_PUL0_P02                                              
                  _IO_PUL0_P03                                              
                  _IO_PUL0_P04                                              
                  _IO_PUL0_P05                                              
                  _IO_PUL0_P06                                              
                  _IO_PUL0_P07                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register. 


  I/O Register Name : PULG                    Address : 0x35
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_PULG                                                  
  Bit             _IO_PULG_PG1                                              
                  _IO_PULG_PG2                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T01CR1                  Address : 0x36
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T01CR1                                                
  Bit             _IO_T01CR1_OE                                             
                  _IO_T01CR1_SO                                             
                  _IO_T01CR1_IF                                             
                  _IO_T01CR1_BF                                             
                  _IO_T01CR1_IR                                             
                  _IO_T01CR1_IE                                             
                  _IO_T01CR1_HO                                             
                  _IO_T01CR1_STA                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T00CR1                  Address : 0x37
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T00CR1                                                
  Bit             _IO_T00CR1_OE                                             
                  _IO_T00CR1_SO                                             
                  _IO_T00CR1_IF                                             
                  _IO_T00CR1_BF                                             
                  _IO_T00CR1_IR                                             
                  _IO_T00CR1_IE                                             
                  _IO_T00CR1_HO                                             
                  _IO_T00CR1_STA                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T11CR1                  Address : 0x38
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T11CR1                                                
  Bit             _IO_T11CR1_OE                                             
                  _IO_T11CR1_SO                                             
                  _IO_T11CR1_IF                                             
                  _IO_T11CR1_BF                                             
                  _IO_T11CR1_IR                                             
                  _IO_T11CR1_IE                                             
                  _IO_T11CR1_HO                                             
                  _IO_T11CR1_STA                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T10CR1                  Address : 0x39
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T10CR1                                                
  Bit             _IO_T10CR1_OE                                             
                  _IO_T10CR1_SO                                             
                  _IO_T10CR1_IF                                             
                  _IO_T10CR1_BF                                             
                  _IO_T10CR1_IR                                             
                  _IO_T10CR1_IE                                             
                  _IO_T10CR1_HO                                             
                  _IO_T10CR1_STA                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : EIC10                   Address : 0x49
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_EIC10                                                 
  Bit             _IO_EIC10_EIE0                                            
                  _IO_EIC10_SL00                                            
                  _IO_EIC10_SL01                                            
                  _IO_EIC10_EIR0                                            
                  _IO_EIC10_EIE1                                            
                  _IO_EIC10_SL10                                            
                  _IO_EIC10_SL11                                            
                  _IO_EIC10_EIR1                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : EIC20                   Address : 0x4a
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_EIC20                                                 
  Bit             _IO_EIC20_EIE0                                            
                  _IO_EIC20_SL00                                            
                  _IO_EIC20_SL01                                            
                  _IO_EIC20_EIR0                                            
                  _IO_EIC20_EIE1                                            
                  _IO_EIC20_SL10                                            
                  _IO_EIC20_SL11                                            
                  _IO_EIC20_EIR1                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : EIC30                   Address : 0x4b
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_EIC30                                                 
  Bit             _IO_EIC30_EIE0                                            
                  _IO_EIC30_SL00                                            
                  _IO_EIC30_SL01                                            
                  _IO_EIC30_EIR0                                            
                  _IO_EIC30_EIE1                                            
                  _IO_EIC30_SL10                                            
                  _IO_EIC30_SL11                                            
                  _IO_EIC30_EIR1                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : SCR                     Address : 0x50
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_SCR                                                   
  Bit             _IO_SCR_TXE                                               
                  _IO_SCR_RXE                                               
                  _IO_SCR_CRE                                               
                  _IO_SCR_AD                                                
                  _IO_SCR_CL                                                
                  _IO_SCR_SBL                                               
                  _IO_SCR_P                                                 
                  _IO_SCR_PEN                                               
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : SMR                     Address : 0x51
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_SMR                                                   
  Bit             _IO_SMR_SOE                                               
                  _IO_SMR_SCKE                                              
                  _IO_SMR_UPCL                                              
                  _IO_SMR_REST                                              
                  _IO_SMR_EXT                                               
                  _IO_SMR_OTO                                               
                  _IO_SMR_MD0                                               
                  _IO_SMR_MD1                                               
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : SSR                     Address : 0x52
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_SSR                                                   
  Bit             _IO_SSR_TIE                                               
                  _IO_SSR_RIE                                               
                  _IO_SSR_BDS                                               
                  _IO_SSR_TDRE                                              
                  _IO_SSR_RDRF                                              
                  _IO_SSR_FRE                                               
                  _IO_SSR_ORE                                               
                  _IO_SSR_PE                                                
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : RDR_TDR                 Address : 0x53
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_RDR_TDR                                               
----------------------------------------------------------------------------

  I/O Register Name : ESCR                    Address : 0x54
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ESCR                                                  
  Bit             _IO_ESCR_SCES                                             
                  _IO_ESCR_CCO                                              
                  _IO_ESCR_SIOP                                             
                  _IO_ESCR_SOPE                                             
                  _IO_ESCR_LBL0                                             
                  _IO_ESCR_LBL1                                             
                  _IO_ESCR_LBD                                              
                  _IO_ESCR_LBIE                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : ECCR                    Address : 0x55
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ECCR                                                  
  Bit             _IO_ECCR_TBI                                              
                  _IO_ECCR_RBI                                              
                  _IO_ECCR_SSM                                              
                  _IO_ECCR_SCDE                                             
                  _IO_ECCR_MS                                               
                  _IO_ECCR_LBR                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : ADC1                    Address : 0x6c
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ADC1                                                  
  Bit             _IO_ADC1_AD                                               
                  _IO_ADC1_ADMVX                                            
                  _IO_ADC1_ADMV                                             
                  _IO_ADC1_ADI                                              
                  _IO_ADC1_ANS0                                             
                  _IO_ADC1_ANS1                                             
                  _IO_ADC1_ANS2                                             
                  _IO_ADC1_ANS3                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : ADC2                    Address : 0x6d
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ADC2                                                  
  Bit             _IO_ADC2_CKDIV0                                           
                  _IO_ADC2_CKDIV1                                           
                  _IO_ADC2_EXT                                              
                  _IO_ADC2_ADIE                                             
                  _IO_ADC2_ADCK                                             
                  _IO_ADC2_TIM0                                             
                  _IO_ADC2_TIM1                                             
                  _IO_ADC2_AD8                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : ADD                     Address : 0x6e-0x6f
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ADD                                                   
  Byte/Word       _IO_ADD_ADDH                                              
                  _IO_ADD_ADDL                                              
----------------------------------------------------------------------------

  I/O Register Name : FSR                     Address : 0x72
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_FSR                                                   
  Bit             _IO_FSR_WRE                                               
                  _IO_FSR_IRQEN                                             
                  _IO_FSR_RDY                                               
                  _IO_FSR_RDYIRQ                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : WREN                    Address : 0x76
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WREN                                                  
  Bit             _IO_WREN_EN0                                              
                  _IO_WREN_EN1                                              
                  _IO_WREN_EN2                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : WROR                    Address : 0x77
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WROR                                                  
  Bit             _IO_WROR_DRR0                                             
                  _IO_WROR_DRR1                                             
                  _IO_WROR_DRR2                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : ILR0                    Address : 0x79
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILR0                                                  
----------------------------------------------------------------------------

  I/O Register Name : ILR1                    Address : 0x7a
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILR1                                                  
----------------------------------------------------------------------------

  I/O Register Name : ILR2                    Address : 0x7b
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILR2                                                  
----------------------------------------------------------------------------

  I/O Register Name : ILR3                    Address : 0x7c
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILR3                                                  
----------------------------------------------------------------------------

  I/O Register Name : ILR4                    Address : 0x7d
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILR4                                                  
----------------------------------------------------------------------------

  I/O Register Name : ILR5                    Address : 0x7e
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILR5                                                  
----------------------------------------------------------------------------

  I/O Register Name : WRAR0                   Address : 0xf80-0xf81
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WRAR0                                                 
----------------------------------------------------------------------------

  I/O Register Name : WRDR0                   Address : 0xf82
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WRDR0                                                 
----------------------------------------------------------------------------

  I/O Register Name : WRAR1                   Address : 0xf83-0xf84
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WRAR1                                                 
----------------------------------------------------------------------------

  I/O Register Name : WRDR1                   Address : 0xf85
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WRDR1                                                 
----------------------------------------------------------------------------

  I/O Register Name : WRAR2                   Address : 0xf86-0xf87
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WRAR2                                                 
----------------------------------------------------------------------------

  I/O Register Name : WRDR2                   Address : 0xf88
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WRDR2                                                 
----------------------------------------------------------------------------

  I/O Register Name : T01CR0                  Address : 0xf92
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T01CR0                                                
  Bit             _IO_T01CR0_F0                                             
                  _IO_T01CR0_F1                                             
                  _IO_T01CR0_F2                                             
                  _IO_T01CR0_F3                                             
                  _IO_T01CR0_C0                                             
                  _IO_T01CR0_C1                                             
                  _IO_T01CR0_C2                                             
                  _IO_T01CR0_IFE                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register. 


  I/O Register Name : T00CR0                  Address : 0xf93
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T00CR0                                                
  Bit             _IO_T00CR0_F0                                             
                  _IO_T00CR0_F1                                             
                  _IO_T00CR0_F2                                             
                  _IO_T00CR0_F3                                             
                  _IO_T00CR0_C0                                             
                  _IO_T00CR0_C1                                             
                  _IO_T00CR0_C2                                             
                  _IO_T00CR0_IFE                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register. 


  I/O Register Name : T01DR                   Address : 0xf94
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T01DR                                                 
----------------------------------------------------------------------------

  I/O Register Name : T00DR                   Address : 0xf95
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T00DR                                                 
----------------------------------------------------------------------------

  I/O Register Name : TMCR0                   Address : 0xf96
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_TMCR0                                                 
  Bit             _IO_TMCR0_FE00                                            
                  _IO_TMCR0_FE01                                            
                  _IO_TMCR0_FE10                                            
                  _IO_TMCR0_FE11                                            
                  _IO_TMCR0_MOD                                             
                  _IO_TMCR0_IIS                                             
                  _IO_TMCR0_T00                                             
                  _IO_TMCR0_T01                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T11CR0                  Address : 0xf97
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T11CR0                                                
  Bit             _IO_T11CR0_F0                                             
                  _IO_T11CR0_F1                                             
                  _IO_T11CR0_F2                                             
                  _IO_T11CR0_F3                                             
                  _IO_T11CR0_C0                                             
                  _IO_T11CR0_C1                                             
                  _IO_T11CR0_C2                                             
                  _IO_T11CR0_IFE                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T10CR0                  Address : 0xf98
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T10CR0                                                
  Bit             _IO_T10CR0_F0                                             
                  _IO_T10CR0_F1                                             
                  _IO_T10CR0_F2                                             
                  _IO_T10CR0_F3                                             
                  _IO_T10CR0_C0                                             
                  _IO_T10CR0_C1                                             
                  _IO_T10CR0_C2                                             
                  _IO_T10CR0_IFE                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : T11DR                   Address : 0xf99
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T11DR                                                 
----------------------------------------------------------------------------

  I/O Register Name : T10DR                   Address : 0xf9a
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_T10DR                                                 
----------------------------------------------------------------------------

  I/O Register Name : TMCR1                   Address : 0xf9b
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_TMCR1                                                 
  Bit             _IO_TMCR1_FE00                                            
                  _IO_TMCR1_FE01                                            
                  _IO_TMCR1_FE10                                            
                  _IO_TMCR1_FE11                                            
                  _IO_TMCR1_MOD                                             
                  _IO_TMCR1_IIS                                             
                  _IO_TMCR1_T00                                             
                  _IO_TMCR1_T01                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : BGR1                    Address : 0xfbc
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_BGR1                                                  
----------------------------------------------------------------------------

  I/O Register Name : BGR0                    Address : 0xfbd
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_BGR0                                                  
----------------------------------------------------------------------------

  I/O Register Name : AIDRL                   Address : 0xfc3
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_AIDRL                                                 
  Bit             _IO_AIDRL_P00                                             
                  _IO_AIDRL_P01                                             
                  _IO_AIDRL_P02                                             
                  _IO_AIDRL_P03                                             
                  _IO_AIDRL_P04                                             
                  _IO_AIDRL_P05                                             
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : CRTH                    Address : 0xfe4
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_CRTH                                                  
  Bit             _IO_CRTH_CRTH0                                            
                  _IO_CRTH_CRTH1                                            
                  _IO_CRTH_CRTH2                                            
                  _IO_CRTH_CRTH3                                            
                  _IO_CRTH_CRTH4                                            
                  _IO_CRTH_CRSEL0                                           
                  _IO_CRTH_CRSEL1                                           
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : CRTL                    Address : 0xfe5
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_CRTL                                                  
  Bit             _IO_CRTL_CRTL0                                            
                  _IO_CRTL_CRTL1                                            
                  _IO_CRTL_CRTL2                                            
                  _IO_CRTL_CRTL3                                            
                  _IO_CRTL_CRTL4                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : SYSC                    Address : 0xfe8
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_SYSC                                                  
  Bit             _IO_SYSC_RSTEN                                            
                  _IO_SYSC_RSTOE                                            
                  _IO_SYSC_EC0SL                                            
                  _IO_SYSC_EXCK0                                            
                  _IO_SYSC_EXCK1                                            
                  _IO_SYSC_PFSEL                                            
                  _IO_SYSC_PGSEL                                            
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : CMCR                    Address : 0xfe9
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_CMCR                                                  
  Bit             _IO_CMCR_CMCEN                                            
                  _IO_CMCR_TBTSEL0                                          
                  _IO_CMCR_TBTSEL1                                          
                  _IO_CMCR_TBTSEL2                                          
                  _IO_CMCR_CMCSEL                                           
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.


  I/O Register Name : CMDR                    Address : 0xfea
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_CMDR                                                  
----------------------------------------------------------------------------

  I/O Register Name : WDTH                    Address : 0xfeb
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WDTH                                                  
----------------------------------------------------------------------------

  I/O Register Name : WDTL                    Address : 0xfec
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_WDTL                                                  
----------------------------------------------------------------------------

  I/O Register Name : ILSR                    Address : 0xfee
----------------------------------------------------------------------------
  Access Type     Symbol Name                 Macro Name
----------------------------------------------------------------------------
  Byte/Word       _IO_ILSR                                                  
  Bit             _IO_ILSR_P04                                              
----------------------------------------------------------------------------

Note : Please substitute the constant in using an easy alternative expression
       when you write this register.





  [History]
   V01L01   13 Feb 2008 - created
   V01L02   02 Jul 2008 - ESCR(0x54) register bit1 error correction
                                    (CC0 -> CCO)[zero -> oh]
                        - SYSC(0xFE8) register bit6 error correction
                                    (PF1_PF0 -> PFSEL)
                        - SYSC(0xFE8) register bit7 error correction
                                    (PG1_PG0 -> PGSEL)
                        - CMCR(0xFE9) register bit4 error correction
                                    (TBTSEL3 -> CMCSEL)
                        - CMCR(0xFE9) register bit5 error correction
                                    (CMCSEL -> reserved)



+-----------------------------------------------------------------------------+
| - The contents of this document are subject to change without notice.       |
|   Customers are advised to consult with sales representatives before        |
|   ordering.                                                                 |
| - The information, such as descriptions of function and application circuit |
|   examples, in this document are presented solely for the purpose of        |
|   reference to show examples of operations and uses of FUJITSU              |
|   MICROELECTRONICS semiconductor device; FUJITSU MICROELECTRONICS does not  |
|   warrant proper operation of the device with respect to use based on such  |
|   information. When you develop equipment incorporating the device based on |
|   such information, you must assume any responsibility arising out of such  |
|   use of the information.                                                   |
|   FUJITSU MICROELECTRONICS assumes no liability for any damages whatsoever  |
|   arising out of the use of the information.                                |
| - Any information in this document, including descriptions of function and  |
|   schematic diagrams, shall not be construed as license of the use or       |
|   exercise of any intellectual property right, such as patent right or      |
|   copyright, or any other right of FUJITSU MICROELECTRONICS or any third    |
|   party or does FUJITSU MICROELECTRONICS warrant non-infringement of any    |
|   third-party's intellectual property right or other right by using such    |
|   information. FUJITSU MICROELECTRONICS assumes no liability for any        |
|   infringement of the intellectual property rights or other rights of third |
|   parties which would result from the use of information contained herein.  |
| - The products described in this document are designed, developed and       |
|   manufactured as contemplated for general use, including without           |
|   limitation, ordinary industrial use, general office use, personal use,    |
|   and household use, but are not designed, developed and manufactured as    |
|   contemplated (1) for use accompanying fatal risks or dangers that, unless |
|   extremely high safety is secured, could have a serious effect to the      |
|   public, and could lead directly to death, personal injury, severe         |
|   physical damage or other loss (i.e., nuclear reaction control in nuclear  |
|   facility, aircraft flight control, air traffic control, mass transport    |
|   control, medical life support system, missile launch control in weapon    |
|   system), or (2) for use requiring extremely high reliability              |
|   (i.e., submersible repeater and artificial satellite). Please note that   |
|   FUJITSU MICROELECTRONICS will not be liable against you and/or any third  |
|   party for any claims or damages arising in connection with                |
|   above-mentioned uses of the products.                                     |
| - Any semiconductor devices have an inherent chance of failure. You must    |
|   protect against injury, damage or loss from such failures by              |
|   incorporating safety design measures into your facility and equipment     |
|   such as redundancy, fire protection, and prevention of over-current       |
|   levels and other abnormal operating conditions.                           |
| - Exportation/release of any products described in this document may        |
|   require necessary procedures in accordance with the regulations of the    |
|   Foreign Exchange and Foreign Trade Control Law of Japan and/or US export  |
|   control laws.                                                             |
+-----------------------------------------------------------------------------+
 (C)2008  FUJITSU MICROELECTRONICS LIMITED Printed in Japan