==========================================================================
	     Installation of Pspice Model of Power IC Driver

			International Rectifier
==========================================================================
                 
A high level abstract behavioral PSPICE model has been developed to simulate 
the electrical performance of IR21365 driver. The model can be used in Pspice
version 8 or later (MicroSim Pspice). The IR21365 package includes three 
files:
   1. Pspice subcircuit model file (IR21365.sub)
   2. Symbol file (IR21365.slb)
   3. Instruction file (IR21365.txt)

The subcircuit model can be called directly in a plain Pspice netlist or
more user friendly pspice schematics. 

To use the subcircuit model within a netlist,simply copy and paste the sub-
circuit text in the netlist using a text editor. The subcircuit model can be
instantiated by an X (subcircuit installation) device. For example:
   Xdriver HIN LIN 0 LO VS HO VB VCC IR21365

To use the subcircuit model in a Pspice schematics editor, follow the steps 
below:
   1. Symbol libray Configuration. From a schematics editor, select Editor 
      Configuration from the Options menu to display Editor Configura-
      tion dialog box. Then select Library Settings to display Library
      Settings dialog box. Type the library name along with its path in the
      Library Name text box. Select the Symbol check box only. Click 
      Add or Add Local to set up a local or global library respectively.
   2. Model library file. In a schematics editor, from Analysis menu,select
      Library and Include Files to display its dialog box. Type in the sub-
      circuit model file name in the upper File Name text box. Then click 
      Add Library* (global use) or Add Library (local use).

Should convergence problems occur, in the .OPTION command, increase the 
ABSTOL = 1pA to 10pA or larger or increase RELTOL = 0.001 to 0.01 or larger.
In addition, adjusting step ceiling, total transient analysis time, or 
iteration number may help. 

International Rectifier reserves the right at any time without notice, to 
update model information. The models are provided as is, without warranty of 
any kind, expressed or implied by IR. Visit specific product pages for 
additional information about technical information including datasheet, 
availability, etc.