Please be advised that the losses incurred during diode reverse recovery are highly dependent on the diF/dt values, 
which are determined by the di/dt of the switch.
The Erec values defined in this model are based on measured data with a particular switch and are influenced by the 
set-up parasitics as well.
In these PLECS models for single diodes, the specified Rg values Rg1, Rg2, ... , Rgn in Ohm correspond to diF/dt values
of diF/dt1, diF/dt2, ..., diF/dtn in A/usec, respectively.
It must be noted that different switches in different set-ups will result in different di/dt values, which will, 
in turn, cause varying Erec losses for the same Rgs defined above.
To obtain a closer approximation of the Erec data for the diode, it is recommended that the corresponding Rg value
be used, given that the di/dt in the application is a known parameter. This may result in a closer correspondence 
between the simulated values and actual Erec losses for the diode.