Flashing new software

The TLD5542-1 multichannel evalboard software can be updated by means of the USB interface without using
dedicated debugger tools. 
This is possible only if the board has software version SW_CostOptimized_4.3 or higher. 
Software version is visible by means of the GUI (Figure 6).

1. Connect the board to an USB port on the PC (be sure FT231X VCP driver is installed)

2. Download and unzip the TLE98xx_BSL (bootstrap loader) file from the TLD5542-1_MULTI_EVL webpage

3. Copy the binary file <code_name>.hex that has to be flashed, into TLE98xx_BSL folder

4. Open a command prompt in the same directory (write „cmd“on the explorer address bar, press enter)

5. Execute the following command line in the command prompt:
   Flash_TLE984x_viaDLL.bat <code_name>.hex      

Flash_TLE984x_viaDLL.bat SW_HBLBIndividualDutyCycle_V1.0.hex

6. Keep S1 button on the evalboard while powering the board ON, by connecting a 12 V power supply

7. Release the S1 button when connection is established. The command line reports:
   o Connect OK, NAD = 0x80, Success!

8. Flashing procedure take up to 1 minute, do not disconnect power supply or the cable during flashing

9. The command lines should report: “INFO: Verify Successful!” Success!”
   o Power-off the board when procedure is over

10. (Optional) repeat from step 4 if the procedure has failed