Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_v2_5_2


DAS Version:	DAS v2.5.2


Date:		21.03.07


Customer:	IFX internal staff; Toolpartner 	


Changes:

1. Changes in servers regarding XC800 derivates
2. New firmware for WigglerBox (v2.6.00) regarding XC800 derivates


####################################################################################################
Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_v2_5


DAS Version:	DAS v2.5.1


Date:		02.03.07


Customer:	IFX internal staff; Toolpartner 	


Changes:

1. No changes of DAS 2.5 sources at all
2. Installer has changed in order to solve a conflict between multiple USB drivers

Notes:

1. The installation is mandatory only for users, who already had the IFX UCAN stick, prototype of miniWiggler(TM) or IFX USB starterkits in use with DAS v2.4, DAS v2.5DRAFT or DAS v2.5


####################################################################################################
Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_v2_5


DAS Version:	DAS v2.5


Date:		02.02.07


Customer:	IFX internal staff; Toolpartner 	


Changes:

1. Changes in WigglerBox-Firmware in terms of stability for 32-, 16- and 8-bit IFX devices (Firmware v2.5.80)  
2. New IFX devices added to servers and WigglerBox Firmware
3. DAS Server "JTAG over USB Chip": Fully support for all relevant 32-, 16- and 8-bit IFX devices
4. Windows WHQL certified drivers for miniWiggler(TM) added
5. Issue with virtual COM Port for Starterkits with FTDI onboard fixed
6. Infineon USB miniWiggler(TM) fully verified and ready for production


####################################################################################################


Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_V2_4


DAS Version:	DAS_v2_4


Date:		22.08.06


Customer:	IFX internal staff; Toolpartner 	


Changes:

1. Changes in WigglerBox-Firmware in terms of stability for 32-, 16- and 8-bit IFX devices
2. New IFX devices added to servers and WigglerBox Firmware
3. DGDS, DGBC, DGPM: Device info Window shows now used Server Port 
4. DAS Server log file shows now wiggler box firmware version
5. DAS Server over USB Chip: Restrict to UCAN/Pegasus devices for this release
6. DAS Server over USB Chip: Optional FTDI device names will be ignored

####################################################################################################





Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_V2_3


DAS Version:	DAS_v2_3


Date:		13.07.06


Customer:	IFX internal staff; Toolpartner 	


Changes:

1. Changes in WigglerBox-Firmware in terms of stability for 32-, 16- and 8-bit IFX devices
2. DAS Server "Das Server over USB Chip" and WHQL certified USB&COM Port driver added
3. Logfile of server shows number of open DAS Server ports
4. Changes in DAS API in terms of robustness
5. New IFX devices added to servers and WigglerBox Firmware


####################################################################################################
Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_V2_2


DAS Version:	DAS_v2_2


Date:		28.04.06


Customer:	IFX Toolpartner	


Changes:

1. OEM free USB driver for Wiggler Box added.



####################################################################################################

Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_V2_1


DAS Version:	DAS_v2_1


Date:		20.03.06


Customer:	IFX Toolpartner	


Changes:

1. Flash Data Error during Firmware Update fixed.
2. Stability for 8bit derivates improved.

####################################################################################################


Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_V2_0


DAS Version:	DAS_v2_0


Date:		16.12.05


Customer:	IFX Toolpartner	


Changes:

1. Firmware Upload for WigglerBox fixed

2. DAS GUI work now without having ADMIN Rights

3. ECP check for PrinterPort Driver removed

4. GDI_DAD issues solved

5. 2 interface OEM free USB driver for HITEX added (usb_das_b1)

6. Improvements in the DAS GUIs (Basic Client and Simulator Control can now be started as well standalone)

7. Perfmeter tool added

8. Latest version (v2200) of WigglerBox Firmware Update added

9. Win98 Support for JTAG driver added


####################################################################################################


Release Notes for Device Access Server (DAS)

CVS-Label:	DAS_V1_9


DAS Version:	DAS_v1.9


Date:		6.9.05


Customer:	IFX Toolpartner	


Changes:

1. XC164CM Support added

2. DAS API DLL
   - DAS List rules checker implemented. If rules are violated, the non
     fatal error DAS_ERROR_LIST_RULE is returned and the list isn't sent.
     The implementation of the check is available in das_api_rules_check.h
     for tool partners.
   - If a DAS List return packet from the DAS Server violates the rule
     n_bytes_ok <= n_bytes, n_bytes_ok is set to 0 and DAS_ERROR_DEVICE_DATA 
     is returned. Previously this has been checked just by an assertion.
     This case may anyway occur only for a non properly implemented ECF.
   - Version number incremented


3. DAS Server JTAG JDRV LPT 
   - Bug fixed: It was not detected properly, whether this is an Installed DAS Server (IDS) 
   - Version number incremented


4. DAS Server USB for Emulation Devices
   - ED: Added enforced firmware download by config file parameter
   - ED: Improved log file output in case of bit "firmware download prohibited" is set
   - JTAG: Added starting of firmware update tool 
	
5. DAS Issue Number 050709f (Bug fixed:  DASHPAS is holding DAS Client files locked, which opened for writing before DASHPAS was started. 

6. DAS Issue Number 050729a (Reboot after installation at XP operating systems necessary) fixed
	 

###################################################################################################



CVS-Label:	DAS_V1_8


DAS Version:	DAS_v1.8


Date:		27.07.05


Customer:	IFX Toolpartner	


Changes:

1. New files for version on DAS_SERVER_JTAG and gdi2das

2. DAS_SERVER_JTAG now returns always an error_code if (n_bytes_ok != n_bytes). Adaptation to DAS_DAD (jtag implementation) and GDI2DAS

3. Allignment check added in DAS_SERVER_JTAG

4. Wrong reset behavior of ifxgwig driver corrected

5. DAS Issue Number 050709b (Initialization of the target registers with the 'init' field from the CFG file) fixed.

6. DAS Issue Number 050709h (Gdi2das returns wrong GPR register values when CP register is not equal to 0xFC00 ) fixed.

	
		 

#########################################################################################

CVS-Label:	DAS_V1_7


DAS Version:	DAS_v1.7


Date:		08.07.05


Customer:	IFX Toolpartner


Changes:	
		 

#########################################################################################


CVS-Label:	DAS_V1_6


DAS Version:	DAS_v1.6


Date:		21.06.05


Customer:	IFX Toolpartner


Changes:	
		 

#########################################################################################




CVS-Label:	DAS_v3.1_Edition_1.5


DAS Version:	DAS_v3.1_Edition_1.5


Date:		15.02.05


Customer:	IFX Toolpartner


Changes:	
		AM(15.02.05): USB11 Server configuration added which just does the DFU download.
		It doesn't open the device nor start a DAS Server thread.
		Operation can be observed as usual with the logfile.
		Note that this is only a development tool for working on the CFI 
		level testbench.
		Needs to be killed with the Windows task manager.

	        UD(28.02.05):
	        das_server_usb_xcp removed from installer
	        das_server_jtag removed from installer. Seperate installer "Das Server JTAG JDRV LPT" available
	        

#########################################################################################

CVS-Label:	DAS_v3_1_Edition_1_4_2


DAS Version:	DAS_v3.1_Edition_1.4


Date:		11.02.2005


Customer:	TASKING/ALTIUM, PLS, Lauterbach, HITEX, VECTOR, DSPACE, Vorwick/BOSCH, Massimo Atti, Bangalore


Changes:	
		1. DAS Server improved in terms of stability
		2. Improved version of "DFU"- and "Tricore-Startup-Code"- Files
		3. New installer generator: InstallShield10.5
		4. 15.02.2005 13:44Microsoft certified USB driver will be installed automatically, if 
		 selected. No customer interaction needed any longer.
		5. Installer detects, what kind of OS is used and it will install the correct JTAG Driver
		6. Reboot after installation can be suppressed. 
		7. New JTAG driver

##########################################################################################