S6SAE100A00VA1001 EVK: Hardware Design Files
================================================================================

This directory contains the hardware design files for S6SAE100AVA1001 EVK. 

The latest HW design files can be found under the current directory. 

Note that this directory also includes archive of the hardware design files
used in the earlier S6SAE100A00VA1001 kit revisions. All these hardware design files
are located under following directory

.\ARCHIVE

The revision number for a given hardware is printed on the back side of the PCBA
(e.g, S6SAE100A00VA1001 Rev02). Make sure to pick the hardware design files matching
to the PCBA. 
================================================================================