XC164CS Release v2.8:

* Following UTP Issues are Been fixed
   * AI00016644
   * AI00016741
   * AI00018153
       
Details of Issue are given below:

*  AI00016644:
    
   Customer Feedback 
   When configuring the PEC channels for DMA transfers, it seems DAvE does not
   allow the destination pointer (DSPTx) to be a memory RAM address for example. Is
   this a DAvE restriction or a XC164CS constrain?

   Internal feedback 
   This customer in New Zealand is actually right about the Dave plugin. Currently it is
   not possible to (PEC) transfer with Dave to a memory area.

*  AI00016741:

   First Name: Jean-Marc
   Last Name: Delaplace
   Email Address: jdelaplace@stago.fr
   Company: Stago Instruments S.A.
   Country: France
   Subject: Missing feature in Dave 2.1 with XC164


   Comment: I found a problem with Dave and the SSC in the XC164. In the SSC
   setting box (tab "Control"), checking the box "Use SSCO8MRST...." reserves the
   three pins for the exclusive use of the SSC. In my case, I use the SSC for output only
   and I use the pin that serves as an input to the SSC as a parallel port output. This is
   not possible using Dave that prevents the ports to be configured as output when the
   SSC is used. Will a new version of Dave address this point?

*  AI00018153:

   The dave DIP system shows only one ASC, the second ASC module (ASC1) is
   missing.

   Please also check that the XC164CM device also has two ASC modules planned.