Digital Application virtual Engineer - DAvE 2.1

 Contents

  

Who's DAvE 

Hi, I'm DAvE, your Digital Application virtual Engineer from Infineon technologies. I'm here to aid you in getting underway to fast and reliable embedded designs with Infineons' range of 8-, 16- and 32-Bit Microcontrollers ...

... but let's finish with the marketing talk and get down to the important details of what I can actually do for you.

I can:

But talk's cheap - the real proof is in the doing, not talking. So let's do ...

 

 

Minimum System Requirements

 

  

Installation Instructions

 

 

Tools

The DAvE CD contains two Compiler Evaluation Version

Keil µVision 2, the new Integrated Development Environment from Keil Software which supports the DAvE Toolinterface. To install µVision 2 start the
SETUP.EXE located in \tools\Keil\Setup on this CD. Link to the Application Note app148.pdf to see how to using the µVision 2 with DAvE.

Tasking C166 Demo, the latest version of the Tasking EDE which supports the DAvE Toolinterface. To install the Tasking Tool start the SETUP.EXE located in \tools\Tasking on this CD. Link to the Application Note README_DEMO.pdf to see how to use the Tasking EDE with DAvE.

 

 

Notes for experienced users of DAvE 1.0

 

 

Support / Feedback

Dear designer, DAvE's only human! We have tested DAvE thoroughly, using a sophisticated test methodology but, as always, in our spirit of no marketing BS, we can only guarantee, that DAvE is 99% bug free. What we ask is that if you - as the end user of DAvE - find part of the 1% that doesn't work, you'll tell us, so we can fix it. Please use DAvE's e-mail address DAvE@infineon.com to let us know what you find or what you think we could do better! For more information on DAvE go to DAvE's web site http://www.infineon.com/DAvE.html .

 

All product names are registered trademarks or trademarks of their respective holders.