Welcome to Installation of IFX Stack Depth Analyzer r1.11
=============================================================

PLEASE READ THIS README FILE BEFORE INTALLATION.

REQUIREMENTS
============
The tool requires Windows XP / Windows 2000 or higher version
with enough free memory based on the application to be tested.

INSTALLATION GUIDE.
===================

Run Setup.exe form the zip file and follow the instructions 
of the installer. The installer will Install IFXTools Stack 
Depth Analyzer on the path provided by the user during 
installation process. It will install two executables. One of 
these is a universal driver that can run in either Command 
Line Interpreter mode or GUI mode.