Welcome to Installation of Signature Analysis Generator(IFXSAG) R1.6.
=====================================================================

PLEASE READ THIS README FILE BEFORE INTALLATION.

REQUIREMENTS
============
The tool requires Windows XP / Windows 2000 or higher version
with enough free memory based on the application to be tested.

INSTALLATION GUIDE.
===================

Run the setup.exe for installing the tool. IFXSAG is a command-line tool.
Execute the tool from the windows command-line after installation.