Infineon XC800 FLOAD - Release Notes

Current Version: XC800 FLOAD v5.4 (January 2013)

Last Version: XC800 FLOAD v5.3.4 (November 2011)

The Infineon XC800 FLOAD is intended to handle the on-chip memories in the microcontrollers of the XC800 family. According to the capabilities of the respectivee on-chip memory device, the program allows erase, program, verify and protect the module. To program a memory device, an Intel-Hex-File can be opened and its contents written into the Flash or XRAM of the device. The target device is connected to the host PC via a standard RS232 or USB ports.

Contents:


Installation

To install Infineon XC800 FLOAD go to the setup directory and run setup.exe.

System requirements:

Supported operating systems:

Please Note:
You will need administrator permissions to install the program on Windows NT based systems.


Supported Microcontroller Families


Supported On-Chip Memory Devices


Supported Communication Devices / Interfaces


Main changes

XC800 FLOAD v5.4

XC800 FLOAD v5.3.4

XC800 FLOAD v5.3.2