XMC Development Tools, Software & Kits
XMC1000 Kits
|
XMC1000 Boot Kit:
Evaluation of XMC1100 series
|
XMC4500 Relax / Relax Lite Kit
|
The XMC4500 Relax Kit and the XMC4500 Relax Lite Kit are new budget-priced evaluation boards for the XMC4000 microcontroller family from Infineon. At the heart of these development platforms is the XMC4500 microcontroller, equipped with an ARM Cortex™-M4F CPU running on 120 MHz, 1MB Flash and 160KB RAM. The Relax Lite Kit offers a complete set of on-board devices and plugs to run USB-based applications and to develop human machine interfaces with buttons and LEDs. The Relax Kit extends Lite Kit functionality with an Ethernet-enabled communication option. It also allows developers to explore mass storage and file systems using a microSD card. In addition, it comes with serial flash memory. Unlike the XMC4000 Hexagon Kits, the XMC4500 Relax and Relax Lite Kits are single-board evaluation platforms. They cannot be extended with application-specific satellite cards for communication, human machine interfaces or actuator and sensor control. Developers should upgrade from the XMC4500 Relax Kit or Relax Lite Kit to the appropriate XMC4000 Hexagon Kit if they require satellite cards for functions such as these. More |
Hexagon Application Kit
|
The Hexagon Application Kit is a versatile new tool for the XMC4000 family. At the heart of this development platform is the CPU board with the new XMC4500 microcontroller. Kit functionality can be expanded to suit specific applications by means of satellite cards. The actuator satellite, for example, provides an extensive range of motor control functions thanks to its resolver circuit, encoder interface and shunt current sensing. The human machine interface (HMI) board comes with an OLED display plus audio, touch and SD/MMC functions. The communication satellite enables developers to implement remote control via Ethernet. This board also supports MultiCAN and RS485 interfaces. In addition to these three satellites, developers can also connect their own boards. More |
DAVE™ 3 – The new generation of DAVE™
|
Infineon’s free development environment, DAVE™ 3 (Digital Application Virtual Engineer), was created to simplify programming and reduce development times. This Eclipse-based platform makes it easy for engineers to develop application software that exposes the full potential of Infineon’s powerful hardware. DAVE™ 3 includes a GNU compiler, a debugger and data visualization utilities. Other commonly used compilers and debuggers can be easily added to this development environment.The platform is built around the DAVE™ apps manager. Using predefined, tested apps, DAVE™ also supports automatic code generation. Alternatively, developers are free to integrate their own apps. Apps can be easily configured using the graphical user interface and adapted to the widest range of applications. More |
3rd Party Software, Tools and Services
|
|
To further facilitate XMC designs, Infineon collaborates with over 20 other providers of complementary development tools, software solutions, training and consulting services. More |
- Documents
- Contact us