Volkswagen to Use Infineon Sensor Chip in Electric Power Steering Systems

Jan 11, 2011 | Business & Financial Press

Neubiberg, Germany – January 11, 2011 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced that in future the Volkswagen AG Business Unit Braunschweig will use Infineon’s Hall sensors in electric power steering systems for vehicles. Infineon’s TLE4998C4 programmable linear Hall sensor will be used for various model ranges. Infineon has already started to deliver the chips.


In the Volkswagen electric power steering systems produced in Braunschweig, Germany, in each case two Hall sensors from Infineon are responsible for accurate steering torque sensing. They measure the steering force exerted and the steering angle, and relay this information to the control unit of the electric power steering system. The latter, in turn, then ensures that the control of the motor responsible for the electric power steering is optimized in terms of the required assist force and energy. The Hall sensors are incorporated in the sensor module of the system supplier to the Braunschweig Business Unit – Valeo Schalter und Sensoren GmbH.


Fundamentally, the TLE4998 Hall sensors are suited for applications requiring accurate rotation and position detection. Automotive applications include, for example, pedal, throttle or gear stick position detection, suspension control or direct torque sensing for electric power steering systems. The special characteristics of Infineon’s Hall sensors are advantageous in this arena. Their temperature compensation and high long-term stability due to stress compensation contribute to a consistently high and robust precision of the signals – throughout the vehicle’s service life and regardless of weather conditions. The TLE4998 Hall sensors support system reliability by a protected digital interface.


Technical information concerning the Hall sensor: unique stress compensation


Infineon is the only manufacturer in the world to provide Hall sensors offering the three interfaces: Short PWM Codes (SPC), Pulse Width Modulation (PWM) and Single Edge Nibble Transmission (SENT). In this way Infineon supports the conversion from analog to digital communication between sensor and control unit of the vehicle steering system. SENT and SPC interfaces allow the system supplier to respond flexibly to automakers’ interface requirements.


Compared to today’s mainstream PWM communication, the SPC interface enhances the accuracy and reliability in safety critical automotive applications as it allows synchronized data transmission with the control unit. This functionality signifies that the microcontroller in the control unit can selectively collect sensor measurement data for processing and has the current measurement data available.


The TLE4998 is designed so as to be capable of compensating for temperature fluctuations and mechanical stress over the lifetime of a vehicle. It has a sensitivity stability three to four times better than that of sensors without stress compensation.


The three interface versions of the TLE4998 family are TLE4998C (SPC), TLE4998P (PWM) and TLE4998S (SENT). Each is available in two packages: PG-SSO-3 with three pins and PG-SSO-4 with four pins. The PG-SSO-4 package version, which is only 1 millimeter thin, allows inserting Infineon’s TLE4998 Hall sensors into even very small air-gaps, as are common in the electric power steering system. Furthermore, a package version is available with two external ceramic capacitors, further improving the EMC capabilities of the sensor and dispensing with external capacitor connection.


Technical information on the TLE 4998 programmable linear Hall sensor is available at www.infineon.com/sensors

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2010 fiscal year (ending September 30), the company reported sales of Euro 3.295 billion with approximately 26,650 employees worldwide. With a global presence, Infineon operates through its subsidiaries in the U.S. from Milpitas, CA, in the Asia-Pacific region from Singapore, and in Japan from Tokyo. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Information Number

INFATV201101.016

Press Photos

  • Infineon's TLE4998C4 programmable linear Hall sensor is used in electric power steering systems by Volkswagen.
    Infineon's TLE4998C4 programmable linear Hall sensor is used in electric power steering systems by Volkswagen.
    TLE4998C4

    JPG | 256 kb | 1800 x 1500 px