Infineon Ships Industry’s First CMOS RF Switches with GaAs Performance

Feb 4, 2008 | Market News

Neubiberg, Germany – February 4, 2008 – Today Infineon Technologies (FSE/NYSE: IFX) announced it is shipping in volume the world’s first RF switches that are manufactured in a CMOS-based process on silicon wafers and offer the equivalent performance of RF switches manufactured in Gallium Arsenide (GaAs) process technology - a technology break-through that has never before been achieved. So far, CMOS-based RF switches had to be manufactured on dedicated, much more expensive sapphire wafers to reach the performance of GaAs switches.

The first CMOS RF switch of a whole new family, the BGS12A, is available in a fine-pitch Wafer-Level Package (WLP) with dimensions of only 0.79mm x 0.54mm, which is approximately 60 percent less printed circuit board (PCB) space compared to the smallest packaged GaAs RF switch on the market. In many wireless products, including cellular phones, WLAN, WiMAX, GPS navigation systems, Bluetooth accessories or remote-keyless entry, RF switches are typically used to implement switching functions for receiving and transmitting (Rx/Tx) data, band select or antenna diversity applications and also enable worldwide roaming. On average, mobile devices are typically equipped with one RF switch. However, some multi-band multi-mode mobile phones are fitted with up to four RF switches.

“Infineon’s CMOS-based RF switches come in a tiny chip-scale package and require no further external components, such as level shifters, offering more space savings for various board designs,” said Michael Mauer, senior director, Silicon Discretes at Infineon Technologies. “With the increasing complexity of modern mobile devices, RF switches are expected to substitute today’s PIN diodes in the next five years.”

According to the US market research group Strategy Analytics, Boston, the worldwide market for RF switches accounted for approximately two billion pieces in 2006 and is expected to double to about four billion pieces by the year 2011.

The new Infineon RF switches are manufactured in a unique RF CMOS technology, combining the benefits of CMOS with outstanding RF performance, such as low insertion loss, low harmonic distortion, good isolation and high power levels. The inherent CMOS advantages include high integration capabilities, cost effectiveness and excellent electrostatic discharge (ESD) robustness. Compared to existing solutions, the CMOS-based RF switches offer the highest integration capabilities; are less expensive than GaAs devices; and allow higher battery life than PIN diodes, because current consumption is significantly reduced. All Infineon RF switches do not require external direct current (DC) blocking capacitors and integrate the complete control logic. CMOS compatible logic levels (1.4 V to 2.8 V) eliminate the need of external level shifters.

Further details on Infineon’s first CMOS RF switch (BGS12A)

The BGS12A is Infineon’s first product in the new CMOS-based RF switches family. It is a general purpose single-pole double-throw (SPDT) RF switch designed for power levels of up to 20dBm, with a P -1dB above 30dBm. The new RF switch offers a high RF performance with an insertion loss of only 0.3dB at a frequency of 1.0GHz, low harmonic distortion, good isolation (34dB at 1.0GHz), and fast switching time of less than 4µs. The interfaces are protected against 1.5kV HBM (Human Body Model) ESD which improves the production yield of manufacturers of mobile device modules and achieves the required ESD levels. The BGS12A is ideal for use in low- and medium-power applications of up to 3GHz.

Pricing and Availability

The BGS12A is available in volume quantities. Pricing starts at USD 0.70 per piece for quantities of 1,000 units.

Infineon will introduce further members of the new RF switch family with additional package options including the thin small leadless package (TSLP) with up to 16 pins, higher power levels of 38dBm and up to nine Tx/Rx ports for a broad range of wireless applications. Volume production of the other family members is expected to begin the second half of 2008.

For more information about Infineon’s CMOS RF switches, please go to www.infineon.com/RFswitches or visit us at the Mobile World Congress (Barcelona, Spain, February 12-14, 2008) in hall 1 on booth #B19.

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, communications, and security. In the 2007 fiscal year (ending September), the company reported sales of Euro 7.7 billion (including Qimonda sales of Euro 3.6 billion) with approximately 43,000 employees worldwide (including approximately 13,500 Qimonda employees). With a global presence, Infineon operates through its subsidiaries in the U.S. from Milpitas, CA, in the Asia-Pacific region from Singapore, and in Japan from Tokyo. Infineon is listed on the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX).

Information Number

INFAIM200802.032

Press Photos

  • Infineon's CMOS RF switch BGS12A is only 0.79mm x 0.54mm wide. Compared to the smallest  Gallium Arsenide (GaAs) RF switch package on the market, the BGS12A takes approximately 60 percent less board space in a mobile device. However, it offers the equivalent performance of GaAs RF switches.
    Infineon's CMOS RF switch BGS12A is only 0.79mm x 0.54mm wide. Compared to the smallest Gallium Arsenide (GaAs) RF switch package on the market, the BGS12A takes approximately 60 percent less board space in a mobile device. However, it offers the equivalent performance of GaAs RF switches.
    BGS12A

    JPG | 869 kb | 3543 x 2953 px