Shareholder Structure
The number of shares held by the investors listed in the following table is taken from the respective latest shareholder notification to Infineon. The stated percentages in the first column refer to the share capital held at the
date of the respective notification. The percentages in the second column refer to the
current share capital and shall present a simplified overview on the current shareholder structure.
More information about the reporting and disclosure requirements of shareholders can be found below the table.
| 100% Free float | relating to the number
of shares at the date of the notification |
relating to the current share capital (1,086,742,085 shares) |
|---|---|---|
| Odey Asset
Management LLP |
3.16%
|
2.18% |
| Norges Bank |
3.15%
|
3.15% |
| Capital Group
International, Inc. |
4.93%
|
3.40% |
| Dodge & Cox
(thereof 9.88% Dodge & Cox International Stock Fund) |
9.95%
|
9.82% |
(Status: as of November 3, 2009)
Disclosure Requirements for Shareholders
The German Securities Trading Act (Wertpapierhandelsgesetz) requires each person whose shareholding
reaches,
exceeds or, after exceeding,
falls
below the 3%, 5%, 10%, 15%, 20%, 25%, 30%, 50% or 75% voting rights thresholds of a listed corporation to notify such corporation and the German Federal Supervisory Authority for Financial Services (Bundesanstalt für Finanzdienstleistungsaufsicht - "BaFin") immediately, but no later than four trading days after they have reached, exceeded or fallen below such a threshold. For the purpose of determining the relevant shareholding, voting rights which are deemed to be held by way of attribution according to the rules of the German Securities Trading Act have to be taken into consideration. The violation of the disclosure requirement has serious consequences: Such holders cannot exercise any rights from those shares until they have satisfied this disclosure requirement (in certain cases the prohibition to exercise these rights lasts even six months). Besides, a fine of up to 200,000 euros can be imposed on the relevant shareholder.
Changes of Address in Share Register
Infineon shareholders can arrange online for a change in their address to be noted in the official share register (by clicking on "Shareholder" on the link below).
registrar services GmbH