Revolutionizing augmented reality with Infineon’s new MEMS scanner for eyeglasses and head-up displays

Aug 9, 2021 | Business & Financial Press

Munich, Germany – 9 August 2021 – What if your everyday eyeglasses became the next media for augmented reality applications? What if every car could display valuable data on the whole windshield to securely guide you through the traffic? The new MEMS* scanner solution from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY), comprising a MEMS mirror and MEMS driver, allows completely new product designs. Its miniature size and low power consumption are the basis for making augmented reality (AR) solutions more widely available for consumer applications such as wearables and for automotive head-up displays.

“Augmented reality solutions enrich real environments with valuable digital data and help people to move around more conveniently and safely in daily life, for business and leisure activities, but especially on the street,” said Charles Chan, head of Infineon’s automotive MEMS product line. “Maps, infotainment or messages projected on everyday glasses guide people to the nearest supermarket or shared car park around the corner. Overlaying valuable information, from route navigation to driver assistance systems, over the car’s complete windshield, instead of just over a small area in front of the driver, is a major step ahead for improving driving safety and convenience.”

Infineon’s MEMS scanner chipset features an innovative tilting mirror which lays the foundation for a new generation of laser beam scanner (LBS) projectors. Compared to alternative system designs and competitive MEMS scanner solutions, Infineon’s new chipset stands out in terms of performance, size, energy consumption and competitive system costs.

Better customer experience, for all car segments

A major challenge when developing AR-HUDs is integrating the system into the dashboard, due to space restrictions. Conventional HUD systems can be more than 30 liters in optical volume, yet still offer only a very modest field of view. By contrast, laser beam scanners based on Infineon’s MEMS scanner chipsets enable HUD systems with minimum optical volume, so they can be integrated into even the smallest dashboard. Easy integration together with a competitive bill of material also bring AR-HUDs with a large field of view to small cars and compact classes.

Digital information in constant view with AR smart glasses

The Infineon MEMS scanner chipset enables the design of an AR micro-projector which is light in weight and can be aesthetically integrated into all-day-wear eyeglasses and sports glasses. Thanks to the chipset’s low power consumption, small batteries can easily be integrated into the frame, allowing the glasses to be worn conveniently throughout the day without the need to frequently recharge the batteries.

To advance the development of AR smart glasses’ systems for the consumer market, Infineon is collaborating with TriLite Technologies GmbH, a Vienna-based start-up. While Infineon looks after the MEMS scanner chipset, TriLite is responsible for system integration and control algorithms that enhance the optical performance of the system. Both companies combine several years of research in optical MEMS and mass manufacturing capabilities.

*Micro Electro Mechanical Systems

About Infineon

Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon are the key to a better future. In the 2020 fiscal year (ending 30 September), Infineon reported revenue of more than €8.5 billion with a workforce of some 46,700 people worldwide. Following the acquisition of the US company Cypress Semiconductor Corporation in April 2020, Infineon is now a global top 10 semiconductor company.

Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Follow us: TwitterFacebookLinkedIn

Information Number

INFXX202108-091

Press Photos

  • Infineon’s MEMS scanner chipset enables AR-HUD systems with minimum optical volume, so they can be integrated into even the smallest dashboard.
    Infineon’s MEMS scanner chipset enables AR-HUD systems with minimum optical volume, so they can be integrated into even the smallest dashboard.
    AR-HUD_Infineon

    JPG | 1.26 mb | 2126 x 1535 px

  • To advance the development of AR smart glasses’ systems for the consumer market, Infineon is collaborating with TriLite Technologies GmbH (Photo: TriLite Technologies GmbH)
    To advance the development of AR smart glasses’ systems for the consumer market, Infineon is collaborating with TriLite Technologies GmbH (Photo: TriLite Technologies GmbH)
    TriLite-Glasses

    JPG | 110 kb | 2126 x 1129 px